Arduino
  • Products
  • More
Arduino
Blog Am I using the 2N2222 correctly?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: scarcesam
  • Date Created: 10 Feb 2017 8:16 PM Date Created
  • Views 1791 views
  • Likes 1 like
  • Comments 9 comments
Related
Recommended

Am I using the 2N2222 correctly?

scarcesam
scarcesam
10 Feb 2017

This is my first use of transistors in a project. I need to control a SainSmart 16-Channel Relay Module using an Arduino 101(3v3 GPIOs). This Relay Module uses 5 vdc through Opto couplers to power the relays. The input pins on the relay board are at 4.4 vdc and need to be brought to GND to switch on.

When I connected the Arduino 101(3v3 GPIOs) directly to the relay module some of the relays would stay on while others would be controlled by the Arduino. It all worked fine when I tried an Arduino UNO(5v GPIOs) in place of the 101. But, I want to use the BLE capabilities of the 101.

So my solution is to use  2N22222N2222 transistors because I’ve read they are good at general purpose low-mid power switching Below is the configuration I think is correct Any feed back would be greatly appreciated I’ve tried reading the Data Sheet but I’m mostly going off of other forum posts

 

Relay Board inputs; +4.4vdc, input to ground 4mA

Arduino 101; 3.3vdc GPIOs, max 20mA per GPIO

T1  2N22222N2222

R1: 10K, to reduce current through the Base to 0.33 mA

R2: 100K, drop down resistor. (is it needed?)




  2N2222.JPG

 

Thanks!

 

Attachments:
image
  • Sign in to reply

Top Comments

  • rachaelp
    rachaelp over 8 years ago in reply to jc2048 +3
    Jon Clift wrote: I (probably) disagree with Don and Rachael on the need for a pull-up. Yes you are right! I (probably) blame that on trying to answer on a forum after 2am when I should really be in be…
  • D_Hersey
    D_Hersey over 8 years ago +2
    R2 doesn't hurt anything, turns the Q off faster, but the solenoid is probably too slow to notice. You might make R1 4-5x more conductive. You probably need a pull-up resistor for the collector. Remember…
  • D_Hersey
    D_Hersey over 8 years ago +2
    http://www.onsemi.com/pub_link/Collateral/P2N2222A-D.PDF These guys claim a gain of 50 min and are using a 1K input resistor driven by 16V for their tests. Truth is, you can get along with a range of values…
Parents
  • scarcesam
    scarcesam over 8 years ago

    First, thanks for all the feedback!

     

    So, the 2N2222s I ordered turned out to be 2N2222As. I chose them because they were cheap on Amazon. And because this is a temporary project, for learning, I'm not too concerned with quality or having the perfect part. I do want to learn how to find the best fitting parts. So maybe MOSFETS next time. I'm still trying to figure out which specs to search on supplier web sites.

     

    However, I think Rachael had the right idea. The Arduino 101 GPIOs alone can't keep the Relay Module input high enough to keep the optos off. But, it works with a 1k pull up resistor on the input from the Arduino to the relay board. This setup should be draining roughly 9 mA through the Arduino. Well below is max of 20mA.

     

    image

     

     

    I Think I'll use the setup above with the pull up resistor. Do I need a resistor for each individual input? I tried 4 inputs though one 1K resistor and it didn't work. I'll play with the values a bit for power savings but that's not super important. The plan is to use the Arduino and relay module to control the two 12v motors on a kids electric ride-on vehicle. I plan on having a common ground between everything but the Relay module will run off of the cars 12v battery and the Arduino will run off of a separate 9v battery.

     

    Above all else this is a learning experience for me. It's my first dabbling in anything less than 110VAC (former electrician).  So, any other tips or suggestions would be greatly appreciated.

     

    Thanks,

    Sam

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • scarcesam
    scarcesam over 8 years ago

    First, thanks for all the feedback!

     

    So, the 2N2222s I ordered turned out to be 2N2222As. I chose them because they were cheap on Amazon. And because this is a temporary project, for learning, I'm not too concerned with quality or having the perfect part. I do want to learn how to find the best fitting parts. So maybe MOSFETS next time. I'm still trying to figure out which specs to search on supplier web sites.

     

    However, I think Rachael had the right idea. The Arduino 101 GPIOs alone can't keep the Relay Module input high enough to keep the optos off. But, it works with a 1k pull up resistor on the input from the Arduino to the relay board. This setup should be draining roughly 9 mA through the Arduino. Well below is max of 20mA.

     

    image

     

     

    I Think I'll use the setup above with the pull up resistor. Do I need a resistor for each individual input? I tried 4 inputs though one 1K resistor and it didn't work. I'll play with the values a bit for power savings but that's not super important. The plan is to use the Arduino and relay module to control the two 12v motors on a kids electric ride-on vehicle. I plan on having a common ground between everything but the Relay module will run off of the cars 12v battery and the Arduino will run off of a separate 9v battery.

     

    Above all else this is a learning experience for me. It's my first dabbling in anything less than 110VAC (former electrician).  So, any other tips or suggestions would be greatly appreciated.

     

    Thanks,

    Sam

    • Cancel
    • Vote Up +2 Vote Down
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.