Arduino
  • Products
  • More
Arduino
Blog Arduino Day - suggestion: DIN housing with LAN, CAN and LoRa
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 30 Mar 2021 8:19 PM Date Created
  • Views 4014 views
  • Likes 12 likes
  • Comments 13 comments
  • arduino day 2021
Related
Recommended

Arduino Day - suggestion: DIN housing with LAN, CAN and LoRa

Jan Cumps
Jan Cumps
30 Mar 2021

For Arduino Day, belated, a few photos of a project I'm working on.

Arduino MKR 1310 LoRa with Ethernet shield and CAN-shield. In a DIN mounted housing and a LoRa range antenna.

image

It is going to be part of a light industrial test setup.

 

The housing is Arduino MKR DIN rail housing from e14 member hwhardsoft.

Inside:

Arduino MKR 1310Arduino MKR 1310 for LoRa, with a MOLEX 105262MOLEX 105262 868/915 flex antenna.

Arduino MKR ETH shieldArduino MKR ETH shield

Arduino MKR CAN shieldArduino MKR CAN shield

 

image

 

This will be one of a few replaceable options.

I also have a TI CC1100 with a rod antenna, put in a smaller DIN housing, that can do sub-1 GHz duty,

an Avnet SmartEdge IIOTConnect that can do CAN, WiFi  and Ethernet,

and a DIN mounted Raspberry Pi that can do Ethernet, Wifi and can be paired with my home-made CAN driver,

 

image

Happy Arduino Day

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 4 years ago +1
    In the above photos, I put the sun-1 GHz antenna on the transparent front to make the photo interesting. As you can see, I had just put some tape on the back and taped it to the front panel from the backside…
Parents
  • jc2048
    jc2048 over 4 years ago

    If that's a DIN rail box and your DIN rail is horizontal (usually the case), then the arrangement you show also places the antenna horizontal. Problem with that is that there are then going to be partial nulls in the response along the plane of the antenna. (The antenna is basically a dipole, though there's a bit of zig-zagging and the ends folded round, which will modify the radiation pattern a little.) You might consider having the antenna vertical (both ends of the link - remember that the radio waves are polarised, so both ends need to match). If you get it vertical, it will be much more of an omnidirectional pattern and you'll be throwing the energy out parallel to the ground (which is usually where you want the energy to go). The obvious exception to that might be if you had the devices one above another on the floors of a building where there then would be an argument for directing energy up and down.

    This document shows their test results.

    https://www.molex.com/pdm_docs/as/AS-105262-0001-001.pdf

    See section 4.5 for the 2d patterns. I might be wrong, but they may have X and Y swapped on the XY plot (but that doesn't negate the general point I'm making above). Perhaps someone with a better knowledge of RF stuff than me might comment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to jc2048

    In the end, I mounted the antenna on the outside, and drilled a hole.

    image

    After some reflection, I prefer this more than adding a vertical DIN rail.
    I've put transparent tape for a little protection - and because the antenna's background only glues perfectly the first time.
    If I really wanted, I'd be able to fit it on the inside, if I'd grind away 2 profiles on the housing's plastic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to jc2048

    In the end, I mounted the antenna on the outside, and drilled a hole.

    image

    After some reflection, I prefer this more than adding a vertical DIN rail.
    I've put transparent tape for a little protection - and because the antenna's background only glues perfectly the first time.
    If I really wanted, I'd be able to fit it on the inside, if I'd grind away 2 profiles on the housing's plastic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data