Blog Arduino Mega 2560 attached to Cetipede sheild
  • Blog
  • Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Arduino requires membership for participation - click to join
Blog Post Actions
  • Subscribe by email
  • More
  • Cancel
  • Share
  • Subscribe by email
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Former Member
  • Date Created: 25 Jan 2014 2:45 PM Date Created
  • Views 1224 views
  • Likes 0 likes
  • Comments 6 comments
  • arduino
Related
Recommended

Arduino Mega 2560 attached to Cetipede sheild

Former Member
Former Member
25 Jan 2014

I am trying to search for a code to couple the Centipede to the Arduino Mega2560, using the Cetipede 64 pin to work with a simple programme such as 1 input on the Mega and sequence of timings;

 

int pin2 = 2;
int pin3 = 3;
int pin4 = 4;
int pin5 = 5;
int pin6 = 6;
int pin7 = 7;
int pin8 = 8;
int pin9 = 9;
int pin10 = 10;
int pin11 = 11;
int pin12 = 12;
int pin13 = 13;
int pin14 = 14;
int pin15 = 15;
int pin16 = 16;
int pin17 = 17;
int pin18 = 18;
int pin19 = 19;
int pin20 = 20;
int pin21 = 21;
int pin22 = 22;
int pin23 = 23;
int pin24 = 24;
int pin25 = 25;
int timer1 = 500;
int timer2 = 500;
int timer3 = 500;
int val = 0;
int state = HIGH; // the current state of the output pin
int reading; // the current reading from the input pin
int previous = LOW; // the previous reading from the input pin
long time = 0; // the last time the output pin was toggled
long debounce = 200; // the debounce time, increase if the output flickers
int interval = 500;
void setup(){
pinMode(pin2, OUTPUT);
pinMode(pin3, OUTPUT);
pinMode(pin4, OUTPUT);
pinMode(pin5, OUTPUT);
pinMode(pin6, OUTPUT);
pinMode(pin7, OUTPUT);
pinMode(pin8, OUTPUT);
pinMode(pin9, OUTPUT);
pinMode(pin10, OUTPUT);
pinMode(pin11, OUTPUT);
pinMode(pin12, OUTPUT);
pinMode(pin13, OUTPUT);
pinMode(pin14, OUTPUT);
pinMode(pin15, OUTPUT);
pinMode(pin16, OUTPUT);
pinMode(pin17, OUTPUT);
pinMode(pin18, OUTPUT);
pinMode(pin19, OUTPUT);
pinMode(pin20, OUTPUT);
pinMode(pin21, OUTPUT);
pinMode(pin22, OUTPUT);
pinMode(pin23, OUTPUT);
pinMode(pin24, INPUT);
pinMode(pin25, INPUT);
}
void loop() {
reading = digitalRead(pin25);
// if the input just went from LOW and HIGH and we've waited long enough
// to ignore any noise on the circuit, toggle the output pin and remember
// the time
if (reading == HIGH && previous == LOW && millis() - time > debounce) {
// ... invert the output
if (state == HIGH)
state = LOW;
else
state = HIGH;
// ... and remember when the last button press was
time = millis();

digitalWrite(pin12, HIGH);
digitalWrite(pin10, HIGH);
delay(timer3);
digitalWrite(pin2, HIGH);
delay(timer1);

digitalWrite(pin3, HIGH);
delay(timer1);
digitalWrite(pin2, LOW);

digitalWrite(pin4, HIGH);
delay(timer1);
digitalWrite(pin3, LOW);

digitalWrite(pin5, HIGH);
delay(timer1);
digitalWrite(pin4, LOW);

digitalWrite(pin6, HIGH);
delay(timer1);
digitalWrite(pin5, LOW);

digitalWrite(pin7, HIGH);
delay(timer1);
digitalWrite(pin6, LOW);

digitalWrite(pin8, HIGH);
delay(timer1);
digitalWrite(pin7, LOW);

digitalWrite(pin9, HIGH);
delay(timer1);
digitalWrite(pin8, LOW);
delay(timer1);
digitalWrite(pin9, LOW);
digitalWrite(pin10, LOW);
digitalWrite(pin12, LOW);
delay(timer2);
}

//round2
reading = digitalRead(pin24);
// if the input just went from LOW and HIGH and we've waited long enough
// to ignore any noise on the circuit, toggle the output pin and remember
// the time
if (reading == HIGH && previous == LOW && millis() - time > debounce) {
// ... invert the output
if (state == HIGH)
state = LOW;
else
state = HIGH;
// ... and remember when the last button press was
time = millis();


digitalWrite(pin13, HIGH);
digitalWrite(pin11, HIGH);
delay(timer3);
digitalWrite(pin2, HIGH);
digitalWrite(pin9, HIGH);
delay(timer1);

digitalWrite(pin3, HIGH);
digitalWrite(pin8, HIGH);
delay(timer1);
digitalWrite(pin2, LOW);
digitalWrite(pin9, LOW);

digitalWrite(pin4, HIGH);
digitalWrite(pin7, HIGH);
delay(timer1);
digitalWrite(pin3, LOW);
digitalWrite(pin8, LOW);

digitalWrite(pin5, HIGH);
digitalWrite(pin6, HIGH);
delay(timer1);
digitalWrite(pin4, LOW);
digitalWrite(pin7, LOW);

delay(timer1);
digitalWrite(pin5, LOW);
digitalWrite(pin6, LOW);

digitalWrite(pin11, LOW);
digitalWrite(pin13, LOW);
delay(timer2);
}
}

 

Hope I get a reply, I am messed up.

  • Sign in to reply
Parents
  • Former Member
    Former Member over 9 years ago

    Finally I solved part of the puzzle.

    // Example code for Centipede Library

    // Works with Centipede Shield or MCP23017 on Arduino I2C port

     

    #include <Wire.h>

    #include <Centipede.h>

     

     

    /* Available commands

      .digitalWrite([0...127], [LOW...HIGH]) - Acts like normal digitalWrite

      .digitalRead([0...127]) - Acts like normal digitalRead

      .pinMode([0...127], [INPUT...OUTPUT]) - Acts like normal pinMode

      .portWrite([0...7], [0...65535]) - Writes 16-bit value to one port (chip)

      .portRead([0...7]) - Reads 16-bit value from one port (chip)

      .portMode([0...7], [0...65535]) - Write I/O mask to one port (chip)

      .pinPullup([0...127], [LOW...HIGH]) - Sets pullup on input pin

      .portPullup([0...7], [0...65535]) - Sets pullups on one port (chip)

      .init() - Sets all registers to initial values

     

      Examples

      CS.init();

      CS.pinMode(0,OUTPUT);

      CS.digitalWrite(0, HIGH);

      int recpin = CS.digitalRead(0);

      CS.portMode(0, 0b0111111001111110); // 0 = output, 1 = input

      CS.portWrite(0, 0b1000000110000001); // 0 = LOW, 1 = HIGH

      int recport = CS.portRead(0);

      CS.pinPullup(1,HIGH);

      CS.portPullup(0, 0b0111111001111110); // 0 = no pullup, 1 = pullup

    */

     

    Centipede CS; // create Centipede object

    int pin7=7;

    int pin6=6;

    void setup()

    {

      Wire.begin(); // start I2C

     

      CS.initialize(); // set all registers to default

    CS.portMode(0, 0b0000000000000000);

     

     

      //TWBR = 12; // uncomment for 400KHz I2C (on 16MHz Arduinos)

     

    }

     

     

    void loop()

    { 

    CS.digitalWrite (pin7, HIGH);

    CS.digitalWrite (pin6, HIGH);

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Former Member
    Former Member over 9 years ago

    Finally I solved part of the puzzle.

    // Example code for Centipede Library

    // Works with Centipede Shield or MCP23017 on Arduino I2C port

     

    #include <Wire.h>

    #include <Centipede.h>

     

     

    /* Available commands

      .digitalWrite([0...127], [LOW...HIGH]) - Acts like normal digitalWrite

      .digitalRead([0...127]) - Acts like normal digitalRead

      .pinMode([0...127], [INPUT...OUTPUT]) - Acts like normal pinMode

      .portWrite([0...7], [0...65535]) - Writes 16-bit value to one port (chip)

      .portRead([0...7]) - Reads 16-bit value from one port (chip)

      .portMode([0...7], [0...65535]) - Write I/O mask to one port (chip)

      .pinPullup([0...127], [LOW...HIGH]) - Sets pullup on input pin

      .portPullup([0...7], [0...65535]) - Sets pullups on one port (chip)

      .init() - Sets all registers to initial values

     

      Examples

      CS.init();

      CS.pinMode(0,OUTPUT);

      CS.digitalWrite(0, HIGH);

      int recpin = CS.digitalRead(0);

      CS.portMode(0, 0b0111111001111110); // 0 = output, 1 = input

      CS.portWrite(0, 0b1000000110000001); // 0 = LOW, 1 = HIGH

      int recport = CS.portRead(0);

      CS.pinPullup(1,HIGH);

      CS.portPullup(0, 0b0111111001111110); // 0 = no pullup, 1 = pullup

    */

     

    Centipede CS; // create Centipede object

    int pin7=7;

    int pin6=6;

    void setup()

    {

      Wire.begin(); // start I2C

     

      CS.initialize(); // set all registers to default

    CS.portMode(0, 0b0000000000000000);

     

     

      //TWBR = 12; // uncomment for 400KHz I2C (on 16MHz Arduinos)

     

    }

     

     

    void loop()

    { 

    CS.digitalWrite (pin7, HIGH);

    CS.digitalWrite (pin6, HIGH);

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data
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
An Avnet Company © 2023 Premier Farnell Limited. All Rights Reserved.