Arduino
  • Products
  • More
Arduino
Blog DHT22 temperature and Humidity Sensor with Arduino Uno and Ethernet Card (ENC or WizNet) (Instant weather Station)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Robert Peter Oakes
  • Date Created: 6 Apr 2014 5:50 AM Date Created
  • Views 4964 views
  • Likes 3 likes
  • Comments 18 comments
  • dht22
  • 5100
  • arduino
  • wiznet
  • enc28j60
Related
Recommended

DHT22 temperature and Humidity Sensor with Arduino Uno and Ethernet Card (ENC or WizNet) (Instant weather Station)

Robert Peter Oakes
Robert Peter Oakes
6 Apr 2014

This is a quick post to show how easy it is to connect a DHT22 temp and Humidity sensor to an Arduino and have it output its reading on a web page that can easily be accessible from anywhere on the internet

With a little more work you can pretty up the display and add other features. This is just to demonstrate a proof of concept to you

 

The library is directly from the Arduino Playground, what I am demonstrating here is how to combine a few libraries to create something useful, a little more than a blinky sketch. I have found through experience that there is a lot of good educational material on the internet to do just a single function but not too much that actually is useful beyond the educational aspect. What I am going to do in the coming weeks is to build upon this sample prototype in this post and create a full blown useful home thermostat or something similar.

 

this is the sensor :-

image

you can also get the cheaper and less accurate DHT11 but will need to change the code ever so slightly, IE, change this "int chk = DHT.read22(DHT22_PIN)" to "int chk = DHT.read11(DHT11_PIN)" and other places with similar references to DHT22image

 

and the ENC Card looks like this

image

or you can use a Wiznet based Shield

image

Parts are available from eBay, AdaFruit, Sparkfun and other suppliers

Please provide feedback as to any features you would like to see in this as we progress and I will try to include some.

 

 

Oh and for those not following along closely, the Arduino is acting as the web server in this case, you don't need a separate server

 

Thanks

 

Peter

 

Code for the proof of concept

#include <SPI.h>
#include <Wire.h>
#include <Ethernet.h>
//#include <UIPEthernet.h>
#include <dht.h>
#include <stdio.h>
dht DHT;
#define DHT22_PIN 2
float combined_temp_C;
float combined_temp_F;  //create a new variable
byte TempHi;              // Variable hold data high byte
byte TempLo;              // Variable hold data low byte
boolean P_N;              // Bit flag for Positive and Negative
boolean P_N112;
boolean P_N212;
unsigned int Decimal;     // Variable hold decimal value
char * strTempC = NULL;
 char * strTempF = NULL;
byte mac[] = { 0x90, 0xA2, 0xDA, 0x00, 0x4E, 0x10 };  // MAC address 84.85.88.16.0.36
byte ip[]  = { 192, 168, 1, 203 };                     // ip-address, please change to fit your network
byte mydns[] = { 192, 168, 1, 1 };            
byte gateway[] = { 192, 168, 1, 1 };             
byte subnet[] = { 255,255,255,0 }; 
EthernetServer server(80);
static char output[300] = "";
void setup() {
 Serial.begin(9600);
 //ethernet
   Ethernet.begin(mac, ip);
   server.begin();
   Serial.print("server is at ");
   Serial.println(Ethernet.localIP());
}
char headerHTML[] = "HTTP/1.1 200 OK\r\n"
          "Content-Type: text/html\r\n"
          "Connection: close\r\n"
          "Refresh: 5\r\n"
          "\r\n"
          "<!DOCTYPE HTML>"
          "<Title>RBBS Server</Title>"
          "<html>";
          
 char footerHTML[] = "</html>" ;
 
 char * TimeElapsed() { // Was Home Page
  long t = millis() / 1000;
  word h = t / 3600;
  byte m = (t / 60) % 60;
  byte s = t % 60;
  sprintf(output, "<h1>%d%d:%d%d:%d%d</h1>" , h/10, h%10, m/10, m%10, s/10, s%10);
  return output;
}
 void sendTempToNetwork(EthernetClient myClient)
 {
      // now humidity / temp sensor
    int chk = DHT.read22(DHT22_PIN);
    myClient.print("Humidity=");
    myClient.print(DHT.humidity,0);
    myClient.print("%");
    myClient.print("<BR/>");
    myClient.print("Temperature=");
    myClient.print(DHT.temperature, 0);
    myClient.write(" ");
    myClient.print("C");
    myClient.print("<BR/>");
    myClient.print("Dewpoint=");
    myClient.print(dewPoint(DHT.temperature,DHT.humidity), 0);
    myClient.write(" ");
    myClient.print("C");
    myClient.print("<BR/><BR/>");
 }
 void sendAnalogToNetwork(EthernetClient myClient)
 {
    // output the value of each analog input pin for good measure
    for (int analogChannel = 0; analogChannel < 6; analogChannel++) {
      int sensorReading = analogRead(analogChannel);
      myClient.print("analog input ");
      myClient.print(analogChannel);
      myClient.print(" is ");
      myClient.print(sensorReading);
      myClient.println("<br />");       
    }
 }
/*******************************************************************************
 * Main Loop
 *******************************************************************************/
void loop() 
{
// listen for incoming clients
  EthernetClient client = server.available();
  if (client) {
    Serial.println("new client");
    // an http request ends with a blank line
    boolean currentLineIsBlank = true;
    while (client.connected()) {
      if (client.available()) {
        char c = client.read();
        Serial.write(c);
        // if you've gotten to the end of the line (received a newline
        // character) and the line is blank, the http request has ended,
        // so you can send a reply
        if (c == '\n' && currentLineIsBlank) {
          // send a standard http response header
          client.print(headerHTML);
          // now send the stuff we want
          client.print(TimeElapsed()); // your old code here
          // do some more stuff
          sendTempToNetwork(client);
          sendAnalogToNetwork(client);
           // were done sending so now send the footer to close the page
          client.println(footerHTML);
          break;
        }
        if (c == '\n') {
          // you're starting a new line
          currentLineIsBlank = true;
        } 
        else if (c != '\r') {
          // you've gotten a character on the current line
          currentLineIsBlank = false;
        }
      }
    }
    // give the web browser time to receive the data
    delay(1);
    // close the connection:
    client.stop();
    Serial.println("client disconnected");
  }
 delay(2000);
}
void Cal_Temp()
{
  if (TempHi&0x80)     // If bit7 of the TempHi is HIGH then the temperature is negative
    P_N = 0;
  else       // Else the temperature is positive
  P_N = 1;
  TempHi = TempHi & 0x7F;   // Remove sign
  TempLo = TempLo & 0xF0;   // Filter out last nibble
  TempLo = TempLo >>4; // Shift right 4 times
  Decimal = TempLo;
  Decimal = Decimal * 625;  // Each bit = 0.0625 degree C
  combined_temp_C= TempHi + TempLo*.0625;
  combined_temp_F = combined_temp_C*1.8+32;
   sprintf(strTempC, "%f", combined_temp_C);
   sprintf(strTempF, "%f", combined_temp_F);
}
////Celsius to Kelvin conversion
//double Kelvin(double celsius)
//{
//        return celsius + 273.15;
//}
// dewPoint function NOAA
// reference: http://wahiduddin.net/calc/density_algorithms.htm 
double dewPoint(double celsius, double humidity)
{
        double A0= 373.15/(273.15 + celsius);
        double SUM = -7.90298 * (A0-1);
        SUM += 5.02808 * log10(A0);
        SUM += -1.3816e-7 * (pow(10, (11.344*(1-1/A0)))-1) ;
        SUM += 8.1328e-3 * (pow(10,(-3.49149*(A0-1)))-1) ;
        SUM += log10(1013.246);
        double VP = pow(10, SUM-3) * humidity;
        double T = log(VP/0.61078);   // temp var
        return (241.88 * T) / (17.558-T);
}
// delta max = 0.6544 wrt dewPoint()
// 5x faster than dewPoint()
// reference: http://en.wikipedia.org/wiki/Dew_point
double dewPointFast(double celsius, double humidity)
{
        double a = 17.271;
        double b = 237.7;
        double temp = (a * celsius) / (b + celsius) + log(humidity/100);
        double Td = (b * temp) / (a - temp);
        return Td;
}

 

The DHT22 Library can be found here

 

http://arduino.cc/playground/Main/DHTLib

 

 

 

This is a sample of the code and also the resulting output on a web browser to show it works

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Attachments:
DCT22_test.ino.zip
  • Sign in to reply

Top Comments

  • gadget.iom
    gadget.iom over 10 years ago in reply to Former Member +1
    In answer to your first question: DHT: Celsius to Fahrenheit Conversion
  • gadget.iom
    gadget.iom over 10 years ago in reply to Former Member +1
    And your second question: Adafruit DHT - Two sensors
Parents
  • Former Member
    Former Member over 11 years ago

    I look forward to your comments.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to Former Member

    just tried your test and now working 100% from Canada

     

    Nice one

     

    look at my later tutorials, I show how to use a much better display page

    here Fast Track to Arduino Programming - Lesson 4b, How to use an Ethernet Shield with a WEB page

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to Former Member

    just tried your test and now working 100% from Canada

     

    Nice one

     

    look at my later tutorials, I show how to use a much better display page

    here Fast Track to Arduino Programming - Lesson 4b, How to use an Ethernet Shield with a WEB page

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data