Arduino
  • Products
  • More
Arduino
Blog Modify Variables on a Running Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Former Member
  • Date Created: 29 Oct 2012 1:02 AM Date Created
  • Views 1806 views
  • Likes 3 likes
  • Comments 8 comments
  • arduino_debugger
  • visual_micro
  • arduino
  • visual_studio
Related
Recommended

Modify Variables on a Running Arduino

Former Member
Former Member
29 Oct 2012

New Release - Arduino Debugger

 

The Arduino Debugger has taken another step forward. Previously the debugger provided trace/break/step and graphical visualizations. The latest release allows the update of  variables and registers while an Arduino is running. Variables can be updated while the Arduino is running normally (in debug) or during a debug break (pause) event.

 

Read more about Modifying Variables On A Running Arduino at visualmicro.com

 

For this example we show a really pointless (and rubbish) arduino program in debug mode. The message trace has been frozen at a point that makes best reading. The entire arduino program code is shown, You can see that the values of variables are defined to be different to the current values shown in the expression watch window. The serial window shows confirmation that the changes to variable values were succesfully accepted by the Arduino. The variables with a yellow background color are read/write.

 

Visual Studio 2012 in debug mode with the Arduino plugin. Click the image to exand

http://www.visualmicro.com/pics/DebugSetVariableRunningExample2.png

Original Arduino Debugger Post

  • Sign in to reply
Parents
  • fustini
    fustini over 13 years ago

    That's exciting to see a debugger for Arduino as it's something I miss from a more traditional microcontroller environments.  Is any way to run this for Linux users like me?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to fustini

    It would be nice to have a linux version but the current system needs Visual Studio Pro. However the majority of the system is not tied to Visual Studio, so if anyone would like to join the vm forum and collaborate on a different version they will be very welcome.

     

    Maybe "Mono" is a possibility? Eclipse seems like hard work but that is because I need simple things.

     

    Suggestions welcome thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 13 years ago in reply to Former Member

    That's good to here the majority is not VS specific.  I was most impressed that you've somehow figured how to add debugging capabilities to the Arduino.  Does one's sketch have to be instrumented for this to work or is it tapping into the AVR's debugging capabilities directly?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fustini
    fustini over 13 years ago in reply to Former Member

    That's good to here the majority is not VS specific.  I was most impressed that you've somehow figured how to add debugging capabilities to the Arduino.  Does one's sketch have to be instrumented for this to work or is it tapping into the AVR's debugging capabilities directly?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Former Member
    Former Member over 13 years ago in reply to fustini

    I was not able to figure out a way to easily provide debug with AVR capabilities. As you rightly say, the solution is to inject serial code into a copy of the sources during a debug compile.

    The code injection does not inject the text messages into the arduino code. Instead, the test messages are stored on the pc in xml files and displayed in the debug viewers when required.

    So this solution is a hybrid between adding serial debug messages and an integrated debugger. It is very easy to use and friendly but might not be a useful solution for time dependant or very limited memory solutions.

    However, we have had a couple of new users that had so many "old fashioned" arduino serial print messages in their code. So many messages that they had filled up the arduino memory and it crashed. When they used the debugger, they were able to remove the serial messages and replace with breakpoint/tracepoints. This released most of the arduino memory and their projects worked well.

    So this is a real world solution that works well but it is not a highly technical or perfect solution. One other nice thing about using serial is that we also support SoftwareSerial and other "Print" transports. So xbee, bluetooth etc can also be used for debug.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 13 years ago in reply to Former Member

    Very interesting to hear more about your approach.  I can identify with ending up with a mess of print statements across a bunch of files with a complicated Arduino project.  I didn't even consider the additional negative that it is taking up memory with the strings.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to fustini

    I'll be honest with you. I did the same before the debugger and also did not realise the implications. Even then, it only became clear to me when the first user sent me his sketch code which caused the arduino to randomly crash Well it wasn't randomly crashing but each time he added a new debug message to try to trap the crash the crash happened in a different locationimage.

     

    At the same time, another user requested that the plugin optionally provide a detailed memory usage report after each arduino compilation. I tested the new memory report feature on the sketch and was surpised to see how easily the debug strings had consumed 80% of the arduino memory. Leaving too little for what the code neded to allocate at runtime . It was an interesting and a useful reminder!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 13 years ago in reply to Former Member

    I really like that you've added a memory usage feature, too.  I was working with a WiFi shield in which the sketch and all the libraries were on the borderline of the ATMega328 SRAM.  It was really maddening troubleshooting under those circumstances.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to fustini

    Not wishing to steal your thunder, but there is another program undergoing beta testing for the Arduino support right now.

     

    Hanno Sander is a NZ'er that works with Parallax and has developed '12blocks' which is multi platform, using drag and drop.

    It's available for a 30 day evaluation and is cheap, given its abilities, and the number of platforms it supports, along with all three OS's.

     

    One of the great features is the ability to modify and get the value of variables in real time.

     

    Keep an eye out for it at www.12blocks.com

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down