<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>Arduino with Current Transformer</title><link>/products/arduino/b/blog/posts/arduino-with-current-transformer</link><description>Hi! Does anyone has any experience with current transformer with arduino?I just bought a split core current transformer (SCT-0400-025) from Magnelab and I want to connect to arduino.According to the datasheet, the input current is 25A and output...</description><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>RE: Arduino with Current Transformer</title><link>https://community.element14.com/products/arduino/b/blog/posts/arduino-with-current-transformer</link><pubDate>Wed, 19 Oct 2016 04:37:34 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:2b01433c-6723-4659-838c-75b3288e1885</guid><dc:creator>Robert Peter Oakes</dc:creator><slash:comments>1</slash:comments><description>&lt;p&gt;As per the datasheet, it already has a burden resistor so does not need an additional one&lt;/p&gt;&lt;p&gt;&amp;nbsp;&lt;/p&gt;&lt;p&gt;You will however probably need an op amp to boost the signal as your only going to get 0.333V at full 25A, this limits the ADCs range quite a lot. A 10x amplification would help a lot taking the input to the ADC to 3.33V, you could use more gain to increase output to close to 5V if your using a 5V reference on the ADC, if not then you will have to adjust to align with the ADC full scale.&lt;/p&gt;&lt;p&gt;&amp;nbsp;&lt;/p&gt;&lt;p&gt;Also the output of the CT is not DC, it is AC so you will have to sample quite fast to profile the waveform, either that or use a diode and a cap to rectify the signal&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=2124&amp;AppID=145&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item></channel></rss>