<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>CSI Camera on Uno Q Media Carrier</title><link>/products/arduino/b/blog/posts/csi-camera-on-uno-q-media-carrier</link><description>I recently purchased an Arduino Media Carrier board for the Uno Q and decided to try it out with the Uno Q that I won in the Show &amp;amp; Tell Contest. I&amp;#39;d like to try out some facial recognition and audio IO applications before receiving my ...</description><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>RE: CSI Camera on Uno Q Media Carrier</title><link>https://community.element14.com/products/arduino/b/blog/posts/csi-camera-on-uno-q-media-carrier</link><pubDate>Mon, 09 Nov 2026 12:09:06 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:d9a5745d-e1ff-4590-9662-2aa094db000a</guid><dc:creator>geralds</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;Hi&amp;nbsp;&amp;nbsp;[mention:dc11ece8204f479e8dce2a47a33b20d3:e9ed411860ed4f2ba0265705b8793d05]&amp;nbsp;,&lt;/p&gt;
&lt;p&gt;Thank you very much for the information. It is a great help for programming my &amp;quot;-Q&amp;quot; boards.&lt;/p&gt;
&lt;p&gt;Yesterday, I tested the audio code&amp;mdash;provided by someone (&lt;a id="" href="https://forum.arduino.cc/u/ptillisch" rel="noopener noreferrer nofollow" target="_blank" data-e14adj="t"&gt;https://forum.arduino.cc/u/ptillisch&lt;/a&gt;) on the Arduino forum&amp;mdash;using the VentunoQ and the Media Carrier Board.&lt;br /&gt;It works! That&amp;rsquo;s fantastic; it provides a solid foundation for further exploration.&lt;/p&gt;
&lt;p&gt;&lt;em&gt;aplay --device=&amp;quot;plughw:CARD=monacogertrude,DEV=0&amp;quot; &amp;quot;/usr/share/sounds/alsa/Front_Center.wav&amp;quot;&lt;/em&gt;&lt;/p&gt;
&lt;p&gt;If I understand correctly, this means the audio interface (the card) is named &amp;quot;monacogertrude.&amp;quot; The Ubuntu operating system includes several pre-existing WAV files in the `/usr/share/sounds/alsa/` directory.&lt;br /&gt;The command above plays the &amp;quot;Front_Center.wav&amp;quot; file.&lt;/p&gt;
&lt;p&gt;The Media Board features a 3.5mm 4-pole jack for a headset.&lt;br /&gt;The output is routed there; I assume `DEV=0` refers to the endpoint.&lt;/p&gt;
&lt;p&gt;I was also given a command for recording audio:&lt;br /&gt;&lt;em&gt;arecord --device=&amp;quot;plughw:CARD=monacogertrude,DEV=1&amp;quot; --duration=5 --format S32_LE --rate=48000 recording.wav&lt;/em&gt;&lt;/p&gt;
&lt;p&gt;However, this doesn&amp;#39;t work yet, as the command doesn&amp;#39;t specify where the `recording.wav` file should be saved. It seems I need to create a folder and the file first and then include that path in the command.&lt;br /&gt;I believe these two commands are a good starting point&amp;mdash;along with digging out the appropriate driver from the system.&lt;br /&gt;Now I have to find in a manual DEV=0, DEV=1.&lt;/p&gt;
&lt;p&gt;In short: The Media Carrier Board and the VentunoQ are capable of communicating with each other.&lt;br /&gt;This also means that the drivers from Arduino are not yet complete and are in urgent need of an update.&lt;/p&gt;
&lt;p&gt;If I&amp;rsquo;ve understood correctly&amp;mdash;and I don&amp;rsquo;t want to state anything inaccurate&amp;mdash;there is also a mention on the Arduino forum that a dedicated &amp;quot;Media Carrier Board&amp;quot; is being developed specifically for the Ventuno-Q.&lt;br /&gt;However, this would mean that &amp;quot;compatibility&amp;quot; is effectively a thing of the past. &lt;br /&gt;Having one board for the UNO-Q and another for the Ventuno-Q doesn&amp;#39;t make sense to me, especially since all the schematics and plans show the same connections&amp;mdash;unless, of course, there is some additional circuitry required on the board for the Ventuno-Q.&lt;br /&gt;Granted, the real difference lies in the codecs on the respective &amp;quot;-Q&amp;quot; boards, but the amplifiers on the Media Board would be identical.&lt;/p&gt;
&lt;p&gt;This is the CODEC on the VentunuQ: MAX98091&lt;br /&gt;&lt;a href="https://www.analog.com/en/products/max98091.html#documentation" rel="noopener noreferrer nofollow" target="_blank" data-e14adj="t"&gt;https://www.analog.com/en/products/max98091.html#documentation&lt;/a&gt;&amp;nbsp;&lt;/p&gt;
&lt;p&gt;Here is the correspondence:&lt;/p&gt;
&lt;p&gt;&lt;a id="" href="https://forum.arduino.cc/t/ventuno-q-media-carrier-waveshare-8-dsi-touch-a-display-overlay-needed/1460252" rel="noopener noreferrer nofollow" target="_blank" data-e14adj="t"&gt;https://forum.arduino.cc/t/ventuno-q-media-carrier-waveshare-8-dsi-touch-a-display-overlay-needed/1460252&lt;/a&gt;&lt;/p&gt;
&lt;p&gt;--&lt;/p&gt;
&lt;p&gt;Update:&lt;/p&gt;
&lt;p&gt;The App Lab is actually 0.12.0 - I installed it yesterday.&lt;br /&gt;&lt;br /&gt;There is also a new Ubuntu operating system image available that can be flashed onto the board&amp;mdash;applicable to&lt;br /&gt; both the UNO-Q,&amp;nbsp;&lt;span&gt;20260528-558,&lt;/span&gt; and the Ventuno-Q,&amp;nbsp;&lt;span&gt;20260729-248&lt;/span&gt;. I have the older versions.&lt;/p&gt;
&lt;p&gt;&lt;a id="" href="https://www.arduino.cc/en/software/linux-images/" rel="noopener noreferrer nofollow" target="_blank" data-e14adj="t"&gt;https://www.arduino.cc/en/software/linux-images/&lt;/a&gt;&lt;/p&gt;
&lt;p&gt;How to flash the image:&lt;/p&gt;
&lt;p&gt;&lt;a id="" href="https://docs.arduino.cc/tutorials/ventuno-q/flash-image/" rel="noopener noreferrer nofollow" target="_blank" data-e14adj="t"&gt;https://docs.arduino.cc/tutorials/ventuno-q/flash-image/&lt;/a&gt;&amp;nbsp;&lt;/p&gt;
&lt;p&gt;However, I still have some concerns regarding whether the flashing process will go smoothly.&lt;/p&gt;
&lt;p&gt;I am unable to install the &amp;quot;adb&amp;quot; command on my Ventuno-Q.&lt;br /&gt;&lt;a href="https://docs.arduino.cc/tutorials/ventuno-q/user-manual/#access-via-adb" rel="noopener noreferrer nofollow" target="_blank" data-e14adj="t"&gt;https://docs.arduino.cc/tutorials/ventuno-q/user-manual/#access-via-adb&lt;/a&gt;&amp;nbsp;&lt;/p&gt;
&lt;p&gt;When I attempt to install it, I encounter an error: &amp;quot;a module cannot be installed; it cannot be found.&amp;quot;&lt;br /&gt;The flashing process involves, among other things, the vendor ID (05c6); if this is lost during the flash, it must be entered manually.&lt;br /&gt;&lt;a href="https://docs.arduino.cc/software/app-lab/setup/linux/#step-2-configure-udev-rules" rel="noopener noreferrer nofollow" target="_blank" data-e14adj="t"&gt;https://docs.arduino.cc/software/app-lab/setup/linux/#step-2-configure-udev-rules&lt;/a&gt;&amp;nbsp;&lt;/p&gt;
&lt;p&gt;And after that we must install the App Lab manuell too.&lt;/p&gt;
&lt;p&gt;...it is growing&amp;nbsp;up to a hard work...&lt;/p&gt;
&lt;p&gt;I&amp;#39;ve purchased two of the supported MIPI/CSI ArduCam, I&amp;#39;m waiting for the flashing until I received and testet this both cameras.&lt;br /&gt;&lt;a id="" href="https://www.arducam.com/arducam-imx577-mini-camera-module-for-qualcomm-rb3g2.html" rel="noopener noreferrer nofollow" target="_blank" data-e14adj="t"&gt;https://www.arducam.com/arducam-imx577-mini-camera-module-for-qualcomm-rb3g2.html&lt;/a&gt;&amp;nbsp;&lt;/p&gt;
&lt;p&gt;Well, this was my last few days.&lt;/p&gt;
&lt;p&gt;Best Regards&lt;/p&gt;
&lt;p&gt;Gerald&lt;br /&gt;--&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=30390&amp;AppID=145&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item><item><title>RE: CSI Camera on Uno Q Media Carrier</title><link>https://community.element14.com/products/arduino/b/blog/posts/csi-camera-on-uno-q-media-carrier</link><pubDate>Mon, 09 Nov 2026 06:39:11 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:d9a5745d-e1ff-4590-9662-2aa094db000a</guid><dc:creator>embeddedguy</dc:creator><slash:comments>1</slash:comments><description>&lt;p&gt;Great to see new board. But I think media carrier board you will get it in the road test.&amp;nbsp;&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=30390&amp;AppID=145&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item></channel></rss>