Arduino Forum How to code a dead band of 10us in Arduino?
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
  • State Not Answered
  • Replies 13 replies
  • Subscribers 404 subscribers
  • Views 2950 views
  • Users 0 members are here
  • deadband
  • project
  • programming
  • inverter
  • arduino
Related

How to code a dead band of 10us in Arduino?

Former Member
Former Member over 11 years ago

Hello all!

I am trying to run an H-bridge Inverter using Arduino. I am generating PWM pulses through Arduino and using IR2110, I am feeding those pulses to the switches. My problem is, I want to add dead band of 10us in programming it self. I want to generate 4 PWM signals A,B,C and D where A and B will have a deadband. C will be a complimentary wave of A and D will be  complimentary wave for B.
But I am not able to get this deadband by putting  " delaymicroseconds(10); " code.

 

Please help me out for this.

Thanks.

Palash

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to dmaruska +3
    From memory, not a data sheet It is the transition time where both upper and lower drivers are off, without this there is a risk that a momentary shorting path will exist as an upper driver and a lower…
  • michaelkellett
    michaelkellett over 11 years ago +1
    It isn't really feasible to implement dead band timing on a micro unless it has hardware support in a timer or motor driver peripheral. Many ARM based micros form ST and NXP and other parts form Microchip…
Parents
  • michaelkellett
    0 michaelkellett over 11 years ago

    It isn't really feasible to implement dead band timing on a micro unless it has hardware support in a timer or motor driver peripheral. Many ARM based micros form ST and NXP  and other parts form Microchip and TI offer this feature but the Atmel based Arduino does not.

    You could consider using a driver chip like this:

    http://www.intersil.com/content/dam/Intersil/documents/isl7/isl78420.pdf

    with hardware dead band control (only up to 220nS - your 10uS is much longer than would normally be considered).

     

    It may be that you have outgrown the Arduino (the IR2110 isn't what I would call a beginner's part) and you should perhaps look at better equipped micros.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to michaelkellett

    Also, I wonder if 10us dead time is very much high or it is okay to deal with?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to Former Member

    You can't expect to just find a circuit and use it - if you think the ISL78420 might do you need to study the data sheet and any app notes. You can't use chips like this without designing pcbs and making them - so it's good to be very confident that your design will work before you start trying to make it.

     

    With regard to the dead time - think about why you need dead time ?

    You can only decide on the right amount by calculation or simulation. If you post the ciruit you are thinking of using and the specification that it must meet, it might be possible to advise you.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to Former Member

    You can't expect to just find a circuit and use it - if you think the ISL78420 might do you need to study the data sheet and any app notes. You can't use chips like this without designing pcbs and making them - so it's good to be very confident that your design will work before you start trying to make it.

     

    With regard to the dead time - think about why you need dead time ?

    You can only decide on the right amount by calculation or simulation. If you post the ciruit you are thinking of using and the specification that it must meet, it might be possible to advise you.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to michaelkellett

    Actually, I have done all that for IR2110 so I don't have much time for this. My IR2110 cards are running well so I need only to code a PWM with appropriate dead band. I though you might have worked on that chip and so asked you to share it. Anyways, I have tried to generate the dead band through a code. I will try it tomorrow and post the results here. Proteus is showing some promising results. Will post here if my inverter works fine image