Arduino Forum ARDUINO UNO LED + SWITCH
  • Blog
  • Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Arduino requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 95 subscribers
  • Views 228 views
  • Users 0 members are here
Related

ARDUINO UNO LED + SWITCH

wimydnvr
wimydnvr over 1 year ago

Hi guys. Can i get an example code for situation below.


if the switch is press, led red will turn on for 3 seconds, then end process.

if the switch is not press, led green will turn on for 3 seconds then end process.

Ive been struggling to do the code.

I use 1 button switch, 1 green led & 1 red led.

  • Reply
  • Cancel
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 1 year ago +3 suggested

    The code for that is really simple so you should be able to figure out what you need.  Here's a link to something that shows an led being lit when a button is pressed: you can extrapolate from that…

  • javagoza
    javagoza over 1 year ago +1 suggested

    Just use a flag to keep track if the process is done or not.

    When you detect a change from press to not press or from no press to press activate the flag

     

    setup(){
         set lastButtonState to pressed;
      …

Parents
  • Andrew J
    0 Andrew J over 1 year ago

    The code for that is really simple so you should be able to figure out what you need.  Here's a link to something that shows an led being lit when a button is pressed: you can extrapolate from that to what you need in terms of turning an led on or off.  Arduino function: delay(3000) will pause execution for 3 seconds (3000 milliseconds).  So you could turn an LED on, delay for 3 seconds, then turn it off.

     

    You will have to decide what you mean by "if the switch is not pressed" because of course the majority of the time it won't be pressed, so how often do you want to light the green LED when it detects the button not pressed. 

     

    The link has code that shows you how to detect if a button is pressed or not pressed and how to turn on and turn off an LED.  It also has pictures on how to wire up the button and LED - for your second LED do the same but with a different digital port, e.g. 4.  You don't need to use more than one breadboard if you don't want to as long as you make sure your wiring is correct.

    • Cancel
    • Up +3 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 1 year ago

    The code for that is really simple so you should be able to figure out what you need.  Here's a link to something that shows an led being lit when a button is pressed: you can extrapolate from that to what you need in terms of turning an led on or off.  Arduino function: delay(3000) will pause execution for 3 seconds (3000 milliseconds).  So you could turn an LED on, delay for 3 seconds, then turn it off.

     

    You will have to decide what you mean by "if the switch is not pressed" because of course the majority of the time it won't be pressed, so how often do you want to light the green LED when it detects the button not pressed. 

     

    The link has code that shows you how to detect if a button is pressed or not pressed and how to turn on and turn off an LED.  It also has pictures on how to wire up the button and LED - for your second LED do the same but with a different digital port, e.g. 4.  You don't need to use more than one breadboard if you don't want to as long as you make sure your wiring is correct.

    • Cancel
    • Up +3 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
No Data