Arduino Day 2020: NanoRama Giveaway
Quiz | NanoRama Giveaway | NanoRama Contest | Fighting Germs Contest | Arduino Tutorials | Arduino Projects | Arduino Homepage
In the comments below: Let Us Know What Arduino Project You Are Planning on Doing for Arduino Day 2020!
We'll be sending out a limited number of Nano boards for project proposals that use them!
This year, Arduino Day will be on March 21, 2020. It will be their 15th birthday and we've decided to celebrate with NanoRama party! We're kicking things off with Nano Giveaway, where we'll make Arduino Nano's new family of boards available on the community for the first time. Say happy birthday to Arduino in the comments below, and let us know what Arduino project you plan on doing for Arduino's birthday. If your project idea includes one of the five Arduino Nano boards listed below, we'll send a the board of your choice for projects that use them. The Nano boards that we are giving away are the Arduino Nano (Classic), Nano Every, Nano 33 IoT, Nano 33 BLE, and Nano BLE Sense.
Beginning on the 21st of March, submit your Arduino Day project in Arduino Projects, Arduino , your blog, or the NanoRama Birthday Special on Project14 using the tag NanoRamaCH. Your project can be a birthday present to celebrate Arduino's 15th birthday, Project14's 3rd birthday, or both! The Arduino Nano family is featured throughout Arduino Day and the upcoming NanoRama competition, however, you're also free to submit any Arduino based project, not just a Nano based project, if you'd prefer. The first 20 people to submit an Arduino project for Arduino Day win an Arduino Nano! We'll also include cool Nano boards along with shopping cart as part of the prizes! The upcoming NanoRama competition closes on May 14th with a winners announcement on May 25th.
Key Dates:
Event | Date |
---|---|
NanoRama (3rd Anniversary of Project14) Launches: | 20th March 2020 |
Arduino Day 2020 (15th Anniversary of Arduino): | 21nd March 2020 |
Nano Winners Announced: | 23rd March 2020 |
NanoRama Closes: | 14th May 2020 |
NanoRama Winners Announced (42nd Anniversary of Star Wars): | 25th May 2020 |
We are giving away 25 Arduino Nano boards (5 of each) for Arduino Projects that Use them!
Here are the Nano boards to choose from:
| ![]() | ![]() |
Nano (Classic) - Giving away 5 for Project Proposals that use them! | Nano Every - Giving away 5 for Project Proposals that use them! | Nano 33 IoT - Giving away 5 for Project Proposals that use them! |
Buy NowBuy Now | ||
The Arduino Nano is a small, complete, and breadboard-friendly board based on the ATmega328P (Arduino Nano 3.x). It has more or less the same functionality of the Arduino Duemilanove, but in a different package. It lacks only a DC power jack, and works with a Mini-B USB cable instead of a standard one. | Perfect for everyday projects, this board is Arduino's 5 V Board in the smallest form factor available: 45x18mm!
The Arduino Nano Every is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the ATMega4809. This will allow you making larger programs than with the Arduino Uno (it has 50% more program memory), and with a lot more variables (the RAM is 200% bigger). | On-board WiFi and Bluetooth
Secure communication is ensured through the Microchip |
Microcontroller: ATMEGA328 Operating Voltage: 5V Analog Inputs: 8 Memory: 32 KB FLASH, 2KB SRAM | Microcontroller: ATMEGA4809 Operating Voltage: 5V Analog Inputs: 8 Memory: 48 KB FLASH, 6KB SRAM | Connectivity: WiFi, Bluetooth Microcontroller: ATSAMD21G18 Operating Voltage: 3.3V Input Voltage: 5V Memory: 256 KB Flash, 32 KB SRAM |
Starting March 21st:
We'll Also Be Giving Away 20 Arduino Nano Boards for the first 20 people to submit Arduino Projects for Arduino Day!
You can use whatever board you like but you'll need to tag your project blog NanoRamaCH!
In the comments below: Let Us Know What Arduino Project You Are Planning on Doing for Arduino Day!
Top Comments
Originally, we were going to post winners of the Nano board giveaway the day before Arduino Day. However, due to the lock down in Chicago caused by the Covid-19 virus threat, the team has been working…
Nanorama! I like it. I was only just saying a few minutes ago that Arduino Day has somehow passed me by in previous years, so this year I must do something. My idea, which I was thinking about only yesterday…
I have a project for work that could use the Arduino Nano 33 IoT.
Here is the potential project: The Shield of Compliance