Documents Arduino Accessories Wishlist and Giveaway
  • Blog
  • Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Arduino requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: dychen
  • Date Created: 28 Apr 2022 3:45 PM Date Created
  • Last Updated Last Updated: 2 May 2022 2:03 PM
  • Views 54604 views
  • Likes 9 likes
  • Comments 38 comments
Related
Recommended

Arduino Accessories Wishlist and Giveaway

Arduinos are some of the most popular microcontrollers around. With the availability of different kinds of Shields (circuit boards that plug into the Arduino to give it more functionality), an Arduino can be made to do pretty much anything. In this wishlist, we cover some of accessories you need to get started with Arduino, and some of the ones we think are just plain cool!

Arduino Wishlist Giveaway

5 winners will win an Arduino UNO R3. In order to win, answer these questions in the comments section below:

- What are some of the coolest things you've built with Arduino? Bonus points for pics!

- Tell us what we missed!  What are some of the things you'd recommend for working with Arduino?

Terms:

Post your answers as a comment below between May 2, 2022 and June 13, 2022.
Our favorite answers will be chosen by the element14 community team, and you will be shipped your prize (or local equivalent) free of charge.

Arduino UNO R3

There are several models of Arduino in different sizes and functionality, including the Portenta and Nano models, which feature modern connectivity options.  In this wishlist, however, we're taking a look at R3 compatible accessories. R3 is the 3rd revision of the Arduino UNO, which added a few new pins along with various other changes.

Arduino UNO

Buy Now

 

Accessories

LEDs are useful for any Arduino projects, whether they're used for testing or part of the final design.

Bi-color LED

Buy Now

 

A breadboard eliminates the need for soldering, making it easy to wire things up.

Breadboard

Buy Now

 

A small breadboard comes in handy for projects that require portability, such has portable devices or wearables.

Small breadboard

Buy Now

 

With Arduinos, the fun starts when you start stacking shields. This stackable header kit gives you more space for stacking.

Stacking Headers

Buy Now

Shields and Modules

PowerBoost 1000

This battery add-on provides power for portable projects and works not only for Arduino, but also SBCs like Raspberry Pi and Beaglebone. It can even keep the project running while recharging.

Powerboost shield

 Buy Now

 

Wi-Fi Bundle

This bundle includes a Wi-Fi shield so you can connect your project to the Internet, as well as capacitive touch slider display, accelerometer, and flexible powering options.

WiFi shield bundle

 Buy Now

 

Ethernet Shield

Connect your Arduino application to the Internet with an Ethernet Shield.

Ethernet Shield

Buy Now

 

Ethernet and PoE Shield

A shield providing Power over Ethernet (PoE) is also available.

Ethernet Shield with PoE

Buy Now

 

GPS/GPRS/GSM Shield

This credit card-sized shield gives an Arduino cellular capabilities, including SMS and telephone functions, as well as GPS.

GPS GSM Shield

 Buy Now

 

IoT Module

An IoT module lets Arduino developers quickly build IoT applications and connect to the cloud without the steep learning curve.

IoT Module

Buy Now

 

NFC/RFID Shield

Add NFC (nearfield communication) and RFID capabilities to your Arduino project with this shield from adafruit.

NFC RFID Shield

 Buy Now

 

Secure IoT Shield

With so many modern devices making wireless connections and passing data back and forth, security becomes an important consideration. This  shield provides a plug and play solution for secure connectivity with proven hardware-based security algorithms.

Secure IoT Shield

Buy Now

TFT Touch Shield

Touch screens are ubiquitous interfaces for modern portable devices. Add a 2.8" full color touch screen to your Arduino project with a Touch Shield.

TFT Touch Shield

 Buy Now

 

LCD Shield

LCD screens are great for simple texting, such as outputting text messages and simple animations.

LCD Shield

Buy Now

 

3D Tracking and Gesture Sensor

This gesture sensor detects everything from taps and swipes to drawing in the air, creating new possibilities for different things you can do.

Tracking and Gesture Sensor

Buy Now

 

Voice Recorder Module

This Voice Recorder Module gives an Arduino record capability. It supports 40 minutes of voice recording and can even work without a controller; just use the on-board record and play buttons.

Voice Recorder Module

 Buy Now

9 Axes Motion Shield

Applications involving health and fitness, as well as automotive or industrial, require motion analysis. A motion shield provides an accelerometer, gyroscope, and magnetometer, covering pretty much every movement.

9 Axes Motion Shield

Buy Now

 

Ultrasonic Ranging Sensor 

This sensor uses ultrasonic waves to determine how far away an object is (up to 4 meters).

Ultrasonic Sensor

Buy Now

 

Wurth Sensor Shield

This shield offers plug and play compatibility with Wurth's sensor EVAL boards, as well as any sensor with an I2C or SPI interface.

Sensor Shield

Buy Now

 

Weather Shield

With its integrated pressure, humidity, and temperature sensors, this shield gives Arduino weather and environmental detection capabilities.

Weather Shield

Buy Now

Arduino Sensor Kit

This sensor kit from Arduino includes a base board and a variety of sensors (light, sound, air pressure, temperature, and accelerometer). It also includes an OLED screen, as well as guided lessons introducing users to Arduino development. For someone just getting started with Arduino, this kit contains all the basics.  Just add an UNO and jump in!

Sensor Kit

Buy Now

 

Motor Control Shield

A motor control shield enables Arduino to control motors. This shield lets you drive two DC motors, controlling the speed and direction of each one independently, with each channel supplying 2A.

Motor Shield

Buy Now

If you need larger motors, this shield lets you control one bi-directional DC motor or two uni-direction DC motors at a typical nominal current of 7A.

Motor Shield

Buy Now

 

I/O Shield For Arduino

This versatile board adds 6 analog I/Os, 6 digital I/Os, and 6 relay outputs to Arduino.

IO Shield

Buy Now

 

ChronoDot Real Time Clock (RTC) Module

This highly accurate clock module drifts less than a minute a year, and works great for time critical projects that can't be synchronized to an external clock.

Clock Shield

Buy Now

  • shield
  • accessories
  • arduino
  • wish list
  • Share
  • History
  • More
  • Cancel
Anonymous

Top Comments

  • Workshopshed
    Workshopshed 2 months ago +3

    I've built a few different things with Arduino tech.

    A binary USB keyboard

    Binary Keyboard 

    A Topsy Turvy Clock
    Clock 

    A Knife Switch (with a remote control switch designed for a Pi)

      

    A Jumbo Servo

      

    My ideal accessory would…

  • colporteur
    colporteur 3 months ago +2

    That is a pretty comprehensive list of items to support an Arduino.

    I find a MOSFET module to interface the low voltage of the Arduino to a higher voltage a very useful kit.

    My Arduino project was to…

  • rsc
    rsc 3 months ago +2

    Screw terminals are useful sometimes.

    https://vetco.net/products/screw-terminal-shield-for-arduino-d30

Parents
  • colporteur
    colporteur 3 months ago

    That is a pretty comprehensive list of items to support an Arduino.

    I find a MOSFET module to interface the low voltage of the Arduino to a higher voltage a very useful kit.

    My Arduino project was to create light and sound animation for a model railroad layout. The two cars (red ellipse) passing at an intersection, flash their headlights and honk their horns when a button on the display is pressed. I combined an Arduino Nano, DFPlayer Module and MOSFET on a PCB to create the light and sound PCB. The PCB is located in a building on the layout (green ellipse).

    I have used the PCB numerous times when I have needed sound and light.

    • Cancel
    • Vote Up +2 Vote Down
    • Reply
    • More
    • Cancel
Comment
  • colporteur
    colporteur 3 months ago

    That is a pretty comprehensive list of items to support an Arduino.

    I find a MOSFET module to interface the low voltage of the Arduino to a higher voltage a very useful kit.

    My Arduino project was to create light and sound animation for a model railroad layout. The two cars (red ellipse) passing at an intersection, flash their headlights and honk their horns when a button on the display is pressed. I combined an Arduino Nano, DFPlayer Module and MOSFET on a PCB to create the light and sound PCB. The PCB is located in a building on the layout (green ellipse).

    I have used the PCB numerous times when I have needed sound and light.

    • Cancel
    • Vote Up +2 Vote Down
    • Reply
    • More
    • Cancel
Children
No Data