Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
AUBoard 15P Avnet AU board-15P(AES-AUB-15P-DK-G, Rev 01) - FMC connector issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 261 subscribers
  • Views 322 views
  • Users 0 members are here
  • fmc
  • AU15board
  • AES-AUB-15P-DK-G
Related

Avnet AU board-15P(AES-AUB-15P-DK-G, Rev 01) - FMC connector issue

Mitilesh
Mitilesh 6 months ago

I am interfacing Avnet AU board-15P(AES-AUB-15P-DK-G,  Rev 01)  with LVDS transmitter on it, to communicate with a external LVDS receiver through FMC connector. I observed that some pins of the FMC connector are mapped to HPIO capable signals and others are mapped to HDIO capable signals.

From the datasheet of Artix-Ultrascale+ FPGA, it is understood that HDIO signals maximum supported data rate is 250Mbps whereas HPIO capable pins support 2.5Gbps.

However, Assigning HDIO signals with lower data rate to FMC connector doesn't seem to be aligned with the FMC standard. 

The basic requirement for our design is to have a interface that support LVDS  transmission with data rate of at least 625Mbps.
I can see a warning in vivado- v 2024.2 tool mentioning illegal placement on those pins. Even though this is a warning, I could see signal integrity issue in the output.

Some of the HDIO signals that are mapped to FMC are following pairs:
 (H14, G14) 
 (J14, J15) 
 (J12, H12)
 (E13, E12)

Attaching the warnings for reference:

 image

Is there any way to have work around for this issue?

  • Sign in to reply
  • Cancel
Parents
  • iksevas
    0 iksevas 5 months ago

    Based on the table below, it looks like that is a limitation if you need to use the HD_DP pins for the data lanes. The issue above seems to be that you are using OSERDESE3 which isn't compatible with HDIO. 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • iksevas
    0 iksevas 5 months ago

    Based on the table below, it looks like that is a limitation if you need to use the HD_DP pins for the data lanes. The issue above seems to be that you are using OSERDESE3 which isn't compatible with HDIO.