Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
AUBoard 15P Controlling AUBoard-15P form Matlab using the JTAG to AXI interface
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 261 subscribers
  • Views 226 views
  • Users 0 members are here
  • AUBoard-15P
Related

Controlling AUBoard-15P form Matlab using the JTAG to AXI interface

Umallik
Umallik 2 months ago

My project requires control of an AUBoard-15 from Matlab (using the Matlab generated JTAG to AXI block). To that end I am required to create a Board definition file using the interface provided in Matlab. Can someone help me with the entries requested below. I do not have access to the schematics. I am not sure how to go about coming up with answers to these questions. 

image

  • Sign in to reply
  • Cancel

Top Replies

  • iksevas
    iksevas 2 months ago in reply to iksevas +1
    Take this for what it is worth from AI:
Parents
  • iksevas
    0 iksevas 2 months ago

    There are only two options for JTAG on the AUBoard - the FPGA and the FMC connector. If you are not using the FMC connector, then the FPGA is the only device in the chain. As far as IR length of the FPGA, you more than likely need to dig into some datasheets for the Artix UltraScale+ and if you are using an FMC card, you will need to determine what devices on that card are in the JTAG chain and similarly find their IR length.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • iksevas
    0 iksevas 2 months ago

    There are only two options for JTAG on the AUBoard - the FPGA and the FMC connector. If you are not using the FMC connector, then the FPGA is the only device in the chain. As far as IR length of the FPGA, you more than likely need to dig into some datasheets for the Artix UltraScale+ and if you are using an FMC card, you will need to determine what devices on that card are in the JTAG chain and similarly find their IR length.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • iksevas
    0 iksevas 2 months ago in reply to iksevas

    Take this for what it is worth from AI:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Umallik
    0 Umallik 2 months ago in reply to iksevas

    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer