Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General What linux core minimal image is required for AVNET MicroZed board?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 360 subscribers
  • Views 697 views
  • Users 0 members are here
  • Using Xilinx Tools
  • ZedBoard General Questions
  • Software Application Development
  • Zedboard Training
Related

What linux core minimal image is required for AVNET MicroZed board?

dexterous.me82
dexterous.me82 over 6 years ago

I have an AVNET microzed board  PB-AES-Z7MB-7Z010-G board.

After building the operating system - Linux for this device - I get the following error in my console.

 

 

    U-Boot SPL 2019.01 (Dec 04 2019 - 05:18:17 +0000)

    mmc boot

    Trying to boot from MMC1

    spl_load_image_fat_os: error reading image system.dtb, err - -2

    spl_load_image_fat: error reading image u-boot.img, err - -2

    SPL: failed to boot from all boot devices

    ### ERROR ### Please RESET the board ###

    U-Boot SPL 2019.01 (Dec 04 2019 - 05:18:17 +0000)

    mmc boot

    Trying to boot from MMC1

 

 

 

 

 

Here is how I have build the Operating System.

 

 

Yocto Source code and meta recipes

 

 

    git clone git://git.yoctoproject.org/poky

    cd poky

    git checkout -b warrior

    git clone  git://git.yoctoproject.org/meta-xilinx

    cd meta-xilinx/

    git checkout -b warrior

    cd ..

    git clone https://github.com/openembedded/meta-openembedded.git

    cd meta-openembedded/

    git checkout -b warrior

    cd ..

   

   

    source oe-init-build-env

   

   

   

    ## Changed the architecture to --

    gedit conf/local.conf

    MACHINE ??= "microzed-zynq7"

   

    Added the meta-layer in the bblayer

   

    /home/s/Yocto_Xilinx/poky/meta-xilinx/meta-xilinx-bsp

    /home/s/Yocto_Xilinx/poky/meta-openembedded/meta-oe \

 

 

Final build command was

#

 

 

    bitbake core-image-minimal

 

 

    ls -l tmp/deploy/images/microzed-zynq7/

    total 22992

    lrwxrwxrwx 2 s s      34 Dec  3 21:25 boot.bin -> boot.bin-microzed-zynq7-2019.01-r0

    lrwxrwxrwx 2 s s      34 Dec  3 21:25 boot.bin-microzed-zynq7 -> boot.bin-microzed-zynq7-2019.01-r0

    -rw-r--r-- 2 s s   84104 Dec  3 21:25 boot.bin-microzed-zynq7-2019.01-r0

    -rw-r--r-- 2 s s 4074496 Dec  3 21:26 core-image-minimal-microzed-zynq7-20191204041353.rootfs.cpio

    -rw-r--r-- 2 s s 2379781 Dec  3 21:26 core-image-minimal-microzed-zynq7-20191204041353.rootfs.cpio.gz.u-boot

    -rw-r--r-- 2 s s     814 Dec  3 21:26 core-image-minimal-microzed-zynq7-20191204041353.rootfs.manifest

    -rw-r--r-- 2 s s 2384005 Dec  3 21:26 core-image-minimal-microzed-zynq7-20191204041353.rootfs.tar.gz

    -rw-r--r-- 2 s s  226135 Dec  3 21:26 core-image-minimal-microzed-zynq7-20191204041353.testdata.json

    lrwxrwxrwx 2 s s      60 Dec  3 21:26 core-image-minimal-microzed-zynq7.cpio -> core-image-minimal-microzed-zynq7-20191204041353.rootfs.cpio

    lrwxrwxrwx 2 s s      70 Dec  3 21:26 core-image-minimal-microzed-zynq7.cpio.gz.u-boot -> core-image-minimal-microzed-zynq7-20191204041353.rootfs.cpio.gz.u-boot

    lrwxrwxrwx 2 s s      64 Dec  3 21:26 core-image-minimal-microzed-zynq7.manifest -> core-image-minimal-microzed-zynq7-20191204041353.rootfs.manifest

    lrwxrwxrwx 2 s s      62 Dec  3 21:26 core-image-minimal-microzed-zynq7.tar.gz -> core-image-minimal-microzed-zynq7-20191204041353.rootfs.tar.gz

    lrwxrwxrwx 2 s s      62 Dec  3 21:26 core-image-minimal-microzed-zynq7.testdata.json -> core-image-minimal-microzed-zynq7-20191204041353.testdata.json

    -rw-r--r-- 2 s s  184951 Dec  3 21:19 modules--4.19-xilinx-v2019.1+git0+9811303824-r0-microzed-zynq7-20191204041353.tgz

    lrwxrwxrwx 2 s s      81 Dec  3 21:19 modules-microzed-zynq7.tgz -> modules--4.19-xilinx-v2019.1+git0+9811303824-r0-microzed-zynq7-20191204041353.tgz

    lrwxrwxrwx 2 s s      36 Dec  3 21:25 u-boot.elf -> u-boot-microzed-zynq7-2019.01-r0.elf

    lrwxrwxrwx 2 s s      36 Dec  3 21:25 u-boot.img -> u-boot-microzed-zynq7-2019.01-r0.img

    -rw-r--r-- 2 s s 5298060 Dec  3 21:25 u-boot-microzed-zynq7-2019.01-r0.elf

    -rw-r--r-- 2 s s  548898 Dec  3 21:25 u-boot-microzed-zynq7-2019.01-r0.img

    lrwxrwxrwx 2 s s      36 Dec  3 21:25 u-boot-microzed-zynq7.elf -> u-boot-microzed-zynq7-2019.01-r0.elf

    lrwxrwxrwx 2 s s      36 Dec  3 21:25 u-boot-microzed-zynq7.img -> u-boot-microzed-zynq7-2019.01-r0.img

    -rw-r--r-- 2 s s     709 Dec  3 21:25 uEnv.txt

    lrwxrwxrwx 2 s s      80 Dec  3 21:19 uImage -> uImage--4.19-xilinx-v2019.1+git0+9811303824-r0-microzed-zynq7-20191204041353.bin

    -rw-r--r-- 2 s s 4162648 Dec  3 21:19 uImage--4.19-xilinx-v2019.1+git0+9811303824-r0-microzed-zynq7-20191204041353.bin

    lrwxrwxrwx 2 s s      80 Dec  3 21:19 uImage-microzed-zynq7.bin -> uImage--4.19-xilinx-v2019.1+git0+9811303824-r0-microzed-zynq7-20191204041353.bin

    lrwxrwxrwx 2 s s      80 Dec  3 21:19 zImage -> zImage--4.19-xilinx-v2019.1+git0+9811303824-r0-microzed-zynq7-20191204041353.bin

    -rw-r--r-- 2 s s 4162584 Dec  3 21:19 zImage--4.19-xilinx-v2019.1+git0+9811303824-r0-microzed-zynq7-20191204041353.bin

    lrwxrwxrwx 2 s s      80 Dec  3 21:19 zImage-microzed-zynq7.bin -> zImage--4.19-xilinx-v2019.1+git0+9811303824-r0-microzed-zynq7-20191204041353.bin

    -rw-r--r-- 2 s s    9402 Dec  3 21:19 zynq-microzed--4.19-xilinx-v2019.1+git0+9811303824-r0-microzed-zynq7-20191204041353.dtb

    lrwxrwxrwx 2 s s      87 Dec  3 21:19 zynq-microzed.dtb -> zynq-microzed--4.19-xilinx-v2019.1+git0+9811303824-r0-microzed-zynq7-20191204041353.dtb

    lrwxrwxrwx 2 s s      87 Dec  3 21:19 zynq-microzed-microzed-zynq7.dtb -> zynq-microzed--4.19-xilinx-v2019.1+git0+9811303824-r0-microzed-zynq7-20191204041353.dtb

 

 

In my SD card, I have put the following image -

 

 

    boot.bin

    system.dtb (zynq-microzed.dtb)

    u-boot.elf

    u-boot.img

    zImage  --> not sure what is it going to pickup

    uImage  --> so uImage again.

 

 

However, after booting/resetting the board I get the error as shown in the top of this post.

  • Sign in to reply
  • Cancel

Top Replies

  • nl-robotics
    nl-robotics over 5 years ago +2
    Hi, I hope you have found the solution by now, I had the same, so just for future reference, here is how I solved it: In default, when building the core-image-minimal, u-boot searches for a second partition…
Parents
  • clem57
    clem57 over 6 years ago

    Have you checked the forums? https://forums.xilinx.com/t5/Processor-System-Design/bootloader-works-from-SD-card-not-from-QSPI-flash/td-p/723125

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 6 years ago

    Have you checked the forums? https://forums.xilinx.com/t5/Processor-System-Design/bootloader-works-from-SD-card-not-from-QSPI-flash/td-p/723125