I am trying to use xilinix JTAG to load uboot.elf on to the RAM.
However, I need the tcl file to preset the processor settings.
source "tcl file" so that it can load my uboot.elf.
I am trying to use xilinix JTAG to load uboot.elf on to the RAM.
However, I need the tcl file to preset the processor settings.
source "tcl file" so that it can load my uboot.elf.
What you need is the Zynq First Stage Boot Loader (FSBL) elf file. This, along with the u-boot elf file and PL bitstream (if you have one), can be used to boot via JTAG or can be packaged into a boot.bin file for booting via SD card, etc. A good place to start with learning the flow of booting u-boot and Linux is one of Avnet's posted PetaLinux BSPs for the MicroZed SOMs. Xilinx User Guide 1144 is an excellent resource developing with PetaLinux.
--Tom
What you need is the Zynq First Stage Boot Loader (FSBL) elf file. This, along with the u-boot elf file and PL bitstream (if you have one), can be used to boot via JTAG or can be packaged into a boot.bin file for booting via SD card, etc. A good place to start with learning the flow of booting u-boot and Linux is one of Avnet's posted PetaLinux BSPs for the MicroZed SOMs. Xilinx User Guide 1144 is an excellent resource developing with PetaLinux.
--Tom
I did that but I can't see anything on the console.
Serial console is blank when I write fsbl.elf to RAM using JTAG?
I have generated fsbl.elf using Symbols - FSBL_DEBUG_INFO.
I do see that if I create a boot gen image using this FSBL.elf and place in SD card.
And then if I change the jumper to SD card mode, I see FSBL prints on the console.
However, I don't see prints coming on to the serial port if I do load the
fsbl.elf using JTAG and JTAG mode.
xsct% targets 2
xsct% source ps7_init.tcl
Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0xffffff28 (Suspended)
Info: ARM Cortex-A9 MPCore #1 (target 3) Stopped at 0xffffff34 (Suspended)
Downloading Program -- C:/Users/abc/Downloads/JTAG_microzed_zynq7010/fsbl.elf
section, .text: 0x00000000 - 0x0000fedb
section, .handoff: 0x0000fedc - 0x0000ff27
section, .init: 0x0000ff28 - 0x0000ff3f
section, .fini: 0x0000ff40 - 0x0000ff57
section, .rodata: 0x0000ff58 - 0x000112d3
section, .data: 0x000112d8 - 0x00014047
section, .eh_frame: 0x00014048 - 0x0001404b
section, .mmu_tbl: 0x00018000 - 0x0001bfff
section, .init_array: 0x0001c000 - 0x0001c003
section, .fini_array: 0x0001c004 - 0x0001c007
section, .rsa_ac: 0x0001c008 - 0x0001d03f
section, .bss: 0x0001d040 - 0x0001ee71
section, .heap: 0x0001ee72 - 0x00020e7f
section, .stack: 0xffff0000 - 0xffffd3ff
100% 0MB 0.1MB/s 00:01
Setting PC to Program Start Address 0x00000000
Successfully downloaded C:/Users/abc/Downloads/JTAG_microzed_zynq7010/fsbl.elf
Infact, I wrote a simple hello world program. However, this hello world isn't
appearing on the console.