Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
General SD card boot fail: XFSBL_ERROR_SD_F_OPEN
  • Forums
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Avnet Boards Forums requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 48 subscribers
  • Views 970 views
  • Users 0 members are here
  • zedboardcmty
Related

SD card boot fail: XFSBL_ERROR_SD_F_OPEN

dugurlu
dugurlu over 2 years ago

Hello,

We're currently testing a custom board. the SD card boot fails with the following log:

Xilinx Zynq MP First Stage Boot Loader

Release 2018.3   Jun  5 2020  -  16:31:27

Reset Mode      :       System Reset

Platform: Silicon (4.0), Cluster ID 0x80000000

Running on A53-0 (64-bit) Processor, Device Name: XCZU7EV

Processor Initialization Done

================= In Stage 2 ============

SD1 Boot Mode

SD: rc= 0

File name is 1:/BOOT.BIN

SD: Unable to open file 1:/BOOT.BIN: 3

                                      XFSBL_ERROR_SD_F_OPEN

Boot Device Initialization failed 0x29

================= In Stage Err ============

Fsbl Error Status: 0x0

 

Our image can boot on carrier board. We compare power-up sequence of the two board. No improvement.

We tried to slow down the clock  from 200MHz to 100MHz. No improvement.

 

Do you have another idea that we could try?

  • Reply
  • Cancel
  • Cancel
Parents
  • narrucmot
    narrucmot over 2 years ago

    A query of the Xilinx forums could be helpful here:

    https://forums.xilinx.com/t5/Xilinx-Evaluation-Boards/zcu102-SD-card-boot-fail-XFSBL-ERROR-SD-F-OPEN/td-p/751573

    https://forums.xilinx.com/t5/ACAP-and-SoC-Boot-and/SD-card-boot-fail-XFSBL-ERROR-SD-F-OPEN/td-p/1062487

     

    Are you using a level shifter on your carrier between the XCZU7EV device and the SD card?  How is the SD clock terminated?

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Cancel
  • dugurlu
    dugurlu over 2 years ago in reply to narrucmot

    We didn't use level shifter between the XCZU7EV device and the SD card. Our design is no different from the carrier board like below.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Cancel
  • narrucmot
    narrucmot over 2 years ago in reply to dugurlu

    How is the SD card boot interface configured?  SD 2.0 or 3.0?  A configuration of SD 2.0 (4-bit) is known to work for the Avnet UltraZed-EV SOM + EV Carrier.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Cancel
  • dugurlu
    dugurlu over 2 years ago in reply to narrucmot

    Thanks your reply. Our configuration is below.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Cancel
Reply
  • dugurlu
    dugurlu over 2 years ago in reply to narrucmot

    Thanks your reply. Our configuration is below.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Cancel
Children
  • narrucmot
    narrucmot over 2 years ago in reply to dugurlu

    I notice your SD1 interface does not enable the WP pin on MIO44.  I believe this is required for the FSBL to boot.  Please consider making this change and rebuild, make a new boot.bin, etc.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Cancel
  • dugurlu
    dugurlu over 2 years ago in reply to narrucmot

    I have tested with wp enable boot image. Still we couldn't boot from sd card.

    • Cancel
    • Vote Up 0 Vote Down
    • Reply