Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General DC Generator
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 363 subscribers
  • Views 1587 views
  • Users 0 members are here
Related

DC Generator

powerking
powerking over 5 years ago

Hi, I would like everyone's option, on making a generator from a PMDC motor

The primary and only task would be to charge a motorcycle size 12v battery. If I used a PMDC motor would I be able to fit a rectifier / regulator to convert the charge to dc and stop the battery overcharging, would this work?

Or is it more complex than this, (and no I can't use a alternator as it will not fit).

Cheers Wayne

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago +4
    Hi Wayne, The only need for a rectifier would be to block the battery power from causing the motor being used as a generator to draw current and run. Once you have the DCPM motor spinning fast enough to…
  • dougw
    dougw over 5 years ago +3
    The short answer is a DC motor can be used as a generator. You will need to figure out what happens at all speeds. It might be useful to look at small wind turbine generators. Alternators are also available…
  • powerking
    powerking over 5 years ago +2
    Thanks for the replies, yes sorry I failed to explain clearly what I'm trying to achieve. I am also a novice in this field(so please be patience with me) My plan is to do a long trip on a 1920's motorcycle…
Parents
  • powerking
    powerking over 5 years ago

    Thanks for the replies, yes sorry I failed to explain clearly what I'm trying to achieve. I am also a novice in this field(so please be patience with me)

    My plan is to do a long trip on a 1920's motorcycle, and I would like to have reliable lights should for some unlikely situation ever need them. Also I would like to be able to recharge my phone by installing a power outlet on the bike.

    The motorcycle does not require the battery to run as it is magneto ignition, the battery would be only for lights and the power outlet

    the original 6v generator(which I do not have) is 84mm diameter and about180mm long. I would like what ever I use to look similar, but be a 12v system

    I not sure  what current I need to generate or size of motor,

    As you could imagine motor speed would vary and it would be driven off the motorcycle engine(1000cc) by belt

    Please let me know if you require any further info or is there a better way, or is it just a bad idea

    Cheers Wayne and thanks for your help

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • powerking
    powerking over 5 years ago

    Thanks for the replies, yes sorry I failed to explain clearly what I'm trying to achieve. I am also a novice in this field(so please be patience with me)

    My plan is to do a long trip on a 1920's motorcycle, and I would like to have reliable lights should for some unlikely situation ever need them. Also I would like to be able to recharge my phone by installing a power outlet on the bike.

    The motorcycle does not require the battery to run as it is magneto ignition, the battery would be only for lights and the power outlet

    the original 6v generator(which I do not have) is 84mm diameter and about180mm long. I would like what ever I use to look similar, but be a 12v system

    I not sure  what current I need to generate or size of motor,

    As you could imagine motor speed would vary and it would be driven off the motorcycle engine(1000cc) by belt

    Please let me know if you require any further info or is there a better way, or is it just a bad idea

    Cheers Wayne and thanks for your help

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jw0752
    jw0752 over 5 years ago in reply to powerking

    Hi Wayne,

     

    With this much potential power it would be advisable to have a regulator circuit to control the voltage that is applied to the battery. You may be able to find something that is designed for use on a commercial motorcycle electrical system.

     

    John