Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General DC Generator
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 363 subscribers
  • Views 1592 views
  • Users 0 members are here
Related

DC Generator

powerking
powerking over 5 years ago

Hi, I would like everyone's option, on making a generator from a PMDC motor

The primary and only task would be to charge a motorcycle size 12v battery. If I used a PMDC motor would I be able to fit a rectifier / regulator to convert the charge to dc and stop the battery overcharging, would this work?

Or is it more complex than this, (and no I can't use a alternator as it will not fit).

Cheers Wayne

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago +4
    Hi Wayne, The only need for a rectifier would be to block the battery power from causing the motor being used as a generator to draw current and run. Once you have the DCPM motor spinning fast enough to…
  • dougw
    dougw over 5 years ago +3
    The short answer is a DC motor can be used as a generator. You will need to figure out what happens at all speeds. It might be useful to look at small wind turbine generators. Alternators are also available…
  • powerking
    powerking over 5 years ago +2
    Thanks for the replies, yes sorry I failed to explain clearly what I'm trying to achieve. I am also a novice in this field(so please be patience with me) My plan is to do a long trip on a 1920's motorcycle…
Parents
  • m6247015
    m6247015 over 3 years ago

    A direct current (DC) meta tags analyzer generator works on the principle that a voltage is induced in a conductor coil when it is rotated in a magnetic field. The rate at which the coil rotates in the magnetic field determines the amount of voltage induced in the coil.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • m6247015
    m6247015 over 3 years ago

    A direct current (DC) meta tags analyzer generator works on the principle that a voltage is induced in a conductor coil when it is rotated in a magnetic field. The rate at which the coil rotates in the magnetic field determines the amount of voltage induced in the coil.