Hi,
I could not boot from QSPI in MMP 7Z100.
I just follow the Lab "zynq_mmp_embedded_design_7z100_v2015_2" to use the make_mcs_file.bat to generate my mcs file. MCS file is generate OK. and also, SDK Program Flash finished without any error. but could not boot from QSPI flash. But I use the Lab pre-build "zynq_mmp_peripheral_test.mcs" and the same SDK program FPGA procedure, the FPGA is boot correctly, is anything wrong from my generate the MCS file? How to generate the correct MCS file?
Jansen Lee