Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Minized - Restore Factory Status not Working
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Subscribers 358 subscribers
  • Views 2257 views
  • Users 0 members are here
Related

Minized - Restore Factory Status not Working

Former Member
Former Member over 8 years ago

Hello,

 

I uploaded a broken Linux to eMMC and now I need to get a Minized back to factory settings, but I´m having a hard time. 

I´m using Vivado 2017.3 and Restore QSPI and EMMC Factory Images -http://zedboard.org/content/restore-qspi-and-emmc-factory-images.


Unlikely the recover documentation, Vivado 2017.3 asks for and fsbl.elf in addition to the bin file.

So I managed to program flash_only_boot_7007S.bin and fsbl (generated from  Tutorial 04 FSBL and Boot from QSPI.)

It programmed the QSPI OK, but now all I get is an u-boot with the following:

U-Boot 2016.07 (Jul 27 2017 - 21:56:59 -0700)
DRAM:  ECC disabled 512 MiB
MMC:   sdhci@e0100000: 0, sdhci@e0101000: 1
SF: Detected N25Q128 with page size 256 Bytes, erase size 64 KiB, total 16 MiB
In:    serial
Out:   serial
Err:   serial
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc1(part 0) is current device
reading image.ub
25198592 bytes read in 2321 ms (10.4 MiB/s)
## Loading kernel from FIT Image at 10000000 ...
Bad FIT kernel image format!
ERROR: can't get kernel image!
Zynq>
 

Shouldn´t flash_only_boot_7007S boot entirely from QSPI? I think it is still loading my broken image.ub in the eMMC.
 
Any shed of light?
 
Regards,
  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    The tutorial you are refering to utilizes Vivado 2017.1. Please install Vivado 2017.1 + SDK and once again go through the instructions.

    That is most likely the cause of your issue.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 8 years ago in reply to jafoste4

    Hi Josh.

    In fact it says in page 3:  "Xilinx SDK 2017.1 or later from https://www.xilinx.com/support/download.html . The
    XSCT tool of this installation can be used to program the QSPI flash, U2.".

    But i'll download 2017.1 and try anyway.

    Thanks for the reply!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 8 years ago in reply to jafoste4

    Hi Josh.

    I re-flashed using 2017.1 and I still get the same error after rebooting:

     

    U-Boot 2016.07 (Jul 27 2017 - 21:56:59 -0700)

    DRAM:  ECC disabled 512 MiB
    MMC:   sdhci@e0100000: 0, sdhci@e0101000: 1
    SF: Detected N25Q128 with page size 256 Bytes, erase size 64 KiB, total 16 MiB
    In:    serial
    Out:   serial
    Err:   serial
    Hit any key to stop autoboot:  0
    switch to partitions #0, OK
    mmc1(part 0) is current device
    reading image.ub
    25198592 bytes read in 2320 ms (10.4 MiB/s)
    ## Loading kernel from FIT Image at 10000000 ...
    Bad FIT kernel image format!
    ERROR: can't get kernel image!
    Zynq>

    I found particulary strange the "mmc1(part 0) is current device" info, since it is suposed to be a QSPI boot only image, right?

    I even did a -erase_only in xsct to ensure that flash_only_boot_7007S.bin was really being flashed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • stefanrousseau
    0 stefanrousseau over 8 years ago

    On the tools versions:
    You are correct.  There is an issue with the document instructions and XSCT for 2017.3.  It does not work as it did for 2017.1 and 2017.2.  The document instructions may have to be updated.  It seems that 2017.3 expects the FSBL to be specified when programming.  And you may need the zynq_fsbl.elf file in your programming directory.  This file is in the /images/linux directory of the BSP-imported project  under Linux.  If you have that file (or one you created during the tutorials), you can use
    exec program_flash -f flash_only_boot_7007S.bin -fsbl zynq_fsbl.elf -flash_type qspi_single

    One difference I have noticed (under 2017.1) between using the -fsbl syntax and not is that the blue DONE LED on minized almost immediately comes on again after using that syntax, while without it the LED remains off until you eventually reset the board.  I do not yet know why that is.

    Currently the latest MiniZed BSP is still 2017.2, so please note that it is not recommended to mix tools versions between Vivado/SDK and PetaLinux.  That being said, also note that the factory default flash_only_boot_7007S.bin file was created under 2016.4.

    In terms of your output from the boot process, it definitely does not look as if your flash programming was successful.  Did you wait for XSCT to report "Flash Operation Successful"?  It takes a while.  I paste my log from that boot process and it differs from yours in a number of places. 

    ********* Boot log after programming flash_only_boot_7007S.bin ***********************************

    U-Boot 2016.07 (Jul 27 2017 - 21:56:59 -0700)

    DRAM:  ECC disabled 512 MiB
    MMC:   sdhci@e0100000: 0, sdhci@e0101000: 1
    SF: Detected N25Q128 with page size 256 Bytes, erase size 64 KiB, total 16 MiB
    *** Warning - bad CRC, using default environment

    In:    serial
    Out:   serial
    Err:   serial
    U-BOOT for

    Hit any key to stop autoboot:  0
    SF: Detected N25Q128 with page size 256 Bytes, erase size 64 KiB, total 16 MiB
    device 0 offset 0x270000, size 0xd80000
    SF: 14155776 bytes @ 0x270000 Read: OK
    ## Loading kernel from FIT Image at 10000000 ...
       Using 'conf@1' configuration
       Verifying Hash Integrity ... OK
       Trying 'kernel@0' kernel subimage
         Description:  Linux Kernel
         Type:         Kernel Image
         Compression:  uncompressed
         Data Start:   0x100000d4
         Data Size:    4075120 Bytes = 3.9 MiB
         Architecture: ARM
         OS:           Linux
         Load Address: 0x00008000
         Entry Point:  0x00008000
         Hash algo:    sha1
         Hash value:   0ba8ef7520fcc3903d7d0b7d611e510db5515298
       Verifying Hash Integrity ... sha1+ OK
    ## Loading ramdisk from FIT Image at 10000000 ...
       Using 'conf@1' configuration
       Trying 'ramdisk@0' ramdisk subimage
         Description:  ramdisk
         Type:         RAMDisk Image
         Compression:  uncompressed
         Data Start:   0x103e72e8
         Data Size:    9973532 Bytes = 9.5 MiB
         Architecture: ARM
         OS:           Linux
         Load Address: unavailable
         Entry Point:  unavailable
         Hash algo:    sha1
         Hash value:   d18a7880ad0b55e0e329d28fac6624576448b03d
       Verifying Hash Integrity ... sha1+ OK
    ## Loading fdt from FIT Image at 10000000 ...
       Using 'conf@1' configuration
       Trying 'fdt@0' fdt subimage
         Description:  Flattened Device Tree blob
         Type:         Flat Device Tree
         Compression:  uncompressed
         Data Start:   0x103e3038
         Data Size:    16894 Bytes = 16.5 KiB
         Architecture: ARM
         Hash algo:    sha1
         Hash value:   d989058f04e066702a50da837782f2c5ed94e7b8
       Verifying Hash Integrity ... sha1+ OK
       Booting using the fdt blob at 0x103e3038
       Loading Kernel Image ... OK
       Loading Ramdisk to 0767d000, end 07ffff1c ... OK
       Loading Device Tree to 07675000, end 0767c1fd ... OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.
    Booting Linux on physical CPU 0x0
    Linux version 4.6.0-xilinx (training@localhost.localdomain) (gcc version 5.2.1 20151005 (Linaro GCC 5.2-2015.11-2) ) #1 SMP PREEMPT Thu Jul 27 22:24:51 PDT 2017
    CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
    CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    Machine model: minized
    bootconsole [earlycon0] enabled
    cma: Reserved 16 MiB at 0x1f000000
    Memory policy: Data cache writealloc
    percpu: Embedded 12 pages/cpu @debca000 s19776 r8192 d21184 u49152
    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
    Kernel command line: console=ttyPS0,115200 earlyprintk
    PID hash table entries: 2048 (order: 1, 8192 bytes)
    Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    Memory: 482712K/524288K available (6319K kernel code, 249K rwdata, 1916K rodata, 1024K init, 212K bss, 25192K reserved, 16384K cma-reserved, 0K highmem)
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
        vmalloc : 0xe0800000 - 0xff800000   ( 496 MB)
        lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
        modules : 0xbf000000 - 0xbfe00000   (  14 MB)
          .text : 0xc0008000 - 0xc090ae84   (9228 kB)
          .init : 0xc0a00000 - 0xc0b00000   (1024 kB)
          .data : 0xc0b00000 - 0xc0b3e7a0   ( 250 kB)
           .bss : 0xc0b3e7a0 - 0xc0b73a38   ( 213 kB)
    Preemptible hierarchical RCU implementation.
            Build-time adjustment of leaf fanout to 32.
            RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
    RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=2
    NR_IRQS:16 nr_irqs:16 16
    efuse mapped to e0800000
    slcr mapped to e0802000
    L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C-310 erratum 769419 enabled
    L2C-310 enabling early BRESP for Cortex-A9
    L2C-310 full line of zeros enabled for Cortex-A9
    L2C-310 ID prefetch enabled, offset 1 lines
    L2C-310 dynamic clock gating enabled, standby mode enabled
    L2C-310 cache controller enabled, 8 ways, 512 kB
    L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
    zynq_clock_init: clkc starts at e0802100
    Zynq clock init
    sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
    clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
    Switching to timer-based delay loop, resolution 3ns
    clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
    timer #0 at e080a000, irq=17
    Console: colour dummy device 80x30
    Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333)
    pid_max: default: 32768 minimum: 301
    Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    CPU: Testing write buffer coherency: ok
    CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    Setting up static identity map for 0x100000 - 0x100058
    CPU1: failed to boot: -1
    Brought up 1 CPUs
    SMP: Total of 1 processors activated (666.66 BogoMIPS).
    CPU: All CPU(s) started in SVC mode.
    devtmpfs: initialized
    VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    pinctrl core: initialized pinctrl subsystem
    NET: Registered protocol family 16
    DMA: preallocated 256 KiB pool for atomic coherent allocations
    cpuidle: using governor menu
    hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
    hw-breakpoint: maximum watchpoint size is 4 bytes.
    zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0xe0880000
    zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
    GPIO IRQ not connected
    XGpio: /amba_pl/gpio@41200000: registered, base is 905
    GPIO IRQ not connected
    XGpio: /amba_pl/gpio@41200000: dual channel registered, base is 904
    GPIO IRQ not connected
    XGpio: /amba_pl/gpio@41210000: registered, base is 903
    GPIO IRQ not connected
    XGpio: /amba_pl/gpio@41220000: registered, base is 895
    vgaarb: loaded
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    media: Linux media interface: v0.10
    Linux video capture interface: v2.00
    pps_core: LinuxPPS API ver. 1 registered
    pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    PTP clock support registered
    EDAC MC: Ver: 3.0.0
    Advanced Linux Sound Architecture Driver Initialized.
    Bluetooth: Core ver 2.21
    NET: Registered protocol family 31
    Bluetooth: HCI device and connection manager initialized
    Bluetooth: HCI socket layer initialized
    Bluetooth: L2CAP socket layer initialized
    Bluetooth: SCO socket layer initialized
    clocksource: Switched to clocksource arm_global_timer
    NET: Registered protocol family 2
    TCP established hash table entries: 4096 (order: 2, 16384 bytes)
    TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
    TCP: Hash tables configured (established 4096 bind 4096)
    UDP hash table entries: 256 (order: 1, 8192 bytes)
    UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
    NET: Registered protocol family 1
    RPC: Registered named UNIX socket transport module.
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    Trying to unpack rootfs image as initramfs...
    Freeing initrd memory: 9740K (c767d000 - c8000000)
    hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
    futex hash table entries: 512 (order: 3, 32768 bytes)
    workingset: timestamp_bits=28 max_order=17 bucket_order=0
    jffs2: version 2.2. (NAND) (SUMMARY)  Copyright 2001-2006 Red Hat, Inc.
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
    dma-pl330 f8003000.dmac:        DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
    Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
    43c00000.serial: ttyS0 at MMIO 0x43c01000 (irq = 166, base_baud = 3000000) is a 16550A
    e0000000.serial: ttyPS1 at MMIO 0xe0000000 (irq = 143, base_baud = 6249999) is a xuartps
    e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 144, base_baud = 6249999) is a xuartps
    ðconsole [ttyPS0] enabled
    console [ttyPS0] enabled
    bootconsole [earlycon0] disabled
    bootconsole [earlycon0] disabled
    xdevcfg f8007000.devcfg: ioremap 0xf8007000 to e081e000
    [drm] Initialized drm 1.1.0 20060810
    brd: module loaded
    loop: module loaded
    m25p80 spi0.0: found n25q128a13, expected m25p80
    m25p80 spi0.0: n25q128a13 (16384 Kbytes)
    4 ofpart partitions found on MTD device spi0.0
    Creating 4 MTD partitions on "spi0.0":
    0x000000000000-0x000000ff0000 : "boot"
    0x000000270000-0x000000ff0000 : "kernel"
    0x000000ff0000-0x000001000000 : "bootenv"
    0x000001000000-0x000001000000 : "spare"
    mtd: partition "spare" is out of reach -- disabled
    e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
    e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    ehci-pci: EHCI PCI platform driver
    usbcore: registered new interface driver usb-storage
    e0002000.usb supply vbus not found, using dummy regulator
    ULPI transceiver vendor/product ID 0x0424/0x0007
    Found SMSC USB3320 ULPI transceiver.
    ULPI integrity check: passed.
    ci_hdrc ci_hdrc.0: EHCI Host Controller
    ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
    ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    mousedev: PS/2 mouse device common for all mice
    i2c /dev entries driver
    i2c i2c-0: of_i2c: modalias failure on /amba_pl/i2c@41600000/i2c4@6b
    Bluetooth: HCI UART driver ver 2.3
    Bluetooth: HCI UART protocol H4 registered
    Bluetooth: HCI UART protocol BCSP registered
    Bluetooth: HCI UART protocol LL registered
    Bluetooth: HCI UART protocol ATH3K registered
    Bluetooth: HCI UART protocol Three-wire (H5) registered
    EDAC MC: ECC not enabled
    Xilinx Zynq CpuIdle Driver started
    sdhci: Secure Digital Host Controller Interface driver
    sdhci: Copyright(c) Pierre Ossman
    sdhci-pltfm: SDHCI platform and OF driver helper
    sdhci-arasan e0100000.sdhci: assigned as wifi host
    mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using DMA
    mmc1: SDHCI controller on e0101000.sdhci [e0101000.sdhci] using DMA
    ledtrig-cpu: registered to indicate activity on CPUs
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    NET: Registered protocol family 10
    sit: IPv6 over IPv4 tunneling driver
    NET: Registered protocol family 17
    Bluetooth: RFCOMM TTY layer initialized
    Bluetooth: RFCOMM socket layer initialized
    Bluetooth: RFCOMM ver 1.11
    Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    Bluetooth: BNEP socket layer initialized
    Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    Bluetooth: HIDP socket layer initialized
    Registering SWP/SWPB emulation handler
    mmc1: new high speed MMC card at address 0001
    hctosys: unable to open rtc device (rtc0)
    wlreg_on: disabling
    ALSA device list:
      No soundcards found.
    Freeing unused kernel memory: 1024K (c0a00000 - c0b00000)
    INIT: mmcblk1boot0: mmc1:0001 Q2J55L partition 1 16.0 MiB
    version 2.88 bootingmmcblk1boot1: mmc1:0001 Q2J55L partition 2 16.0 MiB

    mmcblk1rpmb: mmc1:0001 Q2J55L partition 3 4.00 MiB
     mmcblk1: p1
    FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
    EXT4-fs (mmcblk1rpmb): unable to read superblock
    EXT4-fs (mmcblk1rpmb): unable to read superblock
    EXT2-fs (mmcblk1rpmb): error: unable to read superblock
    FAT-fs (mmcblk1rpmb): unable to read boot sector
    EXT4-fs (mmcblk1rpmb): unable to read superblock
    EXT4-fs (mmcblk1rpmb): unable to read superblock
    EXT2-fs (mmcblk1rpmb): error: unable to read superblock
    FAT-fs (mmcblk1rpmb): unable to read boot sector
    FAT-fs (mmcblk1rpmb): unable to read boot sector
    mount: mounting /dev/mmcblk1rpmb on /run/media/mmcblk1rpmb failed: Input/output error
    mount: mounting /dev/mmcblk1boot0 on /run/media/mmcblk1boot0 failed: Invalid argument
    mount: mounting /dev/mmcblk1boot1 on /run/media/mmcblk1boot1 failed: Invalid argument
    /etc/mdev/mdev-mount.sh: line 28: [: /sys/block/mmcblk1/mmcblk1boot1: binary operator expected
    mount: mounting /dev/mmcblk1 on /run/media/mmcblk1 failed: Device or resource busy
    random: dd urandom read with 3 bits of entropy available
    Fri Jul 28 05:27:22 UTC 2017
    Starting internet superserver: inetd.
    INIT: Entering runlevel: 5
    Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device
    Starting system message bus: dbus.
    Starting Dropbear SSH server: Generating key, this may take a while...
    Public key portion is:
    ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQCgoIuoxYlhAHSMqzYg4DbPkJmmLZ+Jlw9gy6MnCcRtu9T54lQzis0ZUu+D/l+CXhGr2cw/U6RvGEU89yK5Yz6ph471LT09ZTpUCGwOca8P2RnqDHiohNjsKKU97/c4Zmvgi7/UIVb150zXfr+6SV3qDl1kC47NqjfDdwVS91FyCsVMD5+ZxgOUJhFPwL9uyQry0cbmwL2cAcm1EabUf6x7mhmCp1r4s0G2MxFfxwVy5ptY/lPeChVDheayT0fP5EW5MzmQpKEHVF5lTcdy2w5979RX+dwBNGjY9Mod84yDefNGrwCzj/ZYW7SdIJSFbtho6UnhSOKH3LVY/u650bav root@plnx_arm
    Fingerprint: md5 0b:7e:ad:a1:bc:1d:3a:bb:7a:4b:38:df:78:93:35:b9
    dropbear.
    Starting syslogd/klogd: done
    Starting tcf-agent: OK

    PetaLinux 2016.4 plnx_arm /dev/ttyPS0

    plnx_arm login:
     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 8 years ago

    Hi Stefan,

     

    This is odd. 

    I tryed:

    - 2017.3 with fsbl from tutorials

    - 2017.2 with fsbl from tutorials

    - 2017.1 without fsbl as it is not needed

    I always get the same posted results.

     

    For sure I waited for the Flash Operation Successful.

    To double check if flash_only_boot_7007S.bin was really being flashed, I first flashed a Hello Word and reset the board.

     

    Looking at your log, at least the u-boot version is the same (U-Boot 2016.07 (Jul 27 2017 - 21:56:59 -0700)).

     

    Do you mind sharing your bin file? I saw in some other post that the files were updated. I want to double check if I have a working file.

     

    Regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • stefanrousseau
    0 stefanrousseau over 8 years ago

    The file I have should be the same one that is in the zip with the document "Restoring  MiniZed to the Factory State" and the XSCT instructions on page 10.  The link was posted on as

    Restore QSPI and eMMC Factory Images

    Restore QSPI and eMMC Factory Images
      12.Sept.17

    I just re-downloaded the file and file compared the content again with what I am using.  They are the same:
    flash_only_boot_7007S.bin
    Size 16,623,092
    Date 07/27/2017

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 8 years ago in reply to stefanrousseau

    Thanks Stefan.

    Should u-boot enviroment be overwriten when flash_only_boot_7007S.bin is flashed?

     

    For sure my u-boot is trying to boot from MMC:

    cp_kernel2ram=mmc dev 1 && fatload mmc 1 ${netstart} ${kernel_img}
    default_bootcmd=run cp_kernel2ram && bootm ${netstart}
     

    So, I added a custom variable:

    setenv test = yes

    saveenv

     

    Then I flashed flash_only_boot_7007S.bin as follows:

    xsct% exec program_flash -f flash_only_boot_7007S.bin -flash_type qspi_single   
                                                                                    
    ****** Xilinx Program Flash
    ****** Program Flash v2017.1 (64-bit)
      **** SW Build 1846317 on Fri Apr 14 18:54:47 MDT 2017
        ** Copyright 1986-2017 Xilinx, Inc. All Rights Reserved.

    Connecting to hw_server @ TCP:localhost:3121

    WARNING: Failed to connect to hw_server at TCP:localhost:3121
    Attempting to launch hw_server at TCP:localhost:3121

    Connected to hw_server @ TCP:localhost:3121
    Available targets and devices:
    Target 0 : jsn-MiniZed V1-1234-oj1A
        Device 0: jsn-MiniZed V1-1234-oj1A-4ba00477-0

    Retrieving Flash info...

    Initialization done, programming the memory
    BOOT_MODE REG = 0x00000001
    WARNING: [Xicom 50-100] The current boot mode is QSPI.
    If flash programming fails, configure device for JTAG boot mode and try again.
    f probe 0 0 0
    Performing Erase Operation...
    Erase Operation successful.
    INFO: [Xicom 50-44] Elapsed time = 28 sec.
    Performing Program Operation...
    0%...10%...20%...30%...40%...50%...60%...70%...80%...90%...100%
    Program Operation successful.
    INFO: [Xicom 50-44] Elapsed time = 81 sec.

    Flash Operation Successful
    xsct%                                                                         

    And after rebooting that test = yes variable was still showing in printenv

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • stefanrousseau
    0 stefanrousseau over 8 years ago

    Can you confirm that while programming the flash you have the boot mode switch in the "JTAG" position and that when you re-boot, it is in the "Flash" position?  Trying to see if I can get an answer on why env variables will persist beyond re-programming.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • stefanrousseau
    0 stefanrousseau over 8 years ago in reply to stefanrousseau

    It seems that when you saveenv, it saves to an area in flash that is different from the area that is erased and programmed when programming a .bin file.

    I do not know how to change that in XSCT.  I saw above that you tried -erase_only and I do not know where you saw that switch but I tried it and it did not work to erase variables.  But you can force the entire flash to be programmed by doing it from the Hardware Manager inside Vivado.  Open it and connect to the target and add a configuration device.  Pick the Murata 128Mb QSPI single device mt25ql128-qspi-x1-single.

    When programming, you have the option of programming the Configuration File Only (default) or the Entire Configuration Memory Device.  If you select the latter, the saved env variables also get cleared.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • stefanrousseau
    0 stefanrousseau over 8 years ago in reply to stefanrousseau

    Above, it is the Micron flash, not Murata :)  Murata makes the wireless device on the board.  The memories are all from Micron.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>