Hello,
I was able to program the Zed board via USB-JTAG (J17) before. Today, I am unable to program the Zed board and get the following error "JTAG node is not accessible". I did re-install the Digilent cable driver from Xilinx/Vivado folder, but I still received the same error. Any help will be appreciated . Thank you.
16:26:52 INFOt: Launching XSDB server: xsdb.bat -s C:/Xilinx/SDK/2015.2/scripts/xsdb/xsdb/xsdb-server.tcl
16:26:53 INFOt: Processing command line option -hwspec C:/Projects/temp/zed-cib-ip-ver2/zed-cib-ip-ver2.sdk/ssdn_axi_v2_0_wrapper.hdf.
16:26:54 INFOt: XSDB server has started successfully.
16:26:54 INFOt: Checking for hwspec changes in the project ssdn_axi_v2_0_wrapper_hw_platform_0.
16:27:26 INFOt: Connected to target on host '127.0.0.1' and port '3121'.
16:27:26 INFOt: 'targets -set -filter {jtag_cable_name =~ "Digilent Zed 210248657980" && level==0} -index 1' command is executed.
16:27:28 ERRORt: JTAG node is not accessible