Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General JTAG node is not accessible (on Zed Board)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 1960 views
  • Users 0 members are here
Related

JTAG node is not accessible (on Zed Board)

Former Member
Former Member over 9 years ago

Hello,

I was able to program the Zed board via USB-JTAG (J17) before. Today, I am unable to program the Zed board and get the following error "JTAG node is not accessible". I did re-install the Digilent cable driver from Xilinx/Vivado folder, but I still received the same error. Any help will be appreciated . Thank you.

16:26:52 INFOt: Launching XSDB server: xsdb.bat -s C:/Xilinx/SDK/2015.2/scripts/xsdb/xsdb/xsdb-server.tcl
16:26:53 INFOt: Processing command line option -hwspec C:/Projects/temp/zed-cib-ip-ver2/zed-cib-ip-ver2.sdk/ssdn_axi_v2_0_wrapper.hdf.
16:26:54 INFOt: XSDB server has started successfully.
16:26:54 INFOt: Checking for hwspec changes in the project ssdn_axi_v2_0_wrapper_hw_platform_0.
16:27:26 INFOt: Connected to target on host '127.0.0.1' and port '3121'.
16:27:26 INFOt: 'targets -set -filter {jtag_cable_name =~ "Digilent Zed 210248657980" && level==0} -index 1' command is executed.
16:27:28 ERRORt: JTAG node is not accessible

  • Sign in to reply
  • Cancel
Parents
  • jansen0326
    0 jansen0326 over 7 years ago

    Hi,

     in Zedboard pin AB14 connect to FMC-PRSNT signal, don't assign the signal to this pin. This pin is used to control switching JTAG chain to FMC, connect signal to this pin will meet this problem when power on.

    Jansen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jansen0326
    0 jansen0326 over 7 years ago

    Hi,

     in Zedboard pin AB14 connect to FMC-PRSNT signal, don't assign the signal to this pin. This pin is used to control switching JTAG chain to FMC, connect signal to this pin will meet this problem when power on.

    Jansen