Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Advice on a great Petalinux tutorial for MicroZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 356 subscribers
  • Views 519 views
  • Users 0 members are here
Related

Advice on a great Petalinux tutorial for MicroZed

shanedora
shanedora over 7 years ago

I'm just starting out here with my MicroZed board. I'm initially walking through the "Creating a Hardware Design", and "Helloworld" tutorials first. Still have a little bit to go. However, these don't consist of running Linux. My understanding (CORRECT ME IF I'M WRONG) is the "Helloworld" tutorial is a bare metal programming example.

I would like to start my next set of tutorials on PetaLinux because we use it quite frequently here at work. My board came with a micro SD card for pulsar linux which is a Wind River product. I may still walk through the tutorial for that as well but was hoping someone could point me to a tutorial involving PetaLinux.

I would like to follow a tutorial that can relate as close to the environment of which I'm using. I realize everyone uses a slightly different environment but if you have any suggestions on tutorials that would be friendly enough to following along it would be much appreciated.

My Environment
OS: Centos 7
Vivado 2018
MicroZed Board 7010 model
 

  • Sign in to reply
  • Cancel
  • narrucmot
    0 narrucmot over 7 years ago

    A good resource may be the MicroZed Chronicles.  Though eponymous to MicroZed they also cover other boards (e.g. MiniZed and Ultra96) and lots of other Zynq and Zynq MPSoC design topics.  I must admit many of the MicroZed topics are, unfortunately, a bit dated now.  The PetaLinux tools have changed quite a bit since then (2014) and now, so that may make it hard to follow them.  The "episodes" specific to PetaLinux on the MicroZed start at #53.

    http://zedboard.org/content/microzed-chronicles

    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Adam-Taylor-s-MicroZed-Chronicles-Part-53-Linux-and-SMP/ba-p/531429

    Another good resource may be the Speedway course materials we created for the MiniZed board.  This is also a Zynq-based dev board, and these tutorials use the more recent Vivado and PetaLinux 2017.4 tools:

    http://zedboard.org/support/trainings-and-videos

    Developing Zynq Software (Vivado 2017.1 and 2017.4)

    Developing Zynq Hardware (Vivado 2017.1 and 2017.4)

    Integrating Sensors on MiniZed with PetaLinux (2017.1 and 2017.4)

    I hope this helps!

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer