Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General SIMPLE TCP example for Zynq
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 358 subscribers
  • Views 1440 views
  • Users 0 members are here
Related

SIMPLE TCP example for Zynq

grosdode
grosdode over 10 years ago

Hello,
I'm new at the Zynq platform but I already make the software and hardware lab from the training. My next step is to communicate via Ethernet but I can't really sort the Information I found when I google "tcp and Zynq" .
I'm search for a SIMPLE example or tutorial  to send something from the PC an receive it on the Board (microZed) via TCP or UDP.I found a freeRTOS example with six tasks and a lot of stuff I don't need (understand) and a video call "Express Logic's NetX high-performance TCP-IP stack" but both are RTOS. Did I really need a RTOS (I don't want to use a RTOS) ?
Can someone help me?

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    You are not required to have an RTOS nor any OS.  You can do this type of thing with a Bare Metal design.  Although, I would not recommend it due to the amount of effort.  I think it would be easier to use an operating system - be it RTOS or Linux based, mostly because of the overhead associated with using a TCP or UDP stack.  The operating system witll take care of most of that for you.  If you are looking for something like LWIP, there are examples, however, this is not necessarily a "simple TCP or UDP" datagram.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    You are not required to have an RTOS nor any OS.  You can do this type of thing with a Bare Metal design.  Although, I would not recommend it due to the amount of effort.  I think it would be easier to use an operating system - be it RTOS or Linux based, mostly because of the overhead associated with using a TCP or UDP stack.  The operating system witll take care of most of that for you.  If you are looking for something like LWIP, there are examples, however, this is not necessarily a "simple TCP or UDP" datagram.

    --Dan