I'm gone through the tutorial and all worked nearly fine.
Had the following two problems and solved them:
FIRST: http://zedboard.org/content/zedboard-problem-code-sdk
and
SECOND: http://zedboard.org/content/zynq-concepts-tools-and-techniques-zedboard-issues
Now I have an other problem. I can run the application and control it via the tera term. If I decide to press '2' and BTNR all works fine.
If I press '1' there is no reaction to pressing BTNU or any other button.
As the BTNU is connected to the PS part of the Zynq I wonder if there is an error in the zedboard_CTT***.pdf in appendix A.
I copied the code from there and changed the macro names according to FIRST.
The PL part / button BTNR works so it must be something with the software?? or not?
Thanks for any suggestions.
regards,
David