Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Lab 1.3 not working at the final stage
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 354 subscribers
  • Views 514 views
  • Users 0 members are here
Related

Lab 1.3 not working at the final stage

Former Member
Former Member over 12 years ago

Hi all,
  
    Just began exploring the Zedboard. I am sure everybody has completed this . My Lab 1.3 fails at the last stage.

    Hit any key to stop autoboot:0
zed-boot> 

    after Hit any key to stop autoboot:0, I do not get the zed-boot>  prompt.

Instead I see a lot of message pertaining to the kernel code..( error / code crash ...)

    What are the files I need to have in the SD ram.

    I have the following:

    1. devicetree.dtb ( renamed factory file in SD card)
    2. boot.bin ( from lab 1.3 output in SD card)
    3. ramdisk32M.image.gz ( renamed factory file )
    4. ZImage ( from factory file in SD card )

    What did I do wrong ???

  Please help!!

Thank you

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 12 years ago

    Hi lasur2,

    I have not seen a U-Boot crash at this point before when using the git 14.2 release tag.  Did you press a key during the autoboot countdown?  If not, U-Boot will automatically try to boot Linux, which if you are still on Lab 1.3 would be expected to fail.

    Assuming that you are pressing a key to interrupt autoboot and there is a real crash, perhaps you accidentally ended up on the wrong release tag or board config.  You can see what release tag is currently checked out by changing into the U-Boot folder and checking the status of the local repository.

    $ cd u-boot-xlnx
    $ git status

    Also, be sure that you configured U-Boot for ZedBoard using this command:

    $ make zynq_zed_config

    You can also try the lab solution file boot.bin to see if you see the same error.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago

    Hi Folks,

    I also had trouble in the final stage.
    My terminal didn't respond.
    The instruction in step 12, page 16, says power cycle the board. This causes Tera Term to looses the terminal connection. Instead Press BUTTON 7 u201CPS-RSTu201D in the bottom left corner of the board to warm-boot the board.
    Then the terminal starts responding with the uboot-prompt when you send keyboard chars to interupt the booting sequence.

    Just sharing it. Hope this helps.

    Rgds,
    Technicolor
    Just sharing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to zedhed

    Hi Kevin,

        Thanks for the response. I am re-doing the lab as I need to get it working !

       $ cd u-boot-xlnx

       $ git status gives me the following o/p

    # On branch xilinx-14.2-build1-trd
    # Changed but not updated:
    #   (use "git add <file>..." to update what will be committed)
    #   (use "git checkout -- <file>..." to discard changes in working directory)
    #
    #tmodified:   include/configs/zynq_zed.h
    #
    no changes added to commit (use "git add" and/or "git commit -a")


       $ make distclean gives me the following O/p
       awk '(NF && $1 !~ /^#/) { print $1 ": " $1 "_config; $(MAKE)" }' boards.cfg > .boards.depend

       $ make zynq_zed_config gives me
    awk '(NF && $1 !~ /^#/) { print $1 ": " $1 "_config; $(MAKE)" }' boards.cfg > .boards.depend
    Configuring for zynq_zed board...

    Then copy and paste the patch file Now,

    $ git apply 0001-Xilinx-ARM-Experimental-32MB-Ramdisk-on-ZedBoard.patch

    Upto this point is lab1.2 Experiment #2 and I am successful.

    Now when I move to lab1.2 Experiment #3,

    $pwd
    I am in /home/training/u-boot-xlnx

    $ make

    I see the following errors:

    ake: arm-linux-gcc: Command not found
    /bin/sh: arm-linux-gcc: command not found
    dirname: missing operand
    Try `dirname --help' for more information.
    Generating include/autoconf.mk
    /bin/sh: line 3: arm-linux-gcc: command not found
    /bin/sh: arm-linux-gcc: command not found
    dirname: missing operand
    Try `dirname --help' for more information.
    Generating include/autoconf.mk.dep
    /bin/sh: line 3: arm-linux-gcc: command not found
    make: arm-linux-gcc: Command not found
    /bin/sh: arm-linux-gcc: command not found
    dirname: missing operand
    Try `dirname --help' for more information.
    /bin/sh: arm-linux-gcc: command not found
    /bin/sh: arm-linux-ld: command not found
    /bin/sh: arm-linux-gcc: command not found
    dirname: missing operand
    Try `dirname --help' for more information.
    /bin/sh: arm-linux-gcc: command not found
    dirname: missing operand
    Try `dirname --help' for more information.
    arm-linux-gcc -DDO_DEPS_ONLY
    tt-g  -Os   -fno-common -ffixed-r8 -msoft-float   -fno-strict-aliasing  -fno-common -ffixed-r8 -msoft-float  -D__KERNEL__ -I/home/training/u-boot-xlnx/include -fno-builtin -ffreestanding -nostdinc -isystem  -pipe  -DCONFIG_ARM -D__ARM__         -march=armv5 -march=armv7-a -I/home/training/u-boot-xlnx/board/xilinx/common -I/home/training/u-boot-xlnx/board/xilinx/zynq_common -Wall -Wstrict-prototypes -mno-unaligned-access   
    tt-o lib/asm-offsets.s lib/asm-offsets.c -c -S
    make: arm-linux-gcc: Command not found
    make: *** [lib/asm-offsets.s] Error 127


    This is the cross compiler error I suppose. I am not sure how to fix it. please help!!

    Thank you!!


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 12 years ago in reply to Former Member

    Hi lasur2,

    Those error messages seem to indicate that the cross compiler toolchain cannot be found on your system.  I can think of two likely causes for this.  The first cause would be that the CodeSourcery Toolchain did not get installed correctly during the Lab 0.1 exercises.  The second is that the wrong compiler prefix OR incorrect paths have been specified.

    Both the toolchain and the path to the toolchain must be setup on your system.  Otherwise, at build time, the compiler executable will not be found properly.

    One other thing to note is that I used an Ubuntu machine a while back which required me to specify the cross-compiler prefix as part of the make command.  If you have a similar system, you may need to do something like this:

    $ make ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi-

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to zedhed

    Hi Kevin,

       Thanks for your remote support. I was able to debug with your pointer and got the lab1.3 working ..

       I am currently facing difficulty in getting lab 2.3 work. I am debugging on my own. Shall seek your help and pointers in case I run into problems while debug.

    Thank you very much once again!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 12 years ago in reply to Former Member

    Hi lasur2,

    Glad to hear that you were able to get Lab 1.3 working. If you continue to have problems with Lab 2.3, please repost your 2.3 issue as a new topic so that it is easier for other community members to find.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago

    Hi All,
    M stuck at a step behind !

    M not getting message on the serial terminal "Hit any key to stop autoboot: 3"

    And everything stops here, m using tera term for the communication and terminal is not responding at all..
    Can anyone help me on this ?
    below is the copy of my XMD terminal....
    Xilinx Microprocessor Debugger (XMD) Engine
    Xilinx EDK 14.2 Build EDK_P.28xd
    Copyright (c) 1995-2012 Xilinx, Inc.  All rights reserved.

    XMD%
    XMD%
    Accepted a new TCLSock connection from 127.0.0.1 on port 3462
    connect arm hw

    JTAG chain configuration
    --------------------------------------------------
    Device   ID Code        IR Length    Part Name
    1       4ba00477           4        Cortex-A9
    2       03727093           6        XC7Z020

    CortexA9 Processor Configuration
    -------------------------------------
    Version.............................0x00000003
    User ID.............................0x00000000
    No of PC Breakpoints................6
    No of Addr/Data Watchpoints.........1

    Connected to "arm" target. id = 64
    Starting GDB server for "arm" target (id = 64) at TCP port no 1234
    XMD% source ps7_init
    couldn't read file "ps7_init": no such file or directory
    XMD% cd ..
    XMD% cd ..
    XMD% cd ..
    XMD% cd ..
    XMD% cd xilinxtest
    XMD% cd project
    XMD% cd opfile
    XMD% source ps7_init
    couldn't read file "ps7_init": no such file or directory
    XMD% ls
    bootimage.bif
    ps7_init.tcl
    u-boot.bin
    u-boot.elf
    u-boot.mcs
    XMD% source ps7_init.tcl
    XMD% ps7_init
    XMD% dow -data qspi_image.bin 0x08000000
    warning: FPGA is NOT Configured. Accessing FPGA Address space can
    cause the System to hang. Use "fpga" command to Configure the FPGA
    ERROR: Cannot OPEN File
    t - qspi_image.bin

    XMD% init_user
    Info:  Enabling level shifters and clearing fabric port resets
    XMD% dow u-boot.elf
    warning: FPGA is NOT Configured. Accessing FPGA Address space can
    cause the System to hang. Use "fpga" command to Configure the FPGA
    Downloading Program -- u-boot.elf
    tsection, .text: 0x04000000-0x0402aa83
    tsection, .rodata: 0x0402aa84-0x04035a7e
    tsection, .hash: 0x04035a80-0x04035ac7
    tsection, .data: 0x04035ac8-0x0403658f
    tsection, .got.plt: 0x04036590-0x0403659b
    tsection, .u_boot_cmd: 0x0403659c-0x04036bbb
    tsection, .rel.dyn: 0x04036bbc-0x0403c8eb
    tsection, .dynsym: 0x0403c8ec-0x0403c9bb
    tsection, .bss: 0x04036bbc-0x04079acb
    Setting PC with Program Start Address 0x04000000
    XMD% dow -data u-boot.bin 0x08000000
    warning: FPGA is NOT Configured. Accessing FPGA Address space can
    cause the System to hang. Use "fpga" command to Configure the FPGA
    Downloading Data File -- u-boot.bin at 0x08000000
    Progress ............................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................Done
    XMD% con

    RUNNING> XMD% sf probe 0 0 0
    invalid command name "sf"
    XMD% stop
    Processor stopped