Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Lab 1.3 not working at the final stage
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 359 subscribers
  • Views 525 views
  • Users 0 members are here
Related

Lab 1.3 not working at the final stage

Former Member
Former Member over 12 years ago

Hi all,
  
    Just began exploring the Zedboard. I am sure everybody has completed this . My Lab 1.3 fails at the last stage.

    Hit any key to stop autoboot:0
zed-boot> 

    after Hit any key to stop autoboot:0, I do not get the zed-boot>  prompt.

Instead I see a lot of message pertaining to the kernel code..( error / code crash ...)

    What are the files I need to have in the SD ram.

    I have the following:

    1. devicetree.dtb ( renamed factory file in SD card)
    2. boot.bin ( from lab 1.3 output in SD card)
    3. ramdisk32M.image.gz ( renamed factory file )
    4. ZImage ( from factory file in SD card )

    What did I do wrong ???

  Please help!!

Thank you

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Hi All,
    M stuck at a step behind !

    M not getting message on the serial terminal "Hit any key to stop autoboot: 3"

    And everything stops here, m using tera term for the communication and terminal is not responding at all..
    Can anyone help me on this ?
    below is the copy of my XMD terminal....
    Xilinx Microprocessor Debugger (XMD) Engine
    Xilinx EDK 14.2 Build EDK_P.28xd
    Copyright (c) 1995-2012 Xilinx, Inc.  All rights reserved.

    XMD%
    XMD%
    Accepted a new TCLSock connection from 127.0.0.1 on port 3462
    connect arm hw

    JTAG chain configuration
    --------------------------------------------------
    Device   ID Code        IR Length    Part Name
    1       4ba00477           4        Cortex-A9
    2       03727093           6        XC7Z020

    CortexA9 Processor Configuration
    -------------------------------------
    Version.............................0x00000003
    User ID.............................0x00000000
    No of PC Breakpoints................6
    No of Addr/Data Watchpoints.........1

    Connected to "arm" target. id = 64
    Starting GDB server for "arm" target (id = 64) at TCP port no 1234
    XMD% source ps7_init
    couldn't read file "ps7_init": no such file or directory
    XMD% cd ..
    XMD% cd ..
    XMD% cd ..
    XMD% cd ..
    XMD% cd xilinxtest
    XMD% cd project
    XMD% cd opfile
    XMD% source ps7_init
    couldn't read file "ps7_init": no such file or directory
    XMD% ls
    bootimage.bif
    ps7_init.tcl
    u-boot.bin
    u-boot.elf
    u-boot.mcs
    XMD% source ps7_init.tcl
    XMD% ps7_init
    XMD% dow -data qspi_image.bin 0x08000000
    warning: FPGA is NOT Configured. Accessing FPGA Address space can
    cause the System to hang. Use "fpga" command to Configure the FPGA
    ERROR: Cannot OPEN File
    t - qspi_image.bin

    XMD% init_user
    Info:  Enabling level shifters and clearing fabric port resets
    XMD% dow u-boot.elf
    warning: FPGA is NOT Configured. Accessing FPGA Address space can
    cause the System to hang. Use "fpga" command to Configure the FPGA
    Downloading Program -- u-boot.elf
    tsection, .text: 0x04000000-0x0402aa83
    tsection, .rodata: 0x0402aa84-0x04035a7e
    tsection, .hash: 0x04035a80-0x04035ac7
    tsection, .data: 0x04035ac8-0x0403658f
    tsection, .got.plt: 0x04036590-0x0403659b
    tsection, .u_boot_cmd: 0x0403659c-0x04036bbb
    tsection, .rel.dyn: 0x04036bbc-0x0403c8eb
    tsection, .dynsym: 0x0403c8ec-0x0403c9bb
    tsection, .bss: 0x04036bbc-0x04079acb
    Setting PC with Program Start Address 0x04000000
    XMD% dow -data u-boot.bin 0x08000000
    warning: FPGA is NOT Configured. Accessing FPGA Address space can
    cause the System to hang. Use "fpga" command to Configure the FPGA
    Downloading Data File -- u-boot.bin at 0x08000000
    Progress ............................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................Done
    XMD% con

    RUNNING> XMD% sf probe 0 0 0
    invalid command name "sf"
    XMD% stop
    Processor stopped

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    Hi All,
    M stuck at a step behind !

    M not getting message on the serial terminal "Hit any key to stop autoboot: 3"

    And everything stops here, m using tera term for the communication and terminal is not responding at all..
    Can anyone help me on this ?
    below is the copy of my XMD terminal....
    Xilinx Microprocessor Debugger (XMD) Engine
    Xilinx EDK 14.2 Build EDK_P.28xd
    Copyright (c) 1995-2012 Xilinx, Inc.  All rights reserved.

    XMD%
    XMD%
    Accepted a new TCLSock connection from 127.0.0.1 on port 3462
    connect arm hw

    JTAG chain configuration
    --------------------------------------------------
    Device   ID Code        IR Length    Part Name
    1       4ba00477           4        Cortex-A9
    2       03727093           6        XC7Z020

    CortexA9 Processor Configuration
    -------------------------------------
    Version.............................0x00000003
    User ID.............................0x00000000
    No of PC Breakpoints................6
    No of Addr/Data Watchpoints.........1

    Connected to "arm" target. id = 64
    Starting GDB server for "arm" target (id = 64) at TCP port no 1234
    XMD% source ps7_init
    couldn't read file "ps7_init": no such file or directory
    XMD% cd ..
    XMD% cd ..
    XMD% cd ..
    XMD% cd ..
    XMD% cd xilinxtest
    XMD% cd project
    XMD% cd opfile
    XMD% source ps7_init
    couldn't read file "ps7_init": no such file or directory
    XMD% ls
    bootimage.bif
    ps7_init.tcl
    u-boot.bin
    u-boot.elf
    u-boot.mcs
    XMD% source ps7_init.tcl
    XMD% ps7_init
    XMD% dow -data qspi_image.bin 0x08000000
    warning: FPGA is NOT Configured. Accessing FPGA Address space can
    cause the System to hang. Use "fpga" command to Configure the FPGA
    ERROR: Cannot OPEN File
    t - qspi_image.bin

    XMD% init_user
    Info:  Enabling level shifters and clearing fabric port resets
    XMD% dow u-boot.elf
    warning: FPGA is NOT Configured. Accessing FPGA Address space can
    cause the System to hang. Use "fpga" command to Configure the FPGA
    Downloading Program -- u-boot.elf
    tsection, .text: 0x04000000-0x0402aa83
    tsection, .rodata: 0x0402aa84-0x04035a7e
    tsection, .hash: 0x04035a80-0x04035ac7
    tsection, .data: 0x04035ac8-0x0403658f
    tsection, .got.plt: 0x04036590-0x0403659b
    tsection, .u_boot_cmd: 0x0403659c-0x04036bbb
    tsection, .rel.dyn: 0x04036bbc-0x0403c8eb
    tsection, .dynsym: 0x0403c8ec-0x0403c9bb
    tsection, .bss: 0x04036bbc-0x04079acb
    Setting PC with Program Start Address 0x04000000
    XMD% dow -data u-boot.bin 0x08000000
    warning: FPGA is NOT Configured. Accessing FPGA Address space can
    cause the System to hang. Use "fpga" command to Configure the FPGA
    Downloading Data File -- u-boot.bin at 0x08000000
    Progress ............................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................Done
    XMD% con

    RUNNING> XMD% sf probe 0 0 0
    invalid command name "sf"
    XMD% stop
    Processor stopped