Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General using a different board of in tutorial
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 275 views
  • Users 0 members are here
Related

using a different board of in tutorial

Former Member
Former Member over 11 years ago

Hi, I am trying to follow steps in lab four to create a microBlaze system.

http://www.xilinx.com/support/documentation/sw_manuals/xilinx2013_2/ug940-vivado-tutorial-embedded-design.pdf

but I'm using a zed board instead of a KC705 board, so the pin layout file doesn't work for me....anyone knows a way to work around it?

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Lab 4 of this tutorial targets a Kintex-7 device on a KC705 evaluation board. This board has DDR memory connected to the device such that it is available to the MicroBlaze design in the FPGA programmable logic. The ZedBoard uses a Zynq device and the DDR memory on board is only available directly to the ARM PS section of the device.

     

    If you want to implement a MicroBlaze on a ZedBoard you might take a look at these Xilinx forum posts on the subject:

     

    http://forums.xilinx.com/t5/Embedded-Development-Tools/MicroBlaze-on-Zynq-JTAG-mode-vs-SD-card-boot/td-p/293971

    http://forums.xilinx.com/xlnx/board/crawl_message?board.id=EDK&message.id=27712

     

    Or this Xilinx Answer Record:

     

    http://www.xilinx.com/support/answers/50869.html.

     

    You could also take a look at XAPP1093 http://www.xilinx.com/support/documentation/application_notes/xapp1093-amp-bare-metal-microblaze.pdf , but it targets the ZC702 eval board rather than the ZedBoard and you will need to make adjustments.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    Lab 4 of this tutorial targets a Kintex-7 device on a KC705 evaluation board. This board has DDR memory connected to the device such that it is available to the MicroBlaze design in the FPGA programmable logic. The ZedBoard uses a Zynq device and the DDR memory on board is only available directly to the ARM PS section of the device.

     

    If you want to implement a MicroBlaze on a ZedBoard you might take a look at these Xilinx forum posts on the subject:

     

    http://forums.xilinx.com/t5/Embedded-Development-Tools/MicroBlaze-on-Zynq-JTAG-mode-vs-SD-card-boot/td-p/293971

    http://forums.xilinx.com/xlnx/board/crawl_message?board.id=EDK&message.id=27712

     

    Or this Xilinx Answer Record:

     

    http://www.xilinx.com/support/answers/50869.html.

     

    You could also take a look at XAPP1093 http://www.xilinx.com/support/documentation/application_notes/xapp1093-amp-bare-metal-microblaze.pdf , but it targets the ZC702 eval board rather than the ZedBoard and you will need to make adjustments.

     

    -Gary