Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Regarding Basic_IPI_Design_ZedBoard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 353 subscribers
  • Views 216 views
  • Users 0 members are here
Related

Regarding Basic_IPI_Design_ZedBoard

Former Member
Former Member over 11 years ago

Hi

I have downloaded the Basic_IPI_design given as part of the reference design tutorials.However, as I do not have much knowledge about the Vivado Tool Flow, I am not too sure if the bitstream has to be generated in Vivado and programmed into the Zedboard or do I need to open the SDK and browse to the SDK folder present in the design folder and program FPGA through it.
I actually need to show it as a part of a demo and so while I would take my time to get aquainted with the tool Flow, I was actually wanting a quick way of getting through the demo atleast which is kind of very inevitable for me.

Any help would be really appreciated. Please help !!!


Regards
Akanksha 

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    A really good discusion on how the Vivado and SDK tool flow work is in the Avnet Developing Zynqu00AE-7000 All Programmable SoC Software (Vivado 2013.3)Speedway material you can download here: http://zedboard.org/support/trainings-and-videos

    That said, if you want to use the Basic_IPI design as a quick demo the Vivado design and bitsteam have already been "exported" to SDK in this example and a simple peripheral test application already build. SDK is very sensitive to the directory path structure, so if you want to use the existing project without "importing" the project into your new location, you will need to place the project in the directory it expects. It expects to find the "SDK_Export" directory in the following path:
    C:/Development_Projects/Dev_Boards/Avnet_ZedBoard/2013_2/Basic_IPI_Design/Basic_IPI_Design.sdk/SDK/SDK_Export

    You will need to unzip the project and change the directory path/names to match above. This project was build with Vivado 2013.2 it may or may not work without updates/changes in other versions of the tool.

    -Gary