Hello All.
I'm having some trouble with the MicroZed and the 4th tutorial. The first three tutorials went off with out a hitch. And I've been able to follow the system up till now, but I'm stuck in trying to prepare the boot image (experiment 2). Seems that the tool has changed a bit since the demo was written (and doesn't follow).
Basic issue is that I cannot load the correct elf files in the correct manor. The files run (based on the first part of the demo), but when I try using the 'create zynq boot image' something goes wrong. I can generate the file, but when loading the SD card, I no longer get the blue light to come one (suggesting that the FPGA is not loaded correctly).
Not specified in the instructions is what the 'edit partition' should be set for both .elf files. I've tried all combinations, but I'm doing something wrong.
Otherwise is a much nicer system (then say the OMAP environment).
could really use some help here
thanks
-Daniel