Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Can't initialize JTAG chain with FMC XM105 connected to Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 910 views
  • Users 0 members are here
Related

Can't initialize JTAG chain with FMC XM105 connected to Zedboard

Former Member
Former Member over 10 years ago

Hi,

I'm seeking for a solution in order to download bitfile to FPGA using JTAG, while FMC XM105 card is connected to Zedboard.

Datasheet of Zedboard says it's impossible to download bitfile while FMC card is connected, because of FMC-PRSNT signal.

Thanks for the help,

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    Hello Danna,

     

    I am not sure what 'datasheet' for the ZedBoard you are referring to or why it would say it is impossible to download a bitfile while an FMC card is connected.

     

    When an FMC card is plugged into the ZedBoard the FMC-PRSNT signal does cause the ZedBoard JTAG logic to include the FMC card in the JTAG chain as discussed in section 2.10.1 of the ZedBoard HW Users Guide:

     http://zedboard.org/sites/default/files/documentations/ZedBoard_HW_UG_v2_2.pdf

     

    With the FMC card installed you will need to either add a description of the FMC card JTAG device (a BSDL file) so that the program driving the JTAG chain, Vivado or the SDK in the case, understands the registers added to the chain by the additional device, or bypass the JTAG connection on your FMC board. In the case of the XM105 you can do that by placing a jumper across the TDI/TDO pins (6 and 7) of the JTAG header J5 in order to loop the JTAG signal back to the ZedBoard JTAG chain.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    Hello Danna,

     

    I am not sure what 'datasheet' for the ZedBoard you are referring to or why it would say it is impossible to download a bitfile while an FMC card is connected.

     

    When an FMC card is plugged into the ZedBoard the FMC-PRSNT signal does cause the ZedBoard JTAG logic to include the FMC card in the JTAG chain as discussed in section 2.10.1 of the ZedBoard HW Users Guide:

     http://zedboard.org/sites/default/files/documentations/ZedBoard_HW_UG_v2_2.pdf

     

    With the FMC card installed you will need to either add a description of the FMC card JTAG device (a BSDL file) so that the program driving the JTAG chain, Vivado or the SDK in the case, understands the registers added to the chain by the additional device, or bypass the JTAG connection on your FMC board. In the case of the XM105 you can do that by placing a jumper across the TDI/TDO pins (6 and 7) of the JTAG header J5 in order to loop the JTAG signal back to the ZedBoard JTAG chain.

     

    -Gary