Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Most simple workflow for kernel development with Zedboard and FMCOMMS2?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 374 subscribers
  • Views 1482 views
  • Users 0 members are here
Related

Most simple workflow for kernel development with Zedboard and FMCOMMS2?

e14 Contributor
e14 Contributor over 10 years ago

I am brand new to embedded development, and my goal is to do some kernel development with a Zedboard and an attached AD-FMCOMMS2-EBZ/AD9361 transceiver. Although I'd like to learn, I want to get a running system up ASAP, however, I am not sure if my current approach is over-complicating things. So to be clear - I need a a Linux kernel development environment with drivers for the AD9361 and access to the FMCOMMS2 board configured.

So far my approach has been to build a petalinux BSP using an Analog Devices supplied kernel. I was able to successfully build and boot the kernel, and it looks like the driver is compiled into the kernel correctly, however, I am not seeing the device listed under /sys/bus/iio/devices as descibed on the ADI Wiki:

https://wiki.analog.com/resources/tools-software/linux-drivers/iio-transceiver/ad9361

I have very little knowledge of hardware designs and device trees, so I am not sure where my problem lies, and unfortunately I cannot find a guide specific enough to get me up and running.

So, I have two questions:

1. Would using a petalinux BSP and ADI linux kernel w/ AD9361 drivers be a good way to go? If so, is there more detailed guides available for making the kernel aware of the FMCOMMS2 FMC card?

2. Is there a simpler approach? For example, a Linux distribution designed for Zedboard where I can recompile the kernel with AD9361 drivers?

I understand this is a really broad topic, but I was hoping someone could help point me in the right direction.

Thanks for looking!

  • Sign in to reply
  • Cancel
  • mbrown
    0 mbrown over 10 years ago

    The place to start for Linux, Zynq, and ADI boars is -- https://wiki.analog.com/resources/tools-software/linux-software/zynq_images

     

    Their designs use Ubuntu Desktop Linux.  All source code, including drivers, is here -- https://github.com/analogdevicesinc

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Not sure if you are still stumped but this is a lengthy issue.

    1) In order to build the FPGA image required to interface with the FMCOMMS2 board you need Vivado 2014.4.1 (which is not the standard webpack installation) If you don't care too much about messing with the FPGA image I'm sure you can find a bitstream to use without the need for compiling it yourself

    2) Analog has a guide for installing Linaro Linux on an SD card 

    3) Analog has a guide for installing the libiio libraries and gnuradio on the linaro build

    4) ???

    5) Profit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mikenmemphis
    0 mikenmemphis over 9 years ago

    Well thank you. i am being really benifitted by the answers here like this one. Thanks to this great forum.


    Mike Craig
    Internet marketer