Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General ZedBoard Xilinx SDK Program FPGA Failed (USB-JTAG)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 361 subscribers
  • Views 6871 views
  • Users 0 members are here
Related

ZedBoard Xilinx SDK Program FPGA Failed (USB-JTAG)

wespiard
wespiard over 6 years ago

I am trying to program a hello world design to the ZedBoard using the J17 USB-JTAG port. I am following this tutorial: https://reference.digilentinc.com/learn/programmable-logic/tutorials/zybo-getting-started-with-zynq/start

 

I am on step 11 where I have already setup the SDK project and am trying to program the FPGA. I get the following error after about 30 seconds:

 

Program FPGA failed

 

Reason:

Could not find FPGA device on the board for connection 'Local'.

 

Troubleshooting hints:

1. Check whether board is connected to system properly.

1. In case of zynq board, check whether Digilent/Xilinx cable switch settings are correct.

1. If you are using Xilinx Platform Cable USB, ensure that status LED is green.

 

I have tried uninstalling the "USB Receiver" driver that shows up in Device Manager when I plug and unplug the USB cable and restarting my computer but I get the same results.

 

The only thing that shows up in the hardware manager of Vivado is "localhost(0)".

 

Any suggestions?

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 6 years ago

    Note that Zybo and ZedBoard are different boards.

     

    I recommend you review the ZedBoard Configuration and Booting Guide, on the Reference Designs tab at ZedBoard

     

    Zedboard_config-boot_guide_IDS14_1.zip

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wespiard
    0 wespiard over 6 years ago in reply to bhfletcher

    The document you linked has the same steps once in the SDK, given a certain bitfile. My issue is when I actually try to program the FPGA, which is on page 19 of the document you linked.

     

    It also only mentions downloading the Cypress driver (which I believe is just the USB-UART port) which I already have. I can see the UART COM port when I connect a micro USB cable to it, just not when I connect to the USB-JTAG port (J17).

     

    -Wes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • wespiard
    0 wespiard over 6 years ago in reply to bhfletcher

    The document you linked has the same steps once in the SDK, given a certain bitfile. My issue is when I actually try to program the FPGA, which is on page 19 of the document you linked.

     

    It also only mentions downloading the Cypress driver (which I believe is just the USB-UART port) which I already have. I can see the UART COM port when I connect a micro USB cable to it, just not when I connect to the USB-JTAG port (J17).

     

    -Wes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bhfletcher
    0 bhfletcher over 6 years ago in reply to wespiard

    The ZedBoard USB-JTAG cable drivers are supposed to be installed with Vivado, as long as you selected the checkbox to "Install Cable Drivers." You can install them manually and try again.

    https://www.xilinx.com/support/answers/59128.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • wespiard
    0 wespiard over 6 years ago in reply to bhfletcher

    Thank you! Re-installing the driver manually w/ the 64-bit (in my case) version worked, using the following command, after cd'ing into the directory of the installer:

     

    C:\Xilinx\Vivado\2019.1\data\xicom\cable_drivers\nt64>install_drivers_wrapper.bat C:\Xilinx\Vivado\2019.1\data\xicom\cable_drivers\nt64 CC:\Xilinx\Vivado\2019.1\install.log C:\Xilinx\Vivado\2019.1\

    WARNING: Ignoring unknown argument C:\Xilinx\Vivado\2019.1\data\xicom\cable_drivers\nt64

    WARNING: Ignoring unknown argument CC:\Xilinx\Vivado\2019.1\install.log

    WARNING: Ignoring unknown argument C:\Xilinx\Vivado\2019.1\

    INFO: Log file=C:\Xilinx\Vivado\2019.1\data\xicom\cable_drivers\nt64\install_drivers_wrapper.log

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 6 years ago in reply to wespiard

    Thanks for letting us know, and good luck with your design!