I need to put my Zedboard into JTAG independent mode to debug PL side and PS side independently. As explained in UG585 page 718 when I set Zedboard to JTAG independent mode, PS side (ARM) processors will not be accessed by the JTAG connector. When I put Zedboard into JTAG independent mode, I can use inbuilt Digilent JTAG controller of Zedboard to program and debug PL side. I am trying to find a method to program PS side (I don't need to set breakpoints at this stage, just programming the PS side is enough), for this, can I use a Xilinx Platform cable and connect JTAG wires to MIO pins or EMIO pins of PS side as explained in page 722 of UG585? or Do I have to use an ARM JTAG module for this task?