Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard PS side program via PJTAG using Xilinx Platform Cables
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 358 subscribers
  • Views 2210 views
  • Users 0 members are here
  • jtag independent mode
  • pjtag
Related

Zedboard PS side program via PJTAG using Xilinx Platform Cables

darshanaj
darshanaj over 6 years ago

I need to put my Zedboard into JTAG independent mode to debug PL side and PS side independently. As explained in UG585 page 718 when I set Zedboard to JTAG independent mode, PS side (ARM) processors will not be accessed by the JTAG connector. When I put Zedboard into JTAG independent mode, I can use inbuilt Digilent JTAG controller of Zedboard to program and debug PL side. I am trying to find a method to program PS side (I don't need to set breakpoints at this stage, just programming the PS side is enough), for this, can I use a Xilinx Platform cable and connect JTAG wires to MIO pins or EMIO pins of PS side as explained in page 722 of UG585? or Do I have to use an ARM JTAG module for this task? 

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 6 years ago +1 suggested
    Yes you can configure the JTAG to independent mode in ZU+ MPSoC as well. Please try the below commands in XSCT console- xsct% mrd -force 0xFFCA0034 FFCA0034: 00000003 xsct% mwr -force 0xFFCA0030 3 xsct…
Parents
  • clem57
    0 clem57 over 6 years ago

    Yes you can configure the JTAG to independent mode in ZU+ MPSoC as well.

    Please try the below commands in XSCT console-

    xsct% mrd -force 0xFFCA0034
    FFCA0034: 00000003
    xsct% mwr -force 0xFFCA0030 3
    xsct% mrd -force 0xFFCA0034

    If you are using production version of ZU+ device then you should include one more command before you launch HW server because but hw_server called by XSDB or Vivado HW Manager automatically links the DAP to the primary scan chain.

    You can can disable this by setting hw_server parameter processor-debug-claim
    to 2 and then connect XSDB or Vivado HW Manager to this hw_server.

    Here two different methods:

    1. This is how you specify the option at hw_server start-up:

    hw_server -e "set processor-debug-claim 2"

    2. You may also use the --init=script.txt option to load this setting through a file. To use the init option you need to create a initialization script as shown below. In the script you specify the "set processor-debug-claim" parameter.

    # Sample script.txt
    set processor-debug-claim 2

    You start the hw_server as shown below:

     

    hw_server --init=script.txt

    NOTE: After configuring "processor-debug-claim 2", the user must reset the board (power cycle) in order to see the split chain.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 6 years ago

    Yes you can configure the JTAG to independent mode in ZU+ MPSoC as well.

    Please try the below commands in XSCT console-

    xsct% mrd -force 0xFFCA0034
    FFCA0034: 00000003
    xsct% mwr -force 0xFFCA0030 3
    xsct% mrd -force 0xFFCA0034

    If you are using production version of ZU+ device then you should include one more command before you launch HW server because but hw_server called by XSDB or Vivado HW Manager automatically links the DAP to the primary scan chain.

    You can can disable this by setting hw_server parameter processor-debug-claim
    to 2 and then connect XSDB or Vivado HW Manager to this hw_server.

    Here two different methods:

    1. This is how you specify the option at hw_server start-up:

    hw_server -e "set processor-debug-claim 2"

    2. You may also use the --init=script.txt option to load this setting through a file. To use the init option you need to create a initialization script as shown below. In the script you specify the "set processor-debug-claim" parameter.

    # Sample script.txt
    set processor-debug-claim 2

    You start the hw_server as shown below:

     

    hw_server --init=script.txt

    NOTE: After configuring "processor-debug-claim 2", the user must reset the board (power cycle) in order to see the split chain.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer