Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard AXI DMA m_axis_mm2s_tdata[31:0] stuck on zero
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 358 subscribers
  • Views 738 views
  • Users 0 members are here
  • Using Xilinx Tools
  • ZedBoard General Questions
  • Zynq Mini-ITX Hardware Design
  • Zedboard Hardware Design
  • PicoZed Hardware Design
  • Zynq Mini-Module Plus (MMP) Hardware Design
  • MicroZed Hardware Design
  • MiniZed Hardware Design
  • Zedboard Training
Related

Zedboard AXI DMA m_axis_mm2s_tdata[31:0] stuck on zero

maiatec
maiatec over 5 years ago

My application is to transfer a 32 bit from DDR (using DMA) to PL.

I connected the ILA to see the data at the m_axis_mm2s from axi_dma and it shows the m_axis_mm2s_tdata[31:0] always zero besides m_axis_mm2s_tready, m_axis_mm2s_tvalid and m_axis_mm2s_tlast seems ok.imageimage

Cabeçalho 1

/*****************************************************************************/

/**

* @file streamExampleSimpleDMA.c

*

* In this file the basic set up of streaming a package buffer over the AXI

* Stream Interface to a Custom IP core in PL. This is example is highly

* inspired by examples from Xilinx.

*

* <pre>

* MODIFICATION HISTORY:

*

* Ver Who Date Changes

* ----- ---- -------- -------------------------------------------------------

* 1.00a jcla 03/04/16 The example is created based on other examples from

* Xilinx

 

* ***************************************************************************

 

*/

/***************************** Include Files *********************************/

#include "xaxidma.h"

#include "xparameters.h"

#include "xdebug.h"

 

 

/******************** Constant Definitions **********************************/

 

/*

* Device hardware build related constants.

*/

 

#define DMA_DEV_ID XPAR_AXIDMA_0_DEVICE_ID

 

#define MEM_BASE_ADDR 0x40400000

 

#define TX_BUFFER_BASE (MEM_BASE_ADDR + 0x00100000)

 

// The example can be extended to feature a larger stream package, but for

// simplicity it is now set to 0x1

#define MAX_PKT_LEN 0xe //0x20

 

#define TEST_START_VALUE 0x6

 

#define NUMBER_OF_TRANSFERS 10

 

 

/************************** Function Prototypes ******************************/

 

#if (!defined(DEBUG))

extern void xil_printf(const char *format, ...);

#endif

 

/************************** Variable Definitions *****************************/

/*

* Device instance definitions

*/

XAxiDma AxiDma;

 

 

/*****************************************************************************/

/*

* The entry point for this example. It invokes the example function,

* and reports the execution status.

*

* @param None.

*

* @return

* - XST_SUCCESS if example finishes successfully

* - XST_FAILURE if example fails.

*

* @note None.

*

******************************************************************************/

int main()

{

XAxiDma_Config *CfgPtr;

int Status;

int Index;

u8 *TxBufferPtr;

u8 Value;

 

xil_printf("\r\nStarting sending data\r\n");

 

TxBufferPtr = (u8 *)TX_BUFFER_BASE;

 

/* Initialize the XAxi Dma device.

*/

CfgPtr = XAxiDma_LookupConfig(DMA_DEV_ID);

if (!CfgPtr) {

xil_printf("No config found for %d\r\n", DMA_DEV_ID);

return XST_FAILURE;

}

 

Status = XAxiDma_CfgInitialize(&AxiDma, CfgPtr);

if (Status != XST_SUCCESS) {

xil_printf("Initialization failed %d\r\n", Status);

return XST_FAILURE;

}

 

if(XAxiDma_HasSg(&AxiDma)){

xil_printf("Device configured as SG mode \r\n");

return XST_FAILURE;

}

 

/* Disable interrupts, we use polling mode

*/

XAxiDma_IntrDisable(&AxiDma, XAXIDMA_IRQ_ALL_MASK,

XAXIDMA_DEVICE_TO_DMA);

 

Value = TEST_START_VALUE;

// Created the TxBuffer. For now it is set to one however it

// can be extended to a larger number

for(Index = 0; Index < MAX_PKT_LEN; Index ++) {

TxBufferPtr[Index] = Value;

 

Value = (Value + 1) & 0xFF;

}

 

/* Flush the SrcBuffer before the DMA transfer, in case the Data Cache

* is enabled

*/

Xil_DCacheFlushRange((UINTPTR)TxBufferPtr, MAX_PKT_LEN);

 

 

//Sets up the DMA-To-Device so that data i send.

Status = XAxiDma_SimpleTransfer(&AxiDma,(UINTPTR) TxBufferPtr,

MAX_PKT_LEN, XAXIDMA_DMA_TO_DEVICE);

 

if (Status != XST_SUCCESS) {

return XST_FAILURE;

}

 

while (XAxiDma_Busy(&AxiDma,XAXIDMA_DMA_TO_DEVICE)) {} //wait

 

xil_printf("\r\nDone sending data\r\n");

/* Test finishes successfully

*/

return XST_SUCCESS;

 

Mensagem editada por: Herivaldo Maia

  • Sign in to reply
  • Cancel
  • maiatec
    0 maiatec over 5 years ago

    Solved !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 5 years ago in reply to maiatec

    Great! Can maiatec  elaborate with a sentence or two on how?