Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Ultrazed 3EG - display port reference design - desktop linux?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 895 views
  • Users 0 members are here
  • Software Application Development
  • Ultrazed Hardware Design
Related

Ultrazed 3EG - display port reference design - desktop linux?

laurencebarker
laurencebarker over 5 years ago

I've found the displayport reference design for the ultrazed EG I/O carrier.

 

Where I want to get to is: I have desktop Linux running on the ultrazed with a monitor connected to the displayport. I've seen there is a reference design for the ZCU102, but I can't see one for the ultrazed.

 

Is that a simple step from the reference design, a complicated step, or is it just not viable please?

 

 

 

 

Laurence Barker

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 5 years ago

    Hi there,

     

    I'm not sure what you are asking.  Could you be more specific on what your desire is?

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • laurencebarker
    0 laurencebarker over 5 years ago in reply to drozwood90

    I'm trying to reach the point where the ultrazed is like a standalone computer that happens to have an FPGA. It would have a monitor attached to the displayport connection; it would have mouse and keyboard attached. It would run a desktop version of Linux with GUI etc.

     

    The reason I want this is: I will then also be interfacing HF software defined radio with attached ADC, DAC and digital processing in the FPGA. The user interface runs as a Linux application and presents its display to the GUI. I understand very well the signal processing and how to implement in in the FPGA; I don't know much about configuring Linux systems!

     

    I had previously looked at Zynq7020 based boards and one did have a port of desktop Linux with all the appropriate device drivers. I want to answer the same question for newer, Ultrascale SOM boards. I can see that a frame buffer with for example the rotating cube is possible; what I'm trying to find out is how big a step it is to having the desktop GUI form of Linux. It may be a case of simply selecting the right drivers, or it could be much more complicated!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • laurencebarker
    0 laurencebarker over 5 years ago in reply to drozwood90

    I'm trying to reach the point where the ultrazed is like a standalone computer that happens to have an FPGA. It would have a monitor attached to the displayport connection; it would have mouse and keyboard attached. It would run a desktop version of Linux with GUI etc.

     

    The reason I want this is: I will then also be interfacing HF software defined radio with attached ADC, DAC and digital processing in the FPGA. The user interface runs as a Linux application and presents its display to the GUI. I understand very well the signal processing and how to implement in in the FPGA; I don't know much about configuring Linux systems!

     

    I had previously looked at Zynq7020 based boards and one did have a port of desktop Linux with all the appropriate device drivers. I want to answer the same question for newer, Ultrascale SOM boards. I can see that a frame buffer with for example the rotating cube is possible; what I'm trying to find out is how big a step it is to having the desktop GUI form of Linux. It may be a case of simply selecting the right drivers, or it could be much more complicated!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • narrucmot
    0 narrucmot over 5 years ago in reply to laurencebarker

    Hi Laurence,

     

    Currently the only board we have a Linux OS image for that does what you describe (Linux windowed desktop environment with DisplayPort output and mouse/keyboard input) is the Ultra96-V2.  This board is similar to the UltraZed-EG in that they both use the Xilinx Zu+ 3EG MPSoC device, have USB input, and DisplayPort output.  It is certainly possible to leverage the PetaLinux BSP for the Ultra96-V2 to create what you want for the UltraZed-EG.  Much of this task is probably straightforward, but this is isn't something we have or can support right now.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • laurencebarker
    0 laurencebarker over 5 years ago in reply to narrucmot

    Thank you - that was exactly the information I was looking for.

     

    I can look at whether the Ultra96 driver set could move across to the Ultrazed. I can see there are some differences in devices but that gives me a solid start. And potentially I could use an Ultra96 for a prototype for my application: it doesn't have enough I/O connections for the final version but I can de-risk much of the project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 5 years ago in reply to laurencebarker

    Hi there,

     

    I wanted to let you know that we are currently uploading the images for the UltraZed-EG platforms for 2019.2.  These support Vitis and have displayport with ethernet working.  Look for them on the product pages, and expect them to be there within a day or two.

     

    --Dan