Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Long-wired cameras for Jetson Xavier AGX
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 473 views
  • Users 0 members are here
  • gmsl
  • jetson
  • jetson-xavier
  • camera
  • gige
  • getopicszedboard_forum
Related

Long-wired cameras for Jetson Xavier AGX

pra-dan
pra-dan over 5 years ago

Hi,

 

I am developing an autonomous robot that navigates using multiple cameras. Some of the cameras (3-4 of them,) are placed near the Jetson Xavier AGX while some of them (2-3) are at its arm, which is at a distance of 4-5m. The non-distant cameras are not a problem while the cameras a distance require long wiring capable of withstanding rough terrains, as the robot operates in a rugged outdoor environment.

 

I am looking for the following specifications,

Resolution: 5-20 MP

Frame Rate > 25 FPS

Power Requirement: Max upto 24V

Wire Length: 4-5m

Suitability for outdoor usage

 

Does someone have a good suggestion ? I have checked out the [AES-FMC-MC4-AR0231AT-G](https://www.avnet.com/shop/us/products/avnet-engineering-services/aes-fmc-mc4-ar0231at-g-3074457345635644762/) which is a set of 4 GMSL cameras alongwith all the additional circuitry. But its not mentioned if it is compatible with the Jetson Xavier.

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • narrucmot
    0 narrucmot over 5 years ago

    I don't see a way for the Avnet quad camera FMC to connect to the Jetson Xavier.  That FMC module will work best mated with a Avnet UltraZed SOM (UltraZed-EG ) and I/O Carrier Card (UltraZed-EG IO Carrier Card ).  The two are sold together in a starter kit (https://www.avnet.com/shop/us/products/avnet-engineering-services/aes-zu3eg-1-sk-g-3074457345635014225?CMP=GL-Avnet-E14-… ).

     

    If the Jetson is a requirement then perhaps eCON Systems has what you need:https://www.e-consystems.com/nvidia-jetson-camera.asp#xavier-cameras

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • narrucmot
    0 narrucmot over 5 years ago

    I don't see a way for the Avnet quad camera FMC to connect to the Jetson Xavier.  That FMC module will work best mated with a Avnet UltraZed SOM (UltraZed-EG ) and I/O Carrier Card (UltraZed-EG IO Carrier Card ).  The two are sold together in a starter kit (https://www.avnet.com/shop/us/products/avnet-engineering-services/aes-zu3eg-1-sk-g-3074457345635014225?CMP=GL-Avnet-E14-… ).

     

    If the Jetson is a requirement then perhaps eCON Systems has what you need:https://www.e-consystems.com/nvidia-jetson-camera.asp#xavier-cameras

     

    --Tom