Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Petalinux 2020.1 failed to compile with tagged version
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 354 subscribers
  • Views 1926 views
  • Users 0 members are here
  • Ultrazed Hardware Design
Related

Petalinux 2020.1 failed to compile with tagged version

pmdp3
pmdp3 over 5 years ago

Hello,

 

I am trying to build petalinux using ./make_uz7ev_evcc.sh

I set both the petalinux and the hdl version to tag 2020p1_uz_petalinux_UZ7EV_EVCC_20201104_065342

I am using Vitis 2020.1.

When the code runs create_petalinux_project(), it fails at

petalinux-config --silentconfig --get-hw-description=./hw_platform/ -p ${PETALINUX_PROJECTS_FOLDER}/${PETALINUX_PROJECT_NAME}

with:

[INFO] generating user layers

ERROR: Failed to add user layer: /home/pdaye/workspace/ultrazed/git/avnet/petalinux/projects/uz7ev_evcc_2020_1/project-spec/meta-user

ERROR: Failed to config project.

ERROR: Get hw description Failed!

 

Does anyone have an idea to the reason why it is happening?

Yours,

 

Pierre

  • Sign in to reply
  • Cancel

Top Replies

  • drozwood90
    drozwood90 over 5 years ago +1 verified
    Hi there, I think you changed the wrong variable. You do not change the version from 2020.1. That needs to stay the same. The only thing that would change is the meta-avnet definition in common.sh. However…
  • pmdp3
    pmdp3 over 5 years ago +1
    Thank you, it is working now! Yours Pierre
  • drozwood90
    drozwood90 over 5 years ago in reply to pmdp3 +1 suggested
    Hi there, Without knowing exactly which variables you changed, my feeling, related to what you posted, is you removed the ability of the tool to be able to tell what version of tool it is supposed to work…
  • drozwood90
    0 drozwood90 over 5 years ago

    Hi there,

     

    I think you changed the wrong variable.

    You do not change the version from 2020.1.  That needs to stay the same.  The only thing that would change is the meta-avnet definition in common.sh.

    However, you should not have to modify that either.

     

    All you need to do is pull down that tag itself.  All the variables, tagstamp.txt and anything else would be setup properly.

     

    Here is a script that I use when I am working with the 2020.1 tags/tips/etc.

    copy of getClones.sh

    # Zynq 7000 (non-Vitis)
    #branchTag=2020p1_minized_petalinux_MINIZED_20201104_065342
    #branchTag=2020p1_mz_petalinux_MZ7010_FMCCC_20201104_065342
    #branchTag=2020p1_mz_petalinux_MZ7020_FMCCC_20201104_065342
    #branchTag=2020p1_pz_petalinux_PZ7010_FMC2_20201104_065342
    #branchTag=2020p1_pz_petalinux_PZ7015_FMC2_20201104_065342
    #branchTag=2020p1_pz_petalinux_PZ7020_FMC2_20201104_065342
    #branchTag=2020p1_pz_petalinux_PZ7030_FMC2_20201104_065342
    
    
    # UltraScale+ (Vitis Capable)
    #branchTag=2020p1_ultra96v2_oob_ULTRA96V2_20201104_065342
    #branchTag=2020p1_uz_petalinux_UZ3EG_IOCC_20201104_065342
    #branchTag=2020p1_uz_petalinux_UZ3EG_PCIEC_20201104_065342
    branchTag=2020p1_uz_petalinux_UZ7EV_EVCC_20201104_065342
    
    
    #branchTag=2020.1
    
    
    if [ -z ${PETALINUX_VER+x} ]; 
    then 
         echo "PETALINUX_VER is unset"; 
    else 
         echo "PETALINUX_VER is set to '$PETALINUX_VER'"; 
    fi
    
    
    echo "Cloning '$branchTag'"; 
    git clone https://github.com/Avnet/vitis.git
    cd vitis
    git checkout ${branchTag}
    cd ..
    git clone https://github.com/Avnet/bdf.git
    git clone https://github.com/Avnet/hdl.git
    git clone https://github.com/Avnet/petalinux.git
    cd hdl
    git checkout ${branchTag}
    cd ..
    cd petalinux
    git checkout ${branchTag}
    cd ..

     

    Copy this into ~/getClones.sh

    save it, and set it to executable

    sudo chmod 755 getClones.sh

     

    cd to your projects folder

    ex:

    cd ~/projects
    mkdir getTag
    cd getTag

     

    Run the script

    ./getClones.sh

     

    --Dan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • pmdp3
    0 pmdp3 over 5 years ago in reply to drozwood90

    Hello,

     

    Thank you for your quick response to my request! This is very kind of you.

    I am currently running the code you provided.

    In the meantime, and for my personnal knowledge, I don't understand why meta-avnet should have an impact at this point.

    From my reading of the make_uz7ev_evcc.sh script,

    1. First you check the repos and the env variables
    2. Then you check if you have to build the XSA
    3. Then you create the petalinux projet
    4. Then you configure the petalinux project

    The meta-avnet layer is, from what I understand, added during step 4 (configure_petalinux_project ln 89 call config.board.uz7ev_evcc.sh which does the patching).

    So I don't get where the problem could be as I haven't call the meta-avnet layer at that time...

     

    (In the meantime, the code is finished and it works! Thank you very much)

     

    Yours,

     

    Pierre

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pmdp3
    0 pmdp3 over 5 years ago

    Thank you, it is working now!

     

    Yours

     

    Pierre

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 5 years ago in reply to pmdp3

    Hi there,

     

    Without knowing exactly which variables you changed, my feeling, related to what you posted, is you removed the ability of the tool to be able to tell what version of tool it is supposed to work with - which then upsets a chain of events and other variables related to that.

     

    We are working on some cleaner ways to handle this and trying to make things more clear.  This last release was the first time we tried this.

     

    Regardless, I am very happy that you got everything working now!

     

    --Dan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • pmdp3
    0 pmdp3 over 5 years ago

    Hello,

     

    I am very sorry about that but it seems that the issue was a little bit more complicated than I expected.

    I could use the script you gave and, randomly (which is frustrating 3113.contentimage_1.png), it worked but most of the time it didn't.

    I found this post on the Xilinx forum https://forums.xilinx.com/t5/Embedded-Linux/Petalinux-project-2020-2-failed-to-add-user-layer/td-p/1188455

    in which they suggest to change a sysctl value with

    sudo sysctl -n -w fs.inotify.max_user_watches=524288

    Now, it is working all the time...

     

    In the hope that it could help someone else 8422.contentimage_1.png

     

    Pierre

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 5 years ago in reply to pmdp3

    Pierre,

     

    Thank you for posting that.  I had just seen some other users that needed something like that.  I will make sure to get that added into our VM setup guide.

    It is strange, sometimes people do not need that.  Other times they do.  I did not recommend it as I have yet to work out why that is.  Seems you have pushed it far enough that I think we'll just recommend that change.

    Personally, I've just completed building all of the 2020.1 and 2020.2 images and did not need that change.  Go figure.

     

    --Dan