Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Question about bootloader in "SPI SREC Bootloader Example Design for the Arty Evaluation Board"
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 362 subscribers
  • Views 1214 views
  • Users 0 members are here
Related

Question about bootloader in "SPI SREC Bootloader Example Design for the Arty Evaluation Board"

ischoi
ischoi over 3 years ago

Dear AVNET.

I have a question about your product.

* Product reference)

www.avnet.com/.../UG-AES-A7MB-7A35T-G-Arty-SREC-Bootloader-VIV2015-2-V1.pdf

"SPI SREC Bootloader Example Design for the Arty Evaluation Board"
"LIT# 5185-7A35T-Arty-SREC-Bootloader-VIV2015-2-V1"


Question #1)
In the above PDF datasheet at 10.2 (page 50), "10.2 Program the QSPI Flash Using the SDK".

Is the bootloader "SREC Bootloader" or "SREC SPI Bootloader" ?

In "9.3.4 Description of QSPI SREC Bootloader Source Code Edits". "SREC SPI Bootloader" is used.

But, In 10.2 (page 50), "10.2 Program the QSPI Flash Using the SDK", "SREC Bootloader" seems to be used.

Would let me know the bootloader at "10.2 (page 50)" whether it is "SREC Bootloader" or "SREC SPI Bootloader" ?


It is important for me.

I will really appreciate if I can be given answer.

Thank you very much.

Ick-Sung Choi.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +1 verified
    Hi, Not that I'm knowledgeable on this platform, but it's the same thing I think? It's just terminology. You can call it whatever, it's still a bootloader that uses S-record format, decodes that, and…
Parents
  • shabaz
    +1 shabaz over 3 years ago

    Hi, 

    Not that I'm knowledgeable on this platform, but it's the same thing I think? It's just terminology. You can call it whatever, it's still a bootloader that uses S-record format, decodes that, and programs the storage device over SPI. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • ischoi
    0 ischoi over 3 years ago in reply to shabaz

    Thank you for your answer.
    The configuration flash is connected using SPI interface.
    And the "SREC Bootloader" uses BPI interface.
    It is the problem.
    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ischoi
    0 ischoi over 3 years ago in reply to shabaz

    Thank you for your answer.
    The configuration flash is connected using SPI interface.
    And the "SREC Bootloader" uses BPI interface.
    It is the problem.
    Thank you.