• Question regarding Picozed SDR Development Kit

    Greetings,

    I was wondering if the Avnet ZedBoard 7020 is compatible with other Analog Devices FMC module other than the AD-FMCOMMS2-EBZ ?

    For example, could we use AD-FMCDAQ2-EBZ instead of AD-FMCOMMS2-EBZ ?

    The reason behind that is that I want to plug…

  • Development tool chain to be used to compile and deploy code onto UltraZed-EG™︎ SOM - MPSoC XCZU3EG from Simulink ?

    Hello community,

     

    We would like to know what would be the tools chain to be used to build Simulink models and to deploy the generated code from Simulink to the UltraZed-EGTm SOM - MPSoC XCZU3EG (MCU + FPGA) ?

     

    Actually we are looking for something similar to…

  • Zynq 7000 Flash Compatibility

    Dear Sir:

     

           I would like to verify the compatibility of the flash, non-volatile, memory that I plan to interface with my Zynq 7000 Avnet Zedboard.

     

           I plan to use a Micron, serial, NOR, flash - N25Q256A.

     

           UG908  asserts that the Micron, manufacturer family…

  • How to prevent copy/cloning of exe file in the SD card?

    Hello,

    We are using a Zedboard with an FMCOMMS3 ( from analog devices) for a detector system. The executable file for standalone mode is in the SD card of the Zedboard. We are planning to send the detector for customer trials and evaluation.

     

    How do we…

  • How to prevent copy/cloning of exe file in the SD card?

    Hello,

    We are using a Zedboard with an FMCOMMS3 ( from analog devices) for a detector system. The executable file for standalone mode is in the SD card of the Zedboard. We are planning to send the detector for customer trials and evaluation. 

     

    How do we…

  • Can't rebuild & update rootfs

    my Compile environment is  ubuntun18.4+vitis 2020.2+petalinux 2020.2,

    my hardware is   AVET's  UltraZedTm PCIe Carrier Card ,

    my BSP package is uz3eg_pciec_base_2020_2.tar.gz.

    Below is my question:

     

    1. I  created the petalinux project,and build, package the project…

  • UZ3EG_IOCC: kernel hangs at memory init

    I am using UZ3EG IOCC board. For some reason, I'm not using petalinux tool to build the binaries. So building image independently.

     

    My SDCARD image:

         BOOT.bin

         kernel_image=Image

         devicetree_image=devicetree.dtb

         ramdisk_image=uRamdisk.image.gz

     

    bootargs

  • MiniZed support package for Simulink requires Vivado and SDK 2017?

    Hi All,

     

    I'm trying to install Simulink support for the MiniZed board to try out the Mathworks development workflow. in the "Avnet MiniZed Support Package for Simulink\doc\GettingStarted.mlx document it says that the support package requires Vivado and…

  • How Can I reload the original demo program/FPGA configuration that came installed on my MiniZed board?

    Does anyone know where I would find the original bitstream and demo code that came pre-installed on the MiniZed board?

     

    Thanks in advance for the help and best regards,

    Tom Miller

  • ZedBoard Pmod Headers Not Working

    Hi All,

     

    I am working with a ZedBoard trying to test the output functionality of the Pmod headers. The Pmod headers on this ZedBoard have worked in the past, however, when I try to work with them now it appears that they do not transmit any output data…

  • Micro-SD cards for Zynq Ultrascale+ EV

    We have been using SanDisk 8GB UHS-1 cards with no issue until recently. Our latest board is failing to boot, and I found this document which states the UHS-1 is not optimal for this:

    https://avtinc.sharepoint.com/teams/ET-Downloads/Shared%20Documents…

  • Zedboard:  Non Volatile Memory Application

    Dear Sir:

     

          My apologies if this appears to be a "duplicative" post.   I posted this same question earlier and I received an error message.   I checked in at this website and I did not see this post up on the bulletin board.   So I re-posted the same…

  • u-boot fpga loadb issues on Microzed

    A long time ago, I had written in my notes that I could load the FPGA bitstream via TFTP from the u-boot terminal using these commands:

     

    > tftpboot 0x4000000 192.168.8.20:top.bit

    > fpga loadb 0 0x4000000 0x${filesize}

     

    Now when I try this, it looks like…

  • Micron®︎ Xccela™︎ Flash (MT35X) Development Kit

    Hi everyone,

     

    I have Zedboard and Micron daughterboard. I read the Micron Xccela Flash start guide and it said

     

    Quad-SPI NOR (MT25Q) InstructionsThe daughterboard also supports Micron’s Quad-SPI NOR (MT25Q) memory. Follow these instructions, exceptdownload…

  • CP210X driver install on RHEL?

    The UltraZed-EG starter guide at UltraZed-EG Starter Kit | Zedboard  has a setting up the host PC section that points to www.silabs.com/products/mcu/Pages/USBtoUARTBridgeVCPDrivers.aspx to get drivers.  That page no longer exists.

     

    I did find the https:/…

  • Sealed jumpers MiniZed

    Hi All,

     

    I have just unboxed my brand new MiniZed board and followed the document "MiniZed Getting Started Guide". I noticed that the switch S1 boot mode looks like it's sealed with flux, please have a look at the attached photo.

     

    Is there a…

  • UltraZed EG Starter Kit (AES-ZU3EG-1-SK-G) is not working as expected

    I got an UltraZed EG Starter Kit (AES-ZU3EG-1-SK-G) and followed the instructions steps described inside ultrazed_eg_starter_kit_getting_started_guide_v1_1.pdf (http://zedboard.org/sites/default/files/documentations/ultrazed_eg_starter_kit_getting_started_guide_v1_1…

  • Zedboard doesn't boot - Blue light doesn't turn on

    I received a Zedboard Shipped from a friend for getting some hands-on experience, I tried booting from SD Card and QSPI Flash but cannot get the Blue LED to turn on or anything other than the Power LED to turn on in both the cases. My friend mentioned…

  • Maximum frequency inputs of Zedboard PMODs

    Hi, I am new to the Zedboard. I want to use an ADC with SPI 5MHZ throughout, which means SDO will reach to around 100MHZ  with 16bits. Then, I want to use PMODS JA-JD to receive the data from the ADC. What worries me is that could Zedboard PMOD pins are…

  • Zedboard 7Z020, stopped working? (no power LED)

    I've been running a Zedboard for several weeks, and just noticed it stopped running. It is powered by the 12V 3A barrel connector and those points show 12V. Switching off and switching back on, the green power LED isn't lighted. I do not have any external…

  • MicroZed low power mode

         

    Hi,

    Has anyone tried to put the MicroZed module in low power/sleep mode?

     

    What is lowest power level one can hope for ?

     

    By the way I am aware of Adam Taylor tutorial:

    https://forums.xilinx.com/t5/Xcell-Daily-Blog-Archived/Adam-Taylor-s-MicroZed-Chronicles…

  • UltraZed RMA

    We have two suspected DOA UltraZed-EG SOMs ... what is RMA process.

  • UltraZed Integration

    Our new UltraZrd-EG boards won’t come up on our carrier board (dev kit).

     

    We think the UltraZed is DOA.

  • picozed sdr: reboot fails when boot from qspi

    Hi!

     

    We are trying to boot from the qspi nor (32MB) that is embedded on the picozed. When we have por the image is loaded correctly.

    After that, we are using the whole 32MB of the flash.

    When software reset is performed, than the boot rom can't find the fsbl…

  • I want to display data on screen through HDMI port. Please provide verilog code/algorithm for the same. Note: I have 16 bit data for one pixel.

    I want to display data on screen through HDMI port. Please provide verilog code/algorithm for the same. Note: I have 16 bit data for one pixel.