• Question regarding Picozed SDR Development Kit

    Greetings,

    I was wondering if the Avnet ZedBoard 7020 is compatible with other Analog Devices FMC module other than the AD-FMCOMMS2-EBZ ?

    For example, could we use AD-FMCDAQ2-EBZ instead of AD-FMCOMMS2-EBZ ?

    The reason behind that is that I want to plug…

  • Zynq 7000 Flash Compatibility

    Dear Sir:

     

           I would like to verify the compatibility of the flash, non-volatile, memory that I plan to interface with my Zynq 7000 Avnet Zedboard.

     

           I plan to use a Micron, serial, NOR, flash - N25Q256A.

     

           UG908  asserts that the Micron, manufacturer family…

  • How to prevent copy/cloning of exe file in the SD card?

    Hello,

    We are using a Zedboard with an FMCOMMS3 ( from analog devices) for a detector system. The executable file for standalone mode is in the SD card of the Zedboard. We are planning to send the detector for customer trials and evaluation.

     

    How do we…

  • How to prevent copy/cloning of exe file in the SD card?

    Hello,

    We are using a Zedboard with an FMCOMMS3 ( from analog devices) for a detector system. The executable file for standalone mode is in the SD card of the Zedboard. We are planning to send the detector for customer trials and evaluation. 

     

    How do we…

  • UZ3EG_IOCC: kernel hangs at memory init

    I am using UZ3EG IOCC board. For some reason, I'm not using petalinux tool to build the binaries. So building image independently.

     

    My SDCARD image:

         BOOT.bin

         kernel_image=Image

         devicetree_image=devicetree.dtb

         ramdisk_image=uRamdisk.image.gz

     

    bootargs

  • How Can I reload the original demo program/FPGA configuration that came installed on my MiniZed board?

    Does anyone know where I would find the original bitstream and demo code that came pre-installed on the MiniZed board?

     

    Thanks in advance for the help and best regards,

    Tom Miller

  • Zedboard:  Non Volatile Memory Application

    Dear Sir:

     

          My apologies if this appears to be a "duplicative" post.   I posted this same question earlier and I received an error message.   I checked in at this website and I did not see this post up on the bulletin board.   So I re-posted the same…

  • Micron®︎ Xccela™︎ Flash (MT35X) Development Kit

    Hi everyone,

     

    I have Zedboard and Micron daughterboard. I read the Micron Xccela Flash start guide and it said

     

    Quad-SPI NOR (MT25Q) InstructionsThe daughterboard also supports Micron’s Quad-SPI NOR (MT25Q) memory. Follow these instructions, exceptdownload…

  • Zedboard doesn't boot - Blue light doesn't turn on

    I received a Zedboard Shipped from a friend for getting some hands-on experience, I tried booting from SD Card and QSPI Flash but cannot get the Blue LED to turn on or anything other than the Power LED to turn on in both the cases. My friend mentioned…

  • Maximum frequency inputs of Zedboard PMODs

    Hi, I am new to the Zedboard. I want to use an ADC with SPI 5MHZ throughout, which means SDO will reach to around 100MHZ  with 16bits. Then, I want to use PMODS JA-JD to receive the data from the ADC. What worries me is that could Zedboard PMOD pins are…

  • Zedboard 7Z020, stopped working? (no power LED)

    I've been running a Zedboard for several weeks, and just noticed it stopped running. It is powered by the 12V 3A barrel connector and those points show 12V. Switching off and switching back on, the green power LED isn't lighted. I do not have any external…

  • How to boundary scan the "PICOZED[7Z020]Rev.E" by use the "FTDI MPSSE[c232hm-ddhsl-0]" with VB6

    I have the PICOZED[7Z020] Rev.E and I need to try for connect it with FTDI MPSSE [JTAG] to VB6 for make the boundary scan.

    Set HIGH/LOW/TRISTATE logic to any pins.

    Could you advice me for start it?

  • I want to display data on screen through HDMI port. Please provide verilog code/algorithm for the same. Note: I have 16 bit data for one pixel.

    I want to display data on screen through HDMI port. Please provide verilog code/algorithm for the same. Note: I have 16 bit data for one pixel.

  • How to import the selected communication Core From Opencores.org website to Vivado Project

    Hello everyone,

     

     

    I am new to start my career in FPGA design.

     

    I want to know that how to import the selected communication Core from opencores.org website to vivado project ?

     

     

    Thanking you.

  • How to find the traing courses  about the zedboard?

    Hello :

               Now  I  have a zedboard development board that  is  boought  in  2012. Can I   find  the traing courses  about the zedboard?  Now   I   want  to  ues   vivado2018   to  deveplement   it,but  i cant  not  find  the  Relevant information.  How  should  I do?

  • Does the UltraZed-EV SOM support PCIe Gen3x16 on the PL side?

    This is in regards to UltraZed-EV SOM.

     

    Would I be able to build a custom carrier card that brings out the PCIe interface on the PL side?

  • Getting Started UltraZed - EG : Hello World - FAILED

    Hello Everyone,

    I have an Avnet  Ultrazed EG IO Carrier Card with SoM. I'm newbie in the field so I decided to follow the attached Getting Started.

    I followed all the steps in the UltraZed_EG_Starter_Kit_Tutorial_Vivado_2016_4.pdf.

    When I export my bitstream…

  • unable to read file image.ub

    Hi,

    just got my MiniZed and can no longer read the image.ub-file when starting my minized. I was trying to connect it to wifi following: https://forums.xilinx.com/t5/Xcell-Daily-Blog-Archived/Adam-Taylor-s-MicroZed-Chronicles-Part-207-Setting-up-MiniZed…

  • Can I use AFE7444EVM (JESD204B) with PicoZed FMC Carrier V2?

    Hi,

     

    I am currently developing a new application where I need to measure the FFT of three signals that contain multiple frequency components (between 50 and 400 MHz). My initial plan was to use an ADC evaluation module from Texas Instruments (AFE7444EVM…

  • What Happened To the Speedway Videos

    Just a few weeks ago, there were some great videos by Avnet/Speedway that accompanied the hands-on labs for learning about the Xilinx Zynq 70xx series platforms.  Were the videos moved to a different site/link, or cancelled?  Thanks.

  • Zedboard AXI DMA m_axis_mm2s_tdata[31:0] stuck on zero

    My application is to transfer a 32 bit from DDR (using DMA) to PL.

    I connected the ILA to see the data at the m_axis_mm2s from axi_dma and it shows the m_axis_mm2s_tdata[31:0] always zero besides m_axis_mm2s_tready, m_axis_mm2s_tvalid and m_axis_mm2s_tlast…

  • What linux core minimal image is required for AVNET MicroZed board?

    I have an AVNET microzed board  PB-AES-Z7MB-7Z010-G board.

    After building the operating system - Linux for this device - I get the following error in my console.

     

     

        U-Boot SPL 2019.01 (Dec 04 2019 - 05:18:17 +0000)

        mmc boot

        Trying to boot from MMC1

        spl_load_image_fat_os…

  • AXI Interconnect PS PL on Zynq US+

    Hi everyone,

    I am looking for guidance here:

     

    I need to interface my PS processor (application running on PetaLinux) with an IP created using Vivado HLS. My block design is shown below.

    I just want to pass some data to my IP (sha256), have the calculation…

  • AES-FMC-NETW1-G

    Hi,

     

    Just started trying to use a ZEDBoard with an AVNET AES-FMC-NETW1-G FMC card.

     

    The Zedboard (when using the FPGA image supplied with the Zedboard) programs up fine and the Done LED lights.

    The problem is when I plug in the FMC card adn power up the Done…

  • How to connect ZEDBOARD XADC to external analog input?

    Hi,

    I have a ZEDBOARD which I want to interface it to an analog input signal and see the sinusoidal output. I'm following the lab 3 tutorial by Adam Taylor.

    So, as for the first step, I tried to connect the signal generator to Vn and Vp. I expected…