• Minized: INITRAMFS as root filesystem

    Hello,

     

    I want to build Petalinux 2020.2 for the minized with an INITRAMFS as rootfs (ideally it should be stored into the u-boot fitImage which i believe is called image.ub by petalinux).

    I downloaded the 2020.2 bsp from Avnet website and started a new…

  • Reference Design (Vivado Project) for UltraZed-EV Kit

    Hello,

    I am switching from the original ZedBoard to an UltraZed-EV Start Kit.
    My Problem is that I am unable to find a working reference design (preferrably bare-bones as it can get) for Vivado.
    I tried to start with the following project as a template:

  • Petalinux project created from uz3eg_iocc_2020_1.bsp: No kickstart files from WKS_FILES were found

    Hello community

     

    I've created Petalinux project from BSP (v2020.1) for UltraZed-EG IO Carrier Card by Avnet. I try to build project with petalinux-build instrument and it failed with errors:

     

    ERROR: petalinux-image-minimal-1.0-r0 do_image_wic: No kickstart…

  • Long-wired cameras for Jetson Xavier AGX

    Hi,

     

    I am developing an autonomous robot that navigates using multiple cameras. Some of the cameras (3-4 of them,) are placed near the Jetson Xavier AGX while some of them (2-3) are at its arm, which is at a distance of 4-5m. The non-distant cameras are…

  • Petalinux 2020.1 BSP for Microzed ?

    Hi,

    To allow upgrading a MicroZed based design (industrical application)

    to the 2020.1 version, I am looking for the Petalinux BSP for the MicroZed mZ7010

    (i.e. mz7010_fmccc_2020_1.zip)

     

    Is this available somewhere ?

     

    wkr

    Eddy

  • UltraZed-EV Carrier Card-mounting hardware

    Can someone confirm the mounting hardware specifications for the UltraZed-EV Carrier Card kit? Need dimensions/size of the spacers and screws for mouting the SOM to the carrier card. Have a kit where the SOM mounting hardware has gone missing, and trying…

  • Ethernet Losing UDP Packets

    Problem summary:

    The Zedboard Tm appears to occasionally loose UDP packets across the ethernet interface.

     

    Hardware setup:

    2018.3 prebuilt binary (https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/57639129/Zynq+2018.3+Release)

     

    Test setup:

    A UDP packet is…

  • Zedboard, Spansion S25FL256S Flash Programming, FlashRead() Extra Bytes Discovered

    Dear Sir:

     

         I wrote a simple program that writes a page of data to the Spansion flash (S25FL256S) IC on my Avnet Zedboard and then the reads this same data back for inspection.

     

    I have attached a link below so that anyone can identify the particular Zedboard…

  • Board selection

    Hi,

    We need a Xilinx 7-serious evaluation board that can give us access to 150 I/O ports.

    Most of the boards I checked has limited number of I/Os.

    Would you please advise which boards are available for our application?

     

    Thanks

  • Petalinux and MicroZed BSP problems (2019.1)

    It's great to see an update to the BSPs for the Microzed and other boards. I'm trying to get to grips with Petalinux for the MicroZed and it seemed a bit odd that until recently the latest BSP was for 2018.2.

     

    I'm still having issues with the 2019…