Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design U-boot booting error: "Error" handler, esr 0xbf000002
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 340 subscribers
  • Views 1314 views
  • Users 0 members are here
  • android
  • imx8
  • u-boot
  • maaxboard
  • linux
Related

U-boot booting error: "Error" handler, esr 0xbf000002

zafersen
zafersen over 2 years ago

Hi Everyone,

I am working on u boot configuration for the maaxboard (imx8mq) to port to Android. So, I built u boot successfully with maaxboard_defconfig with some additional configs however, I am getting this error, any one has any idea?

here is my new maaxboard_defconfig I called it maaxboard_android_defconfig

maaxboard_android_defconfig:

CONFIG_ARM=y
CONFIG_ARCH_IMX8M=y
CONFIG_SYS_TEXT_BASE=0x40200000
CONFIG_SYS_MALLOC_LEN=0x2000000
CONFIG_SPL_GPIO=y
CONFIG_SPL_LIBCOMMON_SUPPORT=y
CONFIG_SPL_LIBGENERIC_SUPPORT=y
CONFIG_SYS_MALLOC_F_LEN=0x2000
CONFIG_SYS_MEMTEST_START=0x40000000
CONFIG_SYS_MEMTEST_END=0xA0000000
CONFIG_ENV_SIZE=0x4000
CONFIG_ENV_OFFSET=0x400000
CONFIG_SYS_I2C_MXC_I2C1=y
CONFIG_SYS_I2C_MXC_I2C2=y
CONFIG_SYS_I2C_MXC_I2C3=y
CONFIG_DM_GPIO=y
CONFIG_SYS_EXTRA_OPTIONS="ANDROID_SUPPORT"
CONFIG_SPL_TEXT_BASE=0x7E1000
CONFIG_USB_TCPC=n
CONFIG_TARGET_MAAXBOARD=y
CONFIG_ARCH_MISC_INIT=y
CONFIG_SPL_MMC=y
CONFIG_SPL_SERIAL=y
CONFIG_SPL_DRIVERS_MISC=y
CONFIG_SPL=y
CONFIG_IMX_BOOTAUX=y
CONFIG_DEFAULT_DEVICE_TREE="maaxboard"
CONFIG_DISTRO_DEFAULTS=y
CONFIG_REMAKE_ELF=y
CONFIG_BOOTCOMMAND="run distro_bootcmd;run bsp_bootcmd"
CONFIG_DEFAULT_FDT_FILE="maaxboard.dtb"
CONFIG_SYS_LOAD_ADDR=0x40400000
CONFIG_FIT=y
CONFIG_FIT_EXTERNAL_OFFSET=0x3000
CONFIG_SPL_LOAD_FIT=y
# CONFIG_USE_SPL_FIT_GENERATOR is not set
CONFIG_OF_SYSTEM_SETUP=y
CONFIG_BOARD_EARLY_INIT_F=y
CONFIG_BOARD_LATE_INIT=y
CONFIG_SPL_BOARD_INIT=y
CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_USE_SECTOR=y
CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_SECTOR=0x300
CONFIG_SPL_I2C=y
CONFIG_SPL_POWER=y
CONFIG_SPL_WATCHDOG=y
CONFIG_SPL_SEPARATE_BSS=y
CONFIG_SPL_USB_GADGET=y
CONFIG_SPL_USB_SDP_SUPPORT=y
CONFIG_SYS_PROMPT="u-boot=> "
# CONFIG_BOOTM_NETBSD is not set
CONFIG_CMD_ASKENV=y
CONFIG_CMD_ERASEENV=y
CONFIG_CMD_NVEDIT_EFI=y
CONFIG_CMD_NVEDIT_INFO=y
CONFIG_CMD_NVEDIT_LOAD=y
# CONFIG_CMD_CRC32=y
CONFIG_CMD_MEMTEST=y
CONFIG_CMD_DFU=y
CONFIG_CMD_FUSE=y
CONFIG_CMD_GPIO=y
CONFIG_CMD_I2C=y
CONFIG_CMD_MMC=y
CONFIG_CMD_POWEROFF=y
CONFIG_CMD_USB=y
CONFIG_CMD_USB_MASS_STORAGE=y
CONFIG_CMD_SNTP=y
CONFIG_CMD_BMP=y
CONFIG_CMD_CACHE=y
CONFIG_CMD_EFIDEBUG=y
CONFIG_CMD_RTC=y
CONFIG_CMD_TIME=y
CONFIG_CMD_GETTIME=y
CONFIG_CMD_TIMER=y
CONFIG_CMD_REGULATOR=y
CONFIG_CMD_EXT4_WRITE=y
CONFIG_OF_CONTROL=y
CONFIG_ENV_OVERWRITE=y
CONFIG_ENV_IS_IN_MMC=y
CONFIG_SYS_RELOC_GD_ENV_ADDR=y
CONFIG_SYS_MMC_ENV_DEV=1
CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG=y
CONFIG_NET_RANDOM_ETHADDR=y
CONFIG_SAVED_DRAM_TIMING_BASE=0x40000000
CONFIG_DFU_TFTP=y
CONFIG_DFU_MMC=y
CONFIG_DFU_RAM=y
CONFIG_USB_FUNCTION_FASTBOOT=y
CONFIG_UDP_FUNCTION_FASTBOOT=y
CONFIG_FASTBOOT_BUF_ADDR=0x44800000
CONFIG_FASTBOOT_BUF_SIZE=0x19000000
CONFIG_FASTBOOT_FLASH=y
CONFIG_MXC_GPIO=y
CONFIG_DM_I2C=y
CONFIG_SPL_SYS_I2C_LEGACY=y
CONFIG_SYS_I2C_MXC=y
CONFIG_DM_MMC=y
CONFIG_SUPPORT_EMMC_RPMB=y
CONFIG_SUPPORT_EMMC_BOOT=y
CONFIG_MMC_IO_VOLTAGE=y
CONFIG_MMC_UHS_SUPPORT=y
CONFIG_MMC_HS400_SUPPORT=y
CONFIG_FSL_USDHC=y
CONFIG_DM_SPI_FLASH=y
CONFIG_SF_DEFAULT_MODE=0
CONFIG_SF_DEFAULT_SPEED=40000000
CONFIG_SPI_FLASH_STMICRO=y
CONFIG_PHYLIB=y
CONFIG_PHY_ATHEROS=y
CONFIG_DM_ETH=y
CONFIG_PHY_GIGE=y
CONFIG_FEC_MXC=y
CONFIG_MII=y
CONFIG_PHY=y
CONFIG_PHY_IMX8MQ_USB=y
CONFIG_PINCTRL=y
CONFIG_PINCTRL_IMX8M=y
CONFIG_SPL_POWER_LEGACY=y
CONFIG_POWER_DOMAIN=y
CONFIG_IMX8M_POWER_DOMAIN=y
CONFIG_DM_REGULATOR=y
CONFIG_DM_REGULATOR_FIXED=y
CONFIG_DM_REGULATOR_GPIO=y
CONFIG_SPL_POWER_I2C=y
CONFIG_DM_RESET=y
CONFIG_DM_RTC=y
CONFIG_RTC_EMULATION=y
CONFIG_MXC_UART=y
CONFIG_SPI=y
CONFIG_DM_SPI=y
CONFIG_FSL_QSPI=y
CONFIG_SYSRESET=y
CONFIG_SYSRESET_PSCI=y
CONFIG_DM_THERMAL=y
CONFIG_IMX_TMU=y
CONFIG_USB=y
CONFIG_DM_USB=y
CONFIG_USB_XHCI_HCD=y
CONFIG_USB_XHCI_DWC3=y
CONFIG_USB_DWC3=y
CONFIG_USB_GADGET=y
CONFIG_USB_GADGET_MANUFACTURER="FSL"
CONFIG_USB_GADGET_VENDOR_NUM=0x1fc9
CONFIG_USB_GADGET_PRODUCT_NUM=0x0152
CONFIG_SDP_LOADADDR=0x40400000
CONFIG_DM_VIDEO=y
CONFIG_BMP_16BPP=y
CONFIG_BMP_24BPP=y
CONFIG_BMP_32BPP=y
CONFIG_VIDEO_LOGO=y
CONFIG_SYS_WHITE_ON_BLACK=y
CONFIG_VIDEO_IMX8M_DCSS=y
CONFIG_VIDEO_IMX8M_HDMI=y
CONFIG_SPLASH_SCREEN=y
CONFIG_SPLASH_SCREEN_ALIGN=y
CONFIG_LZO=y
CONFIG_BZIP2=y
CONFIG_OF_LIBFDT_OVERLAY=y
CONFIG_EFI_SET_TIME=y
CONFIG_EFI_RUNTIME_UPDATE_CAPSULE=y
CONFIG_EFI_CAPSULE_ON_DISK=y
CONFIG_EFI_CAPSULE_FIRMWARE_RAW=y
CONFIG_EFI_SECURE_BOOT=y

CONFIG_FASTBOOT_UUU_SUPPORT=n
CONFIG_LZ4=y
CONFIG_FLASH_MCUFIRMWARE_SUPPORT=y
CONFIG_APPEND_BOOTARGS=y
CONFIG_AVB_WARNING_LOGO=y
CONFIG_AVB_WARNING_LOGO_COLS=0x1E0
CONFIG_AVB_WARNING_LOGO_ROWS=0x60
CONFIG_VIRTUAL_AB_SUPPORT=y
CONFIG_ANDROID_SUPPORT=y
CONFIG_ANDROID_AB_SUPPORT=y
CONFIG_CMD_ERASEENV=y

Error  output: 

one more additional info:

I am not getting this error directly, first, the booting seems stuck at trying to boot from mmc1 for a few mins, then throwing errors

U-Boot SPL 2022.04-g1c3c2de440-dirty (Jun 24 2023 - 11:32:31 +0100)
power_bd71837_init
set buck8 to 1.2v for DDR4
DDRINFO: start DRAM init
DDRINFO: DRAM rate 2400MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC1
"Error" handler, esr 0xbf000002
elr: 00000000007e6dc8 lr : 00000000007e6164
x 0: 0000000042200010 x 1: 0000000000000000
x 2: 00cef800a2c87f08 x 3: 00000000fddffff8
x 4: 0000000000000000 x 5: 00cef7ffa4e87f18
x 6: 0000000000000000 x 7: 0000000000000007
x 8: 0000000000000001 x 9: 0000000000000002
x10: 0000000000000002 x11: 000000000000000b
x12: 000000000000001f x13: 00000000ce3935cd
x14: 0000000000901590 x15: 000000000000a7f0
x16: 00000000007eae30 x17: 000000009d7075e5
x18: 0000000000185e40 x19: 0000000042200010
x20: c0c8f800c025b4ce x21: 0000000000000040
x22: 0000000000000040 x23: 0000000042200000
x24: 0000000000000000 x25: 0000000000000000
x26: 00000000007f374a x27: 00000000007f3732
x28: 0000000000000000 x29: 0000000000185c70

Code: 52800105 aa0420c4 710004a5 54ffffc1 (cb030045) 
Resetting CPU ...

resetting ...

image

  • Sign in to reply
  • Cancel

Top Replies

  • ggabe
    ggabe over 2 years ago +1
    I would go back to the vanilla maaxboard_defconfig and reestablish the changes to the file step by step to see on which it breaks.
  • ggabe
    ggabe over 2 years ago

    I would go back to the vanilla maaxboard_defconfig and reestablish the changes to the file step by step to see on which it breaks.