Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design MaaXBoard-RT: ITM_Print (SWO Viewer) - for you
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 341 subscribers
  • Views 270 views
  • Users 0 members are here
  • trace
  • debug
  • MaaXBoard-RT
  • Maaxboard RT
  • ITM
  • SWO
Related

MaaXBoard-RT: ITM_Print (SWO Viewer) - for you

tjaekel
tjaekel over 2 years ago

I have converted a SDK project "hello_word" to MaaXBoard-RT and extended it to demonstrate how to use the ITM Trace as "ITM_Print" (with SWO Viewer in IDE).

The demo project is here:

GitHub - tjaekel/MaaXBoard-RT_ITM_Print: MaaXBoard-RT with SWO Viewer (ITM_Print)

You could also use my "big" (and actual) project which uses also ITM_Print (via command "test"):

GitHub - tjaekel/MaaXBoard-RT_SPIder: MaaXBoard-RT SPIder framework

What is ITM_Print?

ITM_Print uses the "SWO Viewer" (provided by the IDE, when running in Debug mode).

You can print messages via a Debugger channel (ITM Trace), using the SWO signal. You can see messages, when enabled (!), in SWO_Viewer window.
You can also input characters and receive it in your running FW (e.g. waiting for an interaction, take a value before keep going...).
It works like a UART (in and out, bi-directional), with these benefits:

  • you can keep code for ITM_Print in your project: the overhead ("runtime penalty" is very small
    if you do not enable in IDE - your project runs in almost full-speed as possible
  • Even you enable SWO_Viewer in IDE: the overhead is still very small:
    such an ITM_Print does not take huge amount of code, does not have a decrease on performance (speed)
  • All the messages go via a "Debug Channel", like a UART, but it is not an UART (not so slow, not so much code)
  • You have still the user UART available (like a second debug log channel)

ITM_Print is much faster as any real UART debug log (e.g. LPUART1 with 115200 baud rate).

How to enable ITM_Print?

You should take a file "retarget_ITM.c" to your project: get it from SDK repository or from the project(s) above.
It provides functions calls as:

int _write(int iFileHandle, char *pcBuffer, int iLength);
int _read(int iFileHandle, char *pcBuffer, int iLength);

You can also use from "cmsis_cm7.h":

__STATIC_INLINE uint32_t ITM_SendChar (uint32_t ch);
__STATIC_INLINE int32_t ITM_ReceiveChar (void);

Add in "pin_mux.c":

You have to add the config for the SWO signal (so that it comes out).
Add in file "pin_mux.c" these lines of code:

IOMUXC_SetPinMux(
IOMUXC_GPIO_LPSR_11_ARM_TRACE_SWO, /* GPIO_LPSR_11 is configured as ARM_TRACE_SWO */
0U);                               /* Software Input On Field: Input Path is determined by functionality */

IOMUXC_SetPinConfig(
IOMUXC_GPIO_LPSR_11_ARM_TRACE_SWO, /* GPIO_LPSR_11 PAD functional properties : */
0x02U);                            /* Slew Rate Field: Slow Slew Rate
                                      Drive Strength Field: high driver
                                      Pull / Keep Select Field: Pull Disable
                                      Pull Up / Down Config. Field: Weak pull down
                                      Open Drain LPSR Field: Disabled
                                      Domain write protection: Both cores are allowed
                                      Domain write protection lock: Neither of DWP bits is locked */

The clock configuration should be already done (in file "clock_config.c"), as:

/* Configure CSTRACE using SYS_PLL2_CLK */
rootCfg.mux = kCLOCK_CSTRACE_ClockRoot_MuxSysPll2Out;
rootCfg.div = 4;
CLOCK_SetRootClock(kCLOCK_Root_Cstrace, &rootCfg);

Remember, which clock will it generate for the ITM (SWO): in most of the cases, where the MCU clock is set to 996 MHz, it should be 132 MHz (remember both values).

How to enable and use "SWO_Viewer"?

When you start a debug session, open the "Perspective" for "SWO ITM Console" (and also "SWO Trace Config" : which can be invoked from the other one).

You have to configure ITM Trace first: in "SWO Trace Config" and "Configuration" click on "Change":
Provide as parameters:

Core Clock Speed (Hz) :   996000000  (or use "Detect": the clock speed is changed during startup!)
Trace Clock Speed (Hz) : 132000000  (related to the CSTRACE clock speed config above)

SWO_Viewer_Config

Start the SWO_Viewer (the "run" icon needs to be pressed).

Now, you should see all ITM_prints and you are able to use the "terminal" (Console) also for inputs (your FW waiting for something received).

SWO_Viewer_Config

SWO_Viewer

--> Don't forget to press on the "run" icon (the green arrow)

Very helpful feature and very fast log message without to compromise your performance in FW.
A second debug channel and no need to use a slow UART to watch your FW.