Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design MaaxBoard-RT: FLEXIO as SPI Master - for you
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 344 subscribers
  • Views 1013 views
  • Users 0 members are here
  • SPIU
  • serial interface
  • MaaXBoard-RT
  • Maaxboard RT
  • FLEXIO
Related

MaaxBoard-RT: FLEXIO as SPI Master - for you

tjaekel
tjaekel over 2 years ago

I have converted SDK example to use FLEXIO as SPI Master implementation (in addition to regular LPSPI),
and extended/modified the example for MaaxBoard-RT:

It demonstrates how to use FLEXIO to implement a SPI Master device and receive on LPSPI2 as slave (loopback test).
ATTENTION: the Debug UART is LPUART6 (LPUART1 pins are needed for LPSPI2 Slave).

The project is here:

tjaekel/MaaxBoard-RT_flexio_spi_edma_lpspi_transfer_-master_cm7: FLEXIO as SPI master plus LSPI2 as slave (github.com)

With default clock config it works up to 47 MHz, with modified clock config (other and faster PLL for FLEXIO2) up to 258 MHz - impressive.

FLEXIO is a very powerful and flexible block in MCU in order to implement your own or additional interfaces, such as SPI, I2C, LIN, SingleWire, ...
I want to use in order to implement a QSPI interface.

  • Sign in to reply
  • Cancel
Parents
  • tjaekel
    tjaekel over 2 years ago

    With changing the clock sources (and stay within the spec.) - the max. SPI SCLK which works: 30 MHz

    The next higher SCLK speed - 60 MHz - has a wrong waveform:
    there are PCS pulses between bytes and not every byte transfer has the same number of clocks (looks "ugly").

    So,
    30 MHz as SPI SCLK is the max. you can get with FLEXIO2 SPI implementation.

    Remark:
    With regular SPI (e.g. LPSPI4) I can get 45 MHz working properly.
    Next speed step, 66 MHz, works still, but the waveform is not "nice" anymore (a longer SCLK pulse on bit 7).

    So, FLEXIO is slower as regular peripherals can do (in terms of SPI).
    30 MHz is the max. clock for any interface emulated with FLEXIO.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tjaekel
    tjaekel over 2 years ago

    With changing the clock sources (and stay within the spec.) - the max. SPI SCLK which works: 30 MHz

    The next higher SCLK speed - 60 MHz - has a wrong waveform:
    there are PCS pulses between bytes and not every byte transfer has the same number of clocks (looks "ugly").

    So,
    30 MHz as SPI SCLK is the max. you can get with FLEXIO2 SPI implementation.

    Remark:
    With regular SPI (e.g. LPSPI4) I can get 45 MHz working properly.
    Next speed step, 66 MHz, works still, but the waveform is not "nice" anymore (a longer SCLK pulse on bit 7).

    So, FLEXIO is slower as regular peripherals can do (in terms of SPI).
    30 MHz is the max. clock for any interface emulated with FLEXIO.