Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design IMX8M High Assurance Boot (HAB) failing with CAAM error
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 339 subscribers
  • Views 573 views
  • Users 0 members are here
Related

IMX8M High Assurance Boot (HAB) failing with CAAM error

tom-h
tom-h over 1 year ago

Hi all,

I'm not sure if this is the right place for this question, but please point me in the right direction if not!

I am currently trying to use High Assurance Boot (HAB) on my IMX8M device. And run into the following error once I have booted up the device:

U-Boot SPL 2021.04-00002-gf752480a4c-dirty (Nov 15 2024 - 16:47:52 +0000)
power_bd71837_init
set buck8 to 1.2v for DDR4
DDRINFO: start DRAM init
DDRINFO: DRAM rate 2400MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0:  RNG instantiated
Normal Boot
Trying to boot from MMC1
hab fuse not enabled

Authenticate image from DDR location 0x401fcdc0...


U-Boot 2021.04-00002-gf752480a4c-dirty (Nov 15 2024 - 16:47:52 +0000)

CPU:   i.MX8MQ rev2.1 1500 MHz (running at 1000 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 46C
Reset cause: POR
Model: Avnet Maaxboard
DRAM:  2 GiB
Error binding driver 'caam_jr': -96
Some drivers failed to bind
Error binding driver 'simple_bus': -96
Some drivers failed to bind
Error binding driver 'simple_bus': -96
Some drivers failed to bind
initcall sequence 00000000bffcd8d0 failed at call 000000004021c440 (err=-96)
### ERROR ### Please RESET the board ###

HAB relies on CAAM, so I am assuming the issue I am facing is the error in binding the driver 'caam_jr'.

I have followed these steps:

https://github.com/Avnet/uboot-imx/blob/maaxboard_v2020.04_5.4.24_2.1.0/doc/imx/habv4/guides/mx8m_se...

I am using the default branch of uboot-imx:

https://github.com/Avnet/uboot-imx

I also needed to add the following extra config option to resolve an undefined reference to sec_init. Which is related to the SPL in the secure boot.

CONFIG_SPL_CRYPTO_SUPPORT=y;

Please can someone help me understand why I am seeing this error. I have followed the instructions referenced above, so any advice other than what is just included in the instructions would be greatly appreciated!

Thanks,

Tom

  • Sign in to reply
  • Cancel

Top Replies

  • tom-h
    tom-h over 1 year ago +2 verified
    It turns out i needed to use a specific set of branches for each of the components needed to build U-Boot to work with HAB. When using the default branches for each of the following repositories it resulted…
Parents
  • tom-h
    +1 tom-h over 1 year ago

    It turns out i needed to use a specific set of branches for each of the components needed to build U-Boot to work with HAB. When using the default branches for each of the following repositories it resulted in the original error. There may be other combinations that work. Here are the following repos:

    git clone --branch "maaxboard_lf-6.1.22-2.0.0" "https://github.com/Avnet/uboot-imx.git"

    git clone --branch "maaxboard_lf-6.1.22-2.0.0" "https://github.com/Avnet/imx-mkimage"

    git clone --branch "maaxboard_lf-6.1.22-2.0.0" "https://github.com/Avnet/imx-atf"

    curl "https://sources.buildroot.net/firmware-imx/firmware-imx-8.22.bin" --output firmware-imx-8.22.bin

    For me I have been following the IMX8m instructions as listed in my original post. The board I am using is the Maaxboard.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • tom-h
    +1 tom-h over 1 year ago

    It turns out i needed to use a specific set of branches for each of the components needed to build U-Boot to work with HAB. When using the default branches for each of the following repositories it resulted in the original error. There may be other combinations that work. Here are the following repos:

    git clone --branch "maaxboard_lf-6.1.22-2.0.0" "https://github.com/Avnet/uboot-imx.git"

    git clone --branch "maaxboard_lf-6.1.22-2.0.0" "https://github.com/Avnet/imx-mkimage"

    git clone --branch "maaxboard_lf-6.1.22-2.0.0" "https://github.com/Avnet/imx-atf"

    curl "https://sources.buildroot.net/firmware-imx/firmware-imx-8.22.bin" --output firmware-imx-8.22.bin

    For me I have been following the IMX8m instructions as listed in my original post. The board I am using is the Maaxboard.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.