Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design IMX8M High Assurance Boot (HAB) failing with CAAM error
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 339 subscribers
  • Views 574 views
  • Users 0 members are here
Related

IMX8M High Assurance Boot (HAB) failing with CAAM error

tom-h
tom-h over 1 year ago

Hi all,

I'm not sure if this is the right place for this question, but please point me in the right direction if not!

I am currently trying to use High Assurance Boot (HAB) on my IMX8M device. And run into the following error once I have booted up the device:

U-Boot SPL 2021.04-00002-gf752480a4c-dirty (Nov 15 2024 - 16:47:52 +0000)
power_bd71837_init
set buck8 to 1.2v for DDR4
DDRINFO: start DRAM init
DDRINFO: DRAM rate 2400MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0:  RNG instantiated
Normal Boot
Trying to boot from MMC1
hab fuse not enabled

Authenticate image from DDR location 0x401fcdc0...


U-Boot 2021.04-00002-gf752480a4c-dirty (Nov 15 2024 - 16:47:52 +0000)

CPU:   i.MX8MQ rev2.1 1500 MHz (running at 1000 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 46C
Reset cause: POR
Model: Avnet Maaxboard
DRAM:  2 GiB
Error binding driver 'caam_jr': -96
Some drivers failed to bind
Error binding driver 'simple_bus': -96
Some drivers failed to bind
Error binding driver 'simple_bus': -96
Some drivers failed to bind
initcall sequence 00000000bffcd8d0 failed at call 000000004021c440 (err=-96)
### ERROR ### Please RESET the board ###

HAB relies on CAAM, so I am assuming the issue I am facing is the error in binding the driver 'caam_jr'.

I have followed these steps:

https://github.com/Avnet/uboot-imx/blob/maaxboard_v2020.04_5.4.24_2.1.0/doc/imx/habv4/guides/mx8m_se...

I am using the default branch of uboot-imx:

https://github.com/Avnet/uboot-imx

I also needed to add the following extra config option to resolve an undefined reference to sec_init. Which is related to the SPL in the secure boot.

CONFIG_SPL_CRYPTO_SUPPORT=y;

Please can someone help me understand why I am seeing this error. I have followed the instructions referenced above, so any advice other than what is just included in the instructions would be greatly appreciated!

Thanks,

Tom

  • Sign in to reply
  • Cancel

Top Replies

  • tom-h
    tom-h over 1 year ago +2 verified
    It turns out i needed to use a specific set of branches for each of the components needed to build U-Boot to work with HAB. When using the default branches for each of the following repositories it resulted…
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.