Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design maaxboard mickledore branch chromium(chromium-ozone-wayland) service can NOT auto startup on wayland
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 339 subscribers
  • Views 346 views
  • Users 0 members are here
  • chromium
  • maaxboard
Related

maaxboard mickledore branch chromium(chromium-ozone-wayland) service can NOT auto startup on wayland

peterzhanggonewithwind
peterzhanggonewithwind over 1 year ago

hi all,
maaxboard mickledore branch chromium(chromium-ozone-wayland) service can NOT auto startup on wayland!
I used zeus branch before, zeus branch worked. before, for zeus branch I posted the solution here
https://community.nxp.com/t5/i-MX-Processors/how-to-write-a-system-service-to-auto-startup-chromium-on/m-p/1275666
https://community.nxp.com/t5/i-MX-Processors/can-not-auto-startup-chromium-chromium-ozone-wayland/td-p/1241104

but I am using the same chromium.service file as below in mickledore branch , but not work
I login with ssh or serial debugging port with root user directly to run chromium --no-sandbox. it works! and I put the command chromium --no-sandbox in /etc/profile and login it works. but I put the command line in /etc/rc.local not work
anyway I need to auto startup, any solutions are OK for me, but not found

[Unit]
Description=launch chromium

[Service]
User=root
Environment=DISPLAY=:0
Environment=XDG_RUNTIME_DIR="/run/user/0"
Type=oneshot
ExecStart=/bin/sleep 9
ExecStart=/home/myuser/mouse.out &
ExecStart=/usr/bin/chromium --no-sandbox --disable-infobars --user-data-dir=/tmp/chromium --gpu-no-context-lost --enable-gpu-rasterization --start-fullscreen --kiosk --no-first-run --incognito http://localhost:3300/iframe.html &

[Install]
WantedBy=multi-user.target

I ran systemctl status chromium, the error oputput is
chromium.service - launch chromium
Loaded: loaded (/etc/systemd/system/chromium.service; enabled; preset: disabled)
Active: failed (Result: exit-code) since Thu 2024-11-21 23:01:07 UTC; 1min 11s ago
Process: 287 ExecStart=/bin/sleep 9 (code=exited, status=0/SUCCESS)
Process: 653 ExecStart=/home/myuser/mouse.out & (code=exited, status=0/SUCCESS)
Process: 719 ExecStart=/usr/bin/chromium --no-sandbox --disable-infobars --user-data-dir=/tmp/chromium --gpu-no-context-lost --enable-gpu-rasterization --start-fullscreen --kiosk --no-first-run --in)
Main PID: 719 (code=exited, status=1/FAILURE)

Nov 21 23:00:51 maaxboard systemd[1]: Starting launch chromium...
Nov 21 23:01:07 maaxboard chromium[723]: [719:719:1121/230107.465704:ERROR:wayland_connection.cc(209)] Failed to connect to Wayland display
Nov 21 23:01:07 maaxboard chromium[723]: [719:719:1121/230107.465925:ERROR:ozone_platform_wayland.cc(226)] Failed to initialize Wayland platform
Nov 21 23:01:07 maaxboard chromium[723]: [719:719:1121/230107.465963:ERROR:env.cc(225)] The platform failed to initialize. Exiting.
Nov 21 23:01:07 maaxboard systemd[1]: chromium.service: Main process exited, code=exited, status=1/FAILURE
Nov 21 23:01:07 maaxboard systemd[1]: chromium.service: Failed with result 'exit-code'.
Nov 21 23:01:07 maaxboard systemd[1]: Failed to start launch chromium.

any help?
Thank you very much.
I also posted issue here:
https://community.nxp.com/t5/i-MX-Processors/maaxboard-mickledore-branch-chromium-chromium-ozone-wayland/m-p/2000243#M231125

  • Sign in to reply
  • Cancel
Parents
  • peterzhanggonewithwind
    0 peterzhanggonewithwind over 1 year ago

    I did before for zeus branch . it worked, but now mickledore NOT work, any help?

    here before posted: community.element14.com/.../can-not-auto-startup-chromium-chromium-ozone-wayland

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • peterzhanggonewithwind
    0 peterzhanggonewithwind over 1 year ago

    I did before for zeus branch . it worked, but now mickledore NOT work, any help?

    here before posted: community.element14.com/.../can-not-auto-startup-chromium-chromium-ozone-wayland
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.