Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Build PETALINUX by Jtag digilent error
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 362 subscribers
  • Views 934 views
  • Users 0 members are here
Related

Build PETALINUX by Jtag digilent error

nguyenductoan
nguyenductoan over 8 years ago

When i boot petalinux on microzed board by Jtag digilent then there are errors:

"Memory write error at 0xF8900020. AP transaction timeout                                                                                                                                                                              
 invoked from within
"::tcf::eval -progress {apply {{msg} {puts $msg}}} {tcf_send_command tcfchan#0 Memory set siiiiB {ea{o{msg o{} A}}} {JTAG-jsn-JTAG-HS2-210249A0D0F2-4ba00477-0.0 4170186780 4 4 7  }}"
    (procedure "::tcf::send_command" line 4)
    invoked from within
"::tcf::send_command $chan Memory set "siiiiB" "ea{o{msg o{} A}}" [list $ctx $start_addr $size $nbytes $mode $bindata]"
    (procedure "mwr" line 133)
    invoked from within
"mwr -force 0XF890001C 0x00000001"
    (procedure "ps7_post_config_3_0" line 5)
    invoked from within
"ps7_post_config_3_0   "
    (procedure "ps7_post_config" line 12)
    invoked from within
"ps7_post_config"
    (file "/tmp/tmp.JWGp6TOuyk" line 5)"

Can you help me to fix it !!!!

I already install digilent cable driver and program on SDK is OK, but in petalinux-boot --jtag DOSENT work

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Can you boot successfully from SD card?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nguyenductoan
    0 nguyenductoan over 8 years ago in reply to jafoste4

    yes, i did. I built on SD with same image is OK, i follow this instruction:

    https://www.xilinx.com/support/answers/66943.html

    It download to board success but when i checked in terminal get error while load image from kernel:

    "AP transaction error, DAP status f0000021" not match ID, Should i change some thing in vivado design to init ps7_init correctly ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello,

    Are you able to run Hello World over Jtag?

    What application are you running?

    Are you using a JTAG HS3 cable from digilent?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nguyenductoan
    0 nguyenductoan over 8 years ago in reply to jafoste4

    well i have already program many projects or examples like Hello using Jtag on SDK tool (Jtag HS2), but when use petalinux software is impossible

    Hopefully

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nguyenductoan
    0 nguyenductoan over 8 years ago in reply to jafoste4

    here is my log whhen run source file zc702.tcl

    xsdb% source zc702.tcl                                                                                             
    INFO: Configuring the FPGA...
    INFO: Downloading bitstream to the target.
    100%    3MB   0.4MB/s  00:10                                                                                       
    Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0xffffff28 (Suspended)                                         
    mctrlval=30800100
    INFO: Downloading ELF file to the target.
    Downloading Program -- /data/soc_project/sys_3/pre-built/linux/images/zynq_fsbl.elf
        section, .text: 0x00000000 - 0x0000d12f
        section, .handoff: 0x0000d130 - 0x0000d17b
        section, .init: 0x0000d17c - 0x0000d193
        section, .fini: 0x0000d194 - 0x0000d1ab
        section, .rodata: 0x0000d1ac - 0x0000d4f7
        section, .data: 0x0000d4f8 - 0x000101df
        section, .eh_frame: 0x000101e0 - 0x000101e3
        section, .mmu_tbl: 0x00014000 - 0x00017fff
        section, .init_array: 0x00018000 - 0x00018003
        section, .fini_array: 0x00018004 - 0x00018007
        section, .rsa_ac: 0x00018008 - 0x0001903f
        section, .bss: 0x00019040 - 0x0001ae6f
        section, .heap: 0x0001ae70 - 0x0001ce6f
        section, .stack: 0xffff0000 - 0xffffd3ff
    100%    0MB   0.1MB/s  00:01                                                                                       
    Setting PC to Program Start Address 0x00000000
    Successfully downloaded /data/soc_project/sys_3/pre-built/linux/images/zynq_fsbl.elf
    Info: ARM Cortex-A9 MPCore #0 (target 2) Running                                                                   
    Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0xd150 (Suspended)                                             
    INFO: Downloading ELF file to the target.                                                                          
    Downloading Program -- /data/soc_project/sys_3/pre-built/linux/images/u-boot.elf
        section, .text: 0x00400000 - 0x0044125f
        section, efi_runtime_text: 0x00441260 - 0x00441277
        section, .rodata: 0x00441278 - 0x00450eea
        section, .hash: 0x00450eec - 0x00450f17
        section, .dtb.init.rodata: 0x00450f20 - 0x0045441f
        section, .data: 0x00454420 - 0x00456477
        section, .got.plt: 0x00456478 - 0x00456483
        section, efi_runtime_data: 0x00456488 - 0x0045654f
        section, .u_boot_list: 0x00456550 - 0x004572f7
        section, .rel.dyn: 0x004572f8 - 0x00460a3f
        section, .bss_start: 0x004572f8 - 0x004572f7
        section, .bss: 0x004572f8 - 0x00496fdb
        section, .bss_end: 0x00496fdc - 0x00496fdb
    100%    0MB   0.1MB/s  00:06                                                                                       
    Setting PC to Program Start Address 0x00400000
    Successfully downloaded /data/soc_project/sys_3/pre-built/linux/images/u-boot.elf
    Info: ARM Cortex-A9 MPCore #0 (target 2) Running                                                                   
    Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0x3ff94240 (Suspended)                                         
    Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0x0 (Vector Catch)                                             
    100%    0MB   0.1MB/s  00:00                                                                                       
    Successfully downloaded /data/soc_project/sys_3/pre-built/linux/images/system.dtb
    100%   55MB   0.1MB/s  14:44                                                                                       
    Successfully downloaded /data/soc_project/sys_3/pre-built/linux/images/zImage
    Info: ARM Cortex-A9 MPCore #0 (target 2) Running

    ###############################################

    ###############################################

    here is uart terminal on board:

    U-Boot 2016.07 (Mar 02 2018 - 19:10:28 +0700)

    DRAM:  ECC disabled 1 GiB
    MMC:   sdhci@e0100000: 0
    SF: Detected S25FL128S_64K with page size 256 Bytes, erase size 64 KiB, total 16 MiB
    *** Warning - bad CRC, using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Net:   ZYNQ GEM: e000b000, phyaddr -1, interface rgmii-id
    eth0: ethernet@e000b000
    U-BOOT for

    ethernet@e000b000 Waiting for PHY auto negotiation to complete....Uncompressing Linux... done, booting the kernel.

    Error: unrecognized/unsupported machine ID (r1 = 0x00000000).

    Available machine support:

    ID (hex)        NAME
    ffffffff        Generic DT based system
    ffffffff        ARM-Versatile Express
    ffffffff        Xilinx Zynq Platform

    Please check your kernel config and/or bootloader.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer